Power & Energy
  • Technologies
  • More
Power & Energy
Documents Alternative Energy Solutions - Wind Turbine Pitch Control
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 24 Feb 2011 8:13 PM Date Created
  • Last Updated Last Updated: 7 Oct 2021 8:51 AM
  • Views 916 views
  • Likes 0 likes
  • Comments 1 comment
Related
Recommended

Alternative Energy Solutions - Wind Turbine Pitch Control

Alternative Energy Solutions - Wind Turbine Pitch Control

Wind Turbine pitch control system is usually built using a controller to employ the pitch control mechanisms and a feedback module for monitoring the output power. High performance MCUs or DSCs are often selected as the controllers of pitch control systems. They are responsible for giving instructions to pitch control mechanisms based on real-time wind speed, preset power rating, pitch information, and output power signal of generator. Pitch control mechanisms are commonly comprised of a motor and a motor driver. Each motor blade needs a single control mechanism, which means three mechanisms in total are required.

 

After the instructions given by controller are received, the motor drivers drive their associated motors to change blade incidence. Meanwhile, the real-time pitch information is sent back to controller. The feedback module, composed of voltage and current sensors, forms the feedback loop which feeds the voltage and current signals from the sensors back to the controller.

 

When wind speed is not higher than the rated speed, the blade incidence stay near the angle 0° (highest power point). This is similar to that of a generator with constant pitch, generating an output power that changes along with wind speed. At higher wind speeds, the pitch control mechanism changes blade incidence so that the output power of generator is within the allowed range.

 

image

 

       
Visit >
image

 

TEXAS INSTRUMENTSDSCRunning an Application from Internal Flash Memory on the TMS320F28xxx DSP (Rev. I)TMS320F28xxxClick here
TEXAS INSTRUMENTSDSCEEPROM Emulation With the TMS320F28xxx DSCsTMS320F28xxxClick here
TEXAS INSTRUMENTSDSCOptimizing Code Performance and Size for Stellaris MicrocontrollersClick here
TEXAS INSTRUMENTSDSCClocking options for Stellaris Family MicrocontrollersClick here
TEXAS INSTRUMENTSDSCAdvanced Linker Techniques for Convenient and Efficient Memory UsageClick here
TEXAS INSTRUMENTSDSCUsing PWM Output as a Digital-to-Analog Converter on a TMS320F280x (Rev. A)TMS320F280xClick here
TEXAS INSTRUMENTSDSCFlash Programming Solutions for the TMS320F28xxx DSCsClick here
TEXAS INSTRUMENTSDSCAn Overview of Designing Analog Interface With TM320F28xx/28xxx DSCs (Rev. A)TM320F28xxClick here
TEXAS INSTRUMENTSDSCCopying Compiler Sections from Flash to RAM on the TMS320F28xxx DSCsTMS320F28xxxClick here
TEXAS INSTRUMENTSDSCConfiguring Source of Multiple ePWM Trip-Zone EventsClick here
TEXAS INSTRUMENTSDSCTMS320F281x Boot ROM Serial Flash ProgrammingTMS320F281xClick here
NXPMicrocontrollerWakeup from Deep Sleep using the CANActivity interruptLPC1700Click here
NXPMicrocontrollerDSP library for LPC1700 and LPC1300LPC1700Click here
NXPMicrocontrollerUsing the LPC1700 power modesLPC1700Click here
NXPMicrocontrollerFAT library EFSL and FatFs port on NXP LPC1700LPC1700Click here
NXPMicrocontrollerMemory to DAC data transfers using the LPC1700's DMALPC1700Click here
NXPMicrocontrollerNXP LPC Cortex-M3 IEC60335 Class B libraryLPC1700Click here
NXPMicrocontrollerIEC 60601-1-8 audible alert generator using the LPC1700LPC1700Click here
NXPMicrocontrollerLPC1700 Ethernet MII Management (MDIO) via softwareLPC1700Click here
NXPMicrocontrollerLPC1700 RTC hardware auto calibrationLPC1700Click here
NXPMicrocontrollerLPC1700 secondary USB bootloaderLPC1700Click here
NXPMicrocontrollerLPC1700 timer triggered memory to GPIO data transferLPC1700Click here
NXPMicrocontrollerPorting uIP1.0 to LPC1700LPC1700Click here
NXPMicrocontrollerUsing Code Read Protection in LPC1700LPC1700Click here
STMICROELECTRONICSMicrocontrollerUSB DFU protocol used in the STM32Tm bootloaderAN3156STM32F10XClick here
STMICROELECTRONICSMicrocontrollerUSART protocol used in the STM32Tm bootloader  AN3155STM32F10XClick here
STMICROELECTRONICSMicrocontrollerCAN protocol used in the STM32Tm bootloaderAN3154STM32F10XClick here
STMICROELECTRONICSMicrocontrollerSTM32Tm’s ADC modes and their applicationsAN3116STM32F10XClick here
STMICROELECTRONICSMicrocontrollerCommunication peripheral FIFO emulation with DMA and DMA timeout in STM32F10x microcontrollers   AN3109STM32F10XClick here
STMICROELECTRONICSMicrocontrollerManaging the Driver Enable signal for RS-485 and IO-Link communications with the STM32Tm’s USART AN3070   STM32F10XClick here
STMICROELECTRONICSMicrocontrollerConfiguring the NicheLiteTm TCP/IP stack for the STM32F107xx microcontrollerAN3000STM32F10XClick here
STMICROELECTRONICSMicrocontrollerSTM8S and STM32Tm MCUs: a consistent 8/32-bit product line for painless migrationAN2945 STM32F10XClick here
STMICROELECTRONICSMicrocontrollerOscillator design guide for ST microcontrollers AN2867STM32F10XClick here
STMICROELECTRONICSMicrocontrollerSmartcard interface with the STM32F10x microcontrollers AN2598STM32F10XClick here
STMICROELECTRONICSMicrocontrollerEEPROM emulation in in STM32F10x microcontrollers   AN2594STM32F10XClick here
STMICROELECTRONICSMicrocontrollerSTM32F10xxx hardware development: getting startedAN2586STM32F10XClick here
STMICROELECTRONICSMicrocontrollerSTM32F10x in-application programming using the USARTAN2557STM32F10XClick here
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    For a commercial wind turbine, the microcontroller and motor driven pitch control sounds appropriate. For smaller wind turbines; less than 400kW(p), correctly setting the stiffness of a spring in a pitch relaxing mechanism at the rotor might seem equally effective and much less prone to error.  If the wind blows too strongly or gusts, axial movement agianst springs has enough power to move the mechanism and adjust blade pitch, to let through excess wind without transferring excess rotatary power to the driveshaft.  There might be a Dutch patent on that somewhere, so please respect that if there is.  I somewhat wish that I had written it up when I first thought of it, with reference to the pitch control lever mechanism of a fourblade propellor on a Mk.II Spitfire fighter aircraft.  When the gust or period of high winds ends, the spring moves the blade pitch back to maintain best power collection.  Implementing the same function with sensors, motors and microcontrollers would be expensive to develop and even more expensive to test, and in any case if the function were the same as can be implemented with springs it might not really be a difference which gets around the patent.