Power & Energy
  • Technologies
  • More
Power & Energy
Documents 5 Myths About Renewable Energy
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: squadMCU
  • Date Created: 7 Dec 2011 7:18 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 4:46 AM
  • Views 735 views
  • Likes 1 like
  • Comments 1 comment
Related
Recommended

5 Myths About Renewable Energy

Residents of the early 21st century live in quite an exciting time. We have a thriving Internet culture, an unprecedented understanding of the natural world and we can even watch episodes of "The Big Bang Theory" on our mobile phones. But of course, the world is ever in transition, and we currently find ourselves suspended between two ages: a time dependent on fossil fuels such as oil and coal, and a future dominated by renewable energy sources. Yet not everyone is sold on this vision. Options vary on just how dependable some of these renewable energy sources are, as well as how well they'll be able to sustain us in a post-fossil fuel era.
 
Out of all this uncertainty, a number of myths, misconceptions and outright lies have risen to the surface. In this article, we'll forgo the loonier notions out there concerning new world orders and Area 51 battery packs. Instead, we'll look at five of the bigger renewable energy myths currently making the rounds.
 
1. Clean Coal Is the Answer. Coal continues to play a vital role in global energy production, and you simply can't reasonably ask everyone to stop burning it -- not when renewable alternatives aren't ready to pick up all the slack. That's where clean coal enters the picture, theoretically to mitigate the impact of coal pollution until such time as it can be abandoned altogether. Problem solved, right? Wrong. A great deal of clean coal technology centers around capturing and storing pollutants that would otherwise be released in the burning process. With CO2, this involves either pumping the gas down wells to depleted oil fields or into deep-sea depths. Not only can the later option potentially endanger marine ecosystems, but also they both require care and monitoring to prevent polluting the environment anyway. Critics charge that all this amounts to a redirecting of pollution, not a true reduction of it.
 
2. Solar Energy Doesn't Provide Enough Juice. Photovoltaic power may not be in a position to solve all our energy problems right now, but its potential for the future is great. Remember, we're talking about leaching energy from a titanic, star -- one that steers an entire system of planets, our atmosphere and life as we know it.
 
3. Wind Turbines Are Noisy, Costly Bird Killers. To be fair, wind turbines do kill birds -- but so do vehicles, skyscrapers, pollution and the introduction of invasive species into their habitats. As daunting as a field of wind turbines may look, they're responsible for statistically few bird deaths -- less than 1 in every 30,000. But even without the death cries of a thousand birds, aren't wind turbines a noise nuisance? Actually, modern turbine technology renders them relatively silent -- essentially no more than the soft, steady whine of wind through the blades
 
4. Renewable Energy Is Worthless Without Government Incentives. Of course it makes sense to invest in renewable technology if a government program is going to pay for most of it through incentives and tax breaks. But this, they argue, artificially backs an unsustainable energy model. While it's true that renewable energy benefits heavily from government incentive programs, it's important to realize that this is true of most energy sources. This includes everything from gasoline and nuclear power to ethanol production and solar power.
 
5. Renewable Sources Can't Replace Fossil Fuels. Just as it would be unreasonable to think renewable sources could take the reins now, it's equally unreasonable to think they can't eventually facilitate an end to fossil fuel dependency. The transition from the sinking ship of Fossil Fuel to the vessel of the future may take longer than we'd like. We might have to live with both for a while, no matter how much we'd like to see the oil age vanish beneath the waves.
 
 
imageimage
http://static.howstuffworks.com/gif/renewable-energy-myths-4.jpghttp://static.howstuffworks.com/gif/renewable-energy-myths-6.jpg

 

Read the complete entry

  • alternative_energy
  • myths
  • energy_harvast
  • alternative
  • Alternative Energy Tags
  • renewable
  • solar
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    1.  Clean coal

    If there were an economically viable way of doing clean coal, it would have gone into production shortly after the optimistic reports in The New Scientist 20+ years ago.  What we have is oil companies, who need to pump something down the hole to squeeze the oil out at historically rather fast rates, asking for subsidies which could otherwise fund genuinely clean energy sources.

     

    2. Solar

    Is just one of a portifolio of genuinely renewable energy sources.  I like solar because it can be installed close to the point of use.  I'd expect to need 3kW+ on each phase of the mains in every street, in countries with modest sunshine like here in the uk.  In Africa, the income from such generators exceeds typical daily costs per person, so minimising long distance transmission also moves ownership of energy generastors to smallholders who might have a more sensible use for modest income than corporates have.

     

    3.  Wind

    Whilst I am opposed to proliferation of too many windmills; built with money borrowed and left to rust in all the wrong places, I am highly in favour of some windmill building, especially where they are responsibly located and managed, and preferably share a 3-phase connection with farms, factories, villages, or with other generators such as village combined heat&power from biomass plus fossil gas, tidal and wave renewables, and solar power.

     

    4.  Subsidy

    Does the total cost of the US DoD in the 1990's and the 1st Iraq Oil War get counted in estimating the subsidies which you all pay for to have cheaper-than-eqilibrium oil and gas ?  I'd hope that subsidies for truly clean renewables achieve more with less.

     

    5. Irreplaceable Fossil Fuels

    It is true that nothing is better than petroleum for its power to weight ratio of fuel and engines apart from nuclear fuels, and I suppose that we'd not want everyone riding around in trucks which run on plutionium.  For some tasks such as 100-1000km point to point travel, I'd prefer a decrease in the number of journeys made rather than an increase in borrowing to pay for big petroleum cars which are good at such jouneys.  For 1 to 100km travel, trains are most efficient or small electric cars most flexible for point to point.  I'd expect some of each.  What we have at the moment is a lot of work being done to transport four heavy chairs and a fancy stereo more than 100 km, with batteries four to ten times bigger than are needed to move two people plus luggage 1 to 100km point to point.  I wonder if the marketing department set the specification?  They are the same people who thought that a premium Hummer was a good choice, which might suggest that we should not listen to them.

     

    When there is a basic <0.8 tonne electric car on the market, that is when I'd consider buying one.  Until then, we have only what we can figure out how to make.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 14 years ago

    1.  Clean coal

    If there were an economically viable way of doing clean coal, it would have gone into production shortly after the optimistic reports in The New Scientist 20+ years ago.  What we have is oil companies, who need to pump something down the hole to squeeze the oil out at historically rather fast rates, asking for subsidies which could otherwise fund genuinely clean energy sources.

     

    2. Solar

    Is just one of a portifolio of genuinely renewable energy sources.  I like solar because it can be installed close to the point of use.  I'd expect to need 3kW+ on each phase of the mains in every street, in countries with modest sunshine like here in the uk.  In Africa, the income from such generators exceeds typical daily costs per person, so minimising long distance transmission also moves ownership of energy generastors to smallholders who might have a more sensible use for modest income than corporates have.

     

    3.  Wind

    Whilst I am opposed to proliferation of too many windmills; built with money borrowed and left to rust in all the wrong places, I am highly in favour of some windmill building, especially where they are responsibly located and managed, and preferably share a 3-phase connection with farms, factories, villages, or with other generators such as village combined heat&power from biomass plus fossil gas, tidal and wave renewables, and solar power.

     

    4.  Subsidy

    Does the total cost of the US DoD in the 1990's and the 1st Iraq Oil War get counted in estimating the subsidies which you all pay for to have cheaper-than-eqilibrium oil and gas ?  I'd hope that subsidies for truly clean renewables achieve more with less.

     

    5. Irreplaceable Fossil Fuels

    It is true that nothing is better than petroleum for its power to weight ratio of fuel and engines apart from nuclear fuels, and I suppose that we'd not want everyone riding around in trucks which run on plutionium.  For some tasks such as 100-1000km point to point travel, I'd prefer a decrease in the number of journeys made rather than an increase in borrowing to pay for big petroleum cars which are good at such jouneys.  For 1 to 100km travel, trains are most efficient or small electric cars most flexible for point to point.  I'd expect some of each.  What we have at the moment is a lot of work being done to transport four heavy chairs and a fancy stereo more than 100 km, with batteries four to ten times bigger than are needed to move two people plus luggage 1 to 100km point to point.  I wonder if the marketing department set the specification?  They are the same people who thought that a premium Hummer was a good choice, which might suggest that we should not listen to them.

     

    When there is a basic <0.8 tonne electric car on the market, that is when I'd consider buying one.  Until then, we have only what we can figure out how to make.