Robotics
  • Technologies
  • More
Robotics
Blog [Building a Quadcopter] [Part 2]
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ipv1
  • Date Created: 4 Nov 2014 7:18 AM Date Created
  • Views 2382 views
  • Likes 2 likes
  • Comments 13 comments
  • inderpreet
  • frame
  • ip_iot
  • quadcopter
Related
Recommended

[Building a Quadcopter] [Part 2]

ipv1
ipv1
4 Nov 2014

Prelude

The previous post is at: [Building a quadcopter] [Part 1]

 

In the last post, I started by linking to the various resources and buying the basics and then testing the 'air' by getting the motors to run. In this post I will share my experience in building my own frame.

 

The frame

 

Since the BLDCs and ESC are OK tested at this point, I wanted to start with the frame. A look online and those carbon fibre frames are beautiful. Unfortunately, they are also very expensive and for those who know me, I get an allowance that keeps my shopping habits in control. Hence the next best thing is to build one. Easier said than done, what do I build with? I have a lot of scrap wood lying around so that would be  my material of choice. But before we start we need instructions or atleast some design rule with which to work.

 

Using google, I found these.

  • http://blog.oscarliang.net/build-a-quadcopter-beginners-tutorial-1/
  • Quadcopter project - Homemade frame - Pylo
  • Cheap, Sturdy, 1-Hour Quadcopter
  • http://copter.ardupilot.com/wiki/advanced-multicopter-design/

 

The interesting stuff is the dimensions. I was not able to find the exact theory behind the frame design but I did get an idea of what could be right. Here is a drawing from the above links

image

 

 

I am using 10 inch props so this could have been used as is. But I increased the distance between props from 10.5in to 16in. This was because I wanted to give the electronics a little more room an wanted to experiment with larger frame dimensions. In my mind, if I increase the inter prop distance, I will gain manuverability- sensitivity to small changes in prop RPMs (newton's levers right?) On the other hand, I will loose stability. Thats OK since I am going to experiment and if I find it to be too unstable, I can always shorten the arms.

 

With that, I took some scrap wood and sandwiched the joints in plywood in the center. The result is...

image

The motors needed to be mounted hence a bit of drilling was necessary. I also made some sinks for the shaft of the motors. Applicable for this case but may not be necessary for all motors.

image

image

image

 

Some zip ties and we have the ESC in place.

imageimage

Thats good. Now I need some landing gear. For that I had some 8in  PVC pipes in the scrap. So I cut some rings out and stuck them to the arms of the quad. The result is easier to understand...

image

With that we have a frame. I did take test electronics and mount them on the frame then wired a long wire to a pot and tried to see if it could lift. Here is the result.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

As you can see we need a brain for this thing. In the next post I will try some sensors and see if we can design a logic for this thing.

 

Cheers,

IP

  • Sign in to reply

Top Comments

  • DAB
    DAB over 12 years ago +1
    From baby steps to the sky above. Not bad for a quick and dirty airframe. DAB
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago +1
    I like the simplistic approach, it is nice to see a project not involving expensive parts to make it work, instead going for the home made solution, very cool. I am watching with interest as this is a…
  • shabaz
    shabaz over 12 years ago in reply to Robert Peter Oakes +1
    Hi! Great idea, definitely could be worth an experiment. I know nothing about air quality sensors, so I'm guessing, but I suppose depending on the type of sensor, it might need air flow anyway (although…
Parents
  • DAB
    DAB over 12 years ago

    From baby steps to the sky above.

     

    Not bad for a quick and dirty airframe.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 12 years ago

    From baby steps to the sky above.

     

    Not bad for a quick and dirty airframe.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • ipv1
    ipv1 over 12 years ago in reply to DAB

    Thank you sir,

    I'm learning.

     

    Ip