Robotics
  • Technologies
  • More
Robotics
Blog Building a Robot! (Simulated)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 12 Nov 2015 6:33 PM Date Created
  • Views 2939 views
  • Likes 9 likes
  • Comments 24 comments
  • simulation
  • robotics
  • gazebo
Related
Recommended

Building a Robot! (Simulated)

shabaz
shabaz
12 Nov 2015

After having built a couple of small wheeled platforms (a crude attempt called XMP-1 and a slightly better one called XMP-2) I was curious what simulation tools were out there specifically geared toward robotics design.

This is just a quick summary of one of the simulation tools that are available, called Gazebo.

 

Gazebo was incredibly easy to get going – a single command line will install it onto Linux, and when run it is easy to add bits and pieces from the toolbar and get going.

I’ve yet to work through the tutorials but I’m hoping to eventually simulate XMP-2 so I can write better code easily.

 

Here is a screenshot of Gazebo, and a quick video showing some basic physics, pushing the robot into coke cans.

image

 

Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

More complex movements are possible too. Here is a robot gripper with torque being applied to part of it:

image

Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The simulation includes gravity and friction and many attributes are configurable.

The models can be created in XML files, and the tutorials look comprehensive.

The example below from a tutorial shows a snippet of a robot, where a box-shaped chassis is needed. The <pose> element contains the position (xyz, and orientation in three dimensions). The <collision> and <geometry> elements contain a <box> element which defines a box of size 0.4x0.2x0.1m in this example.

Usually they are the same; one element is used for the graphics, and the other is for the collision-detection algorithm to use.

image

 

The simulation can be connected up to real hardware or software through the use of an application programming interface (API), so it is possible to test robotics software before you've built the hardware, or you can interface your sensors and start programming movements.

It all looks extremely interesting!

Check out the second part by clicking here, which goes into detail about how to construct a model (based on a real hardware robot called XMP-2) and how to control it using external stimulus.

  • Sign in to reply

Top Comments

  • DAB
    DAB over 10 years ago +1
    I agree. I was not aware that Gazebo existed, but it definitely looks interesting to look at mechanical designs. I will add it to my list of tools to check out. Thanks, DAB
  • shabaz
    shabaz over 10 years ago +1
    Hi Shabaz! Really, thank you to point on this. It seems very good. At the moment I am working on the following "robotizations" Camera slider with controller and horizontal programmable movement; camera…
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to shabaz +1
    Hello Shabaz! Many thanks for the update. In the meantime I am installing the software that is really intriguing. I'm going to try and understand how to produce a simple single mechanical movement or linkage…
Parents
  • balearicdynamics
    balearicdynamics over 10 years ago

    Hi Shabaz!

     

    It sounds strange but I had serious problems installing Gazebo with the single-command. Used a newly fresh installation of Ubuntu 14.04.3 LT (the last updated) and I get serious issues of dependencies. Maybe there is something I have missed or not read in the Gazebo installation tutorial. What method did you used? The shell script I have downloaded it from the main gazebo site ...

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to balearicdynamics

    Hi Enrico,

     

    I Installed ubuntu-14.04.3-desktop-amd64.iso and then in a terminal as normal user did 'sudo ls' (just so that it wouldn't

    prompt for a password during the single install line below, which includes sudo in there; probably I didn't need to

    do this, but just in case) and then did this command line:

    wget -O /tmp/gazebo6_install.sh http://osrf-distributions.s3.amazonaws.com/gazebo/gazebo6_install.sh; sudo sh /tmp/gazebo6_install.sh


    and then it was able to run (by typing gazebo).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to balearicdynamics

    Hi Enrico,

     

    Ah, that's it. Just found this which appears the same sympton:

    https://bitbucket.org/osrf/gazebo_tutorials/issues/42/gazebo6-installation-failing-on-ubuntu

    That user's solution was to install 64-bit.

    That URL appears to have set the issue to 'resolved' but I don't see why. Surely users on 32-bit would still experience the issue : (

    Anyway, not sure where the root cause is, but 64-bit will work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to shabaz

    Hello Shabaz,

     

    thank you for the link. Good to know, so (just a minute) I will remove the vm, download the 64 bit version then install it etc ...  image I'll notice you if it works of if it is a problem of the island.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to shabaz

    Hi Shabaz,

     

    we can definitely consider the issue specific of the Ubuntu 32 bit. Unfortunately this is not mentioned at all (by contrary the declare the support for both 32 and 64 bit versions). I have recreated a VM with Ununtu 14.04.3 LT 64 bit just now, following - as you have done - a normal installation. Then launched the script (using wget instead downloading the script but I think it is the same). Gazebo started the installation, downloaded all the packages and all completed without any warning nor errors. Launched gazebo... Et voilá image

     

    Thank you for your support and feedback. Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to balearicdynamics

    Hey Enrico,

     

    That's awesome!

    Yeah it was just chance that I'd picked 64-bit. If I'd picked 32-bit I would have been totally stuck.

    Glad it is functioning. Have fun!! Will be interesting to see what uses we can put such an application.

    I've yet to use the API, but might take me a week to get round to that : (

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to shabaz

    Hi Shabaz!

     

    We should keep this post alive...

     

    The project I am working on are also partially work, so I will use it asap. What I should explore is if the program can accept external cad drawings in some formats. Not essential but useful in some cases.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to shabaz

    Hi Shabaz!

     

    We should keep this post alive...

     

    The project I am working on are also partially work, so I will use it asap. What I should explore is if the program can accept external cad drawings in some formats. Not essential but useful in some cases.

     

    Enrico