Robotics
  • Technologies
  • More
Robotics
Blog Drones get OK’d to fly, lend a helping hand
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 6 Jun 2014 6:51 PM Date Created
  • Views 2942 views
  • Likes 0 likes
  • Comments 26 comments
  • privacy
  • law
  • rules
  • drone
  • spy
  • cabeatwell
  • camera
  • surveillance
Related
Recommended

Drones get OK’d to fly, lend a helping hand

Catwell
Catwell
6 Jun 2014

Drones are becoming more and more apparent in everyday life. When they aren’t being used to film tricky angles in the next Fast and the Furious movie (we know... give it a break), they’re being used to ticket drivers with a particularly heavy foot. While certain people are a bit nervous around the flying machinery, some new drones may win their hearts for the very cool services they are providing to society.

 

image

Draganflyer X4ES (image courtesy of DraganFly)

 

Probably one of the coolest new drones out on the market is the Draganflyer X4ES, which will be used as a farmhand to farmers by monitoring crops and testing soil quality. The 36.25in box is equipped with Sony cameras and is similar to a helicopter in its flight style. The drone was recently approved by the U.S. Department of Transportation’s Federal Aviation Administration to engage in a clinical trial on North Dakota farms to see just how useful the flying machines can be.

 

The program is the first of many to go live on one of six FAA unmanned aerial systems test sites, selected by Congress in 2013. Two separate trials will be conducted to discover whether or not it’s worthwhile to regularly utilize drones as farmhands in the foreseeable future.

 

FAA Administrator Michael Huerta said the test will be incredibly important for assessing the risk and safety of utilizing the technology regularly within the country. The tests will not only assess the feasibility of using drone technology to enhance agriculture, but also aims to show the public the benefits of drone technology.

 

The first test will run May 5th at North Dakota State University’s Carrington Research Extension Center. The second and final test will run at Sullys Hill National Game Preserve over the summer. The flight permit is, however, valid for two years and the machines are likely to take to the skies yet again. The drones that weren’t asked to participate in this year’s agricultural tasks will take on other notable projects, including aiding in the recovery of WWII soldiers.

 

Drones are the newest addition to the BentProp Project, which seeks to recover casualties from WWII. When the initiative took to the water, drones were the perfect candidate for the job. Team members relied upon 3D Robotics’ octocoper drones, which both mapped out the environment and discovered hot spots that might have represented still-active bombs. The drones were a huge aid to the tactics team, giving them the best insight on where to search first.

 

image

3D Robotics’ Quadrocoper (image courtesy of 3D Robotics)

 

Despite the benefits drones bring to society through their advanced aerial technology, public opinion about them remains relatively unchanged. A recent survey conducted by Pew Research discovered that 63 percent of Americans believe the nation would be worse off if commercial or personal drones are granted flight clearance. Overall, the study found that 59 percent of the population believes technology will enhance their lives, but depending on the industry, people seem to be rather frightened by this advancement. It doesn’t seem our world will be robot-run anytime soon. Sorry, George Jetson.

 

C

See more news at:

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • Problemchild
    Problemchild over 12 years ago in reply to Problemchild +2
    An Owl for Shabaz www.youtube.com/watch
  • shabaz
    shabaz over 12 years ago in reply to mcb1 +1
    It's an interesting thought experiment. If UAVs became one day safer than road vehicles, (e.g. vision/sensors improving to the point that it's safer than a human) would people want to reduce the lorries…
  • Problemchild
    Problemchild over 12 years ago in reply to Problemchild +1
    A donkey type of device may well be more useful after all we have used donkeys for thousands of years for lugging heavy stuff but haven't used Eagles to carry much other than the occasional secret letter…
Parents
  • mcb1
    mcb1 over 12 years ago

    These are interesting reading with regard to operation in commercial airspace.

    http://www.scoop.co.nz/stories/AK1209/S00384/wellington-unmanned-drone-poses-significant-safety-risk.htm

    http://www.stuff.co.nz/the-press/business/9885743/Getting-commercial-drones-aloft-proves-tricky

    Tiny drones pose air safety risk - National News | TVNZ

     

    Bearing in mind that radar doesn't cover the oceans and there is a dependance of aircraft based systems to report where they are.

    http://www.nzherald.co.nz/nz/news/article.cfm?c_id=1&objectid=10875042

    http://www.nzherald.co.nz/nz/news/article.cfm?c_id=1&objectid=10874979

     

    Every other object that flies in the airspaces requires to have a transponder, but no-one has come up with something for drones.

    I think more focus on how to identify where they are is equally important, which will also help with the complaints from neighbours, etc.

     

    Mark

     

    and this conversation is one that is more worrying due to ignorance of what the rules are and why.

    http://www.parkflyers.org.nz/modules/newbb/viewtopic.php?topic_id=4069

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to mcb1

    I'm no expert in this, but I was wondering, I suppose if these devices had the capability to (say) automatically self-land in a slow controlled manner when batteries are running low, have some mechanisms to avoid flying into people (e.g. thermal or usual camera imaging) then it might accelerate getting accepted by many people, i.e. some basic set of requirements that should be something that people could look for when purchasing these, e.g. a "safety level 1" mark (not saying this needs legislation [I know nothing about quadcopters so I can't comment]).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 12 years ago in reply to mcb1

    I'm no expert in this, but I was wondering, I suppose if these devices had the capability to (say) automatically self-land in a slow controlled manner when batteries are running low, have some mechanisms to avoid flying into people (e.g. thermal or usual camera imaging) then it might accelerate getting accepted by many people, i.e. some basic set of requirements that should be something that people could look for when purchasing these, e.g. a "safety level 1" mark (not saying this needs legislation [I know nothing about quadcopters so I can't comment]).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mcb1
    mcb1 over 12 years ago in reply to shabaz

    Shabaz, John

    The issue is a drone or more correctly a UAV (Unmanned Aerial Vehicle) is not just your average toy quad, hex or even opto-copter.

    There are some serious sized ones out there being used for Search and Rescue, along with the really large sized Military drones we've seen.

    Currently NZ Coastguard have one large enough to drop a liferaft and can fly for 12-13hrs before refuelling.

     

    Anything flying in a controlled airspace is either a hazard because it could end up getting sucked into an engine (birds get chopped up, but metal things tend to destroy the blades), or a distraction to pilots landing, hence the need to control airspace around an airport.

    Aircraft generally have a transponder on board which is then visible to ATC and can interact with the other aircraft's TCAS system, so even if they haven't filed a flight plan (ie told ATC where they are going), the systems can work to avoid a near miss, or collision.

    I know there is work being done to provide an approved 'transponder' that will suit UAV, but it's not public information and I'm not sure of the size UAV they wish to apply them to.

     

     

     

    For hazards to persons on the ground, then yes in an ideal world the safety mechanism onboard could make a controlled descent.

    Will this always work?, From my many years in electronics, failure is inevitable ...it's just when.

    Can you safely land an opto-copter with a 2kg payload and 8 high speed and very sharp blades into a crowd of people from above when they are crossing a noisy street.?

    I suggest NO, so the 'fail to safe' option here is limit where and when they can fly.

     

    Is it fair?. Well maybe not, but then the only uncontrolled thing I know on the streets is a bicycle, skateboard or mobility scooter, since you don't need registration or a licence/test to operate it, and it's capable of injuring one or more people, however they don't generally sneak up on you from above.

     

     

    The noise issue is a secondary problem, that the various regional or local authorities can control, in much the same way if you decided to play loud music all the time.

    Luckily in America you can carry a gun and use it, so you have the distinct advantage of shooting the damn thing, and if the operater was using POV display he might get the idea when you wave the gun at it.

     

    So while the PR types sit in their rooms dreaming up these weird and wacky marketing ideas, the real world tends to apply logic and safety so that no-one gets hurt.

    When you're sitting in the aircraft about to take-off or land, you might want to contemplate on which side is making the rules for your safe flight.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to mcb1

    Yeah the sub foot diameter things are fairly harmless but as you say I've seen plenty even around here used for  Photographic purposes that are over a Metre in diameter and stay up for ages. Now the price has reduced and they are proliferating I can as you say see the problems when them and us interact.

     

    Mark could you imagine a world where 1000's of Amazon Drones dance across any given city delivering your orders, they would be quite massive ...BOZO Drone image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to Problemchild

    could you imagine a world where 1000's of Amazon Drones dance across any given city delivering your orders

    No. It's fantasyland as the reality is far too hard to do in the real world.

    It would need a vision system to deal with wires, trees and other unplanned obstacles.

     

    In NZ (and I imagine similar in the rest of the world) the limit for aircraft is 1000ft over a built-up area, and 500ft over rural.

    A 2, 3 or even 5kg payload is a lot of damage if it were to have the ability to go bang.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to mcb1

    Yeah, obviously an explosive one would be very bad but they wouldn't care about the rules anyway .

     

    A 5Kg package would mean at least  say a 20 KG craft. Could you imagine a 25KG craft with blades crashing in to you at say 50+MPh  or a car or even a house it would cause plenty of damage!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to Problemchild

    You are right about not caring about rules, however currently anything like that attracts a lot of attention, since its NOT normal.

     

    I'm not sure about weight to payload, but like most things that defy gravity, every extra kg means more fuel, so the battery will be a limiting factor for run times to be worthwhile.

     

    In this whole fantasy, the delivery is probably the least expense, since you still need to warehouse the goods, arrange for a robot/human to remove it, and package it for flight, program the drone about where to fly and attach the package, then open the door and send it, along with the return.

    So I'm unsure where they think they will save money, given the high initial cost, and the high maintenance v a few dollars to the courier.

     

    There are some potential uses for SAR, but from what I've seen so far its the designer/supplier who is providing most of the "need".

    We saw a few get used in Chch after the earthquakes to survey the inside of buildings, but the reality was the pictures were not HD quality, they kicked up dust making close inspection a problems, and one became MIA, so what use they were is debatable when you can't see cracks in structural beams, etc.

     

    There is GPS controlled one that a guy in our club used to take regular videos over the city centre, but was done with full permission.

    https://quakestudies.canterbury.ac.nz/store/collection/350

    http://www.ceismic.org.nz/news/aerial-videos-of-christchurch

     

    Mark