Robotics
  • Technologies
  • More
Robotics
Blog My Path to Learn Robotics
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: yosoufe
  • Date Created: 2 Mar 2021 9:17 PM Date Created
  • Views 4176 views
  • Likes 13 likes
  • Comments 11 comments
  • intel
  • robotics
  • opencv
  • realsense
  • 3d scanning
Related
Recommended

My Path to Learn Robotics

yosoufe
yosoufe
2 Mar 2021

Hello,

The main purpose of this post is to break the long silence in the Robotics Section of the element14 and also a bit of showing off my progress on my personal learning experience.

 

Please let me know what you think and if you like these kinds of blogs in element14.

 

  • Introduction
  • What I have done
  • Next step
  • Some Links

 

Introduction

I would like to learn about mapping and one of the relatively affordable options is experimenting with Intel RealSense sensors. They are not cheap but they are much cheaper than industrial LIDAR. There are still more affordable LIDAR options like Slamtec LIDARs but they are only in 2D.

 

So here we go. I have chosen RealSense sensors for my learning.

  • D435i which is an RGB-D sensor which means it can output depth information as well as color.
  • T265 which is using two gray-scale fish-eye cameras and outputs the pose of the camera relative to the location when it turned on. It does the visual odometry on the camera and frees the CPU and the application writer from this calculation.
  • Both of them connected through USB and USB 3.0 would give the best perfomance.

 

The following image is showing my setup. The Top sensor is the D435i and the bottom one is T265. They are both connected to a NVIDIA Jetson Nano (very first version) and the whole system is mounted on a 3D printed chassis that I modified and printed from the DonkeCar Project. You can find the fusion 360 model of the chassis here: https://a360.co/2E9mb4H . I tried to use the preview embedding feature of fusion 360 here but it did not work.

 

{gallery:width=740,height=600,autoplay=false} My Gallery Title

image

My Setup

 

What I have done

To start I needed a way to read the sensor data in Jetson Nano. Unfortunately they do not release the binaries for the Jetson but there are some instructions on how to compile the library from the source and install it on Jetson. Here I documented how I am compiling the librealsense for Jetson and specific python version.

 

The other challenge is that they do not have python examples as much as C++ examples, so I had to convert their C++ examples into python. What I like about python is the pydoc module that shows the documentations and all available functions and classes in all the modules.

 

python3 -m pydoc -p 9999

 

This is running a web server at localhost:9999 that includes all the documentation of all modules. Using docs and the C++ examples I could write some python scripts to capture the data from these two senors.

 

For visualization of the 3d data I decided to use Pangolin. Pangolin is a lightweight wrapper for OpenGL and I saw it being used in some open source SLAM (Simultaneous Localization and Mapping) Projects. It was quite fast and easy to draw something on the screen in 3D for me. Consider that I am not that much familiar with computer graphics. And of course they have python bindings.

 

I had some results being able to draw the sensor measurements live on the screen as point cloud until the following gif image that I am very happy about.

 

image

 

Why am I happy? Here you see a mouse sitting on a table beside some orchids. The point cloud data is coming from different location of the sensors in space. but the objects are being drawn on the screen relatively in a fix location. I know it is not perfect. They are moving a bit. But this means to some extent It knows where sensor is in 3D space and from where it is capturing the measurements.

 

To be more clear, you are seeing this.

 

image

 

Why isn't it perfect? The big factor is that I am still not considering the displacement between two sensors. I am finding the pose of the sensors from the T265 sensor and getting the point cloud from D435i. But these two are not exactly on top of each other. So using the pose of the T265 for D435i is not exactly correct here. So the next step is to calibrate these two sensor relative to each other and find the displacement between these two. That is next step.

 

The sensor measurements are in different coordinate systems. The point cloud in the following system relative to D435i.

 

image

and the poses from T265 is in the following coordinate system

image

Of course I considered this rotation to calculate the points relative to a fixed coordinate system. But I am ignoring the displacement between two sensors. Intel has a good articles about the coordinate systems of these two sensors here and here.


The following image shows a the math I used so far. Currently I am ignoring the translation part of the transformation matrix between the two sensors.

 

image

 

Next step

is proper calibration of these two sensor. I have some ideas about calibration. I had to do a similar thing as an assignment as a job interview in US (although I did not get that job) It was fun experience and I documented that here: https://github.com/yosoufe/CameraLidarCalibration

 

 

Since I am just playing with these stuff. there is no force on what to do next. There are other options to learn. For example recently I learned a bit about deep learning for classification of point cloud data. It would be interesting to try it with live sensor measurements.

 

Some Links

  • I am doing this work on my GitHub repository here.
  • Intel RealSense
  • Sign in to reply

Top Comments

  • robogary
    robogary over 5 years ago +6
    Truely awesome work, the 3D is impressive. Donkey Car is on my bucket list, and of course the vision system is key. I've used a PIXYCAM (with Arduino) on a project, and that was tough challenge for me…
  • dubbie
    dubbie over 5 years ago +5
    There's a Robotics section in Element14! Well I never knew that. I'll have to try and find it. I really liked the 3D mapping work you have done as it is something I have always wanted but never managed…
  • dougw
    dougw over 5 years ago +4
    Very interesting project. It looks like you are getting pretty good resolution as well. I will enjoy following your progress.
Parents
  • dubbie
    dubbie over 5 years ago

    There's a Robotics section in Element14! Well I never knew that. I'll have to try and find it. I really liked the 3D mapping work you have done as it is something I have always wanted but never managed, for my mobile robots. I am looking forward to your future Blogs in this area.

     

    Dubbie

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • yosoufe
    yosoufe over 5 years ago in reply to dubbie

    Yes. There is a robotics community here. Robotics

     

    It has not been active for a long time. So let's revive it image

     

    Thanks

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 5 years ago in reply to yosoufe

    Yousof,

     

    I'll have to dig out a robot (or two) and blog something into this area. Umm - what shall it be!

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • yosoufe
    yosoufe over 5 years ago in reply to dubbie

    I am looking forward to reading about your robots. image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • yosoufe
    yosoufe over 5 years ago in reply to dubbie

    I am looking forward to reading about your robots. image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dubbie
    dubbie over 5 years ago in reply to yosoufe

    Yousof,

     

    It might have to be the Marty robot I received recently (Unboxing A Box from E14 | element14 | Dubbie Dubbie) or maybe the latest version of the Worm robot (Crawling Worm Robot #3 : The 3D Printed Version | element14 | Dubbie Dubbie) which is sitting on my desk waiting to be tested. So many robots, so little time.

     

    Dubbie