Robotics
  • Technologies
  • More
Robotics
Blog ROS2 Learning Series - Blog 6 - Advanced Programming - Part 1
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: crisdeodates
  • Date Created: 13 Apr 2024 5:35 PM Date Created
  • Views 1489 views
  • Likes 3 likes
  • Comments 2 comments
  • Robot operating System
  • robotics
  • ROS2
  • ROS
Related
Recommended

ROS2 Learning Series - Blog 6 - Advanced Programming - Part 1

crisdeodates
crisdeodates
13 Apr 2024
ROS2 Learning Series - Blog 6 - Advanced Programming - Part 1

ROS2 Camera Stream Project

Previously we got some basic insight on how to program ROS2 nodes and services. Now let us take a step further in ROS2 programming. 

 

We will create a publisher node to capture a video stream from a camera and publish it to a topic.

We will also create a subscriber node who will subscribe to the camera stream topic and display it in an OpenCV window. 

Install the OpenCV dependencies.

$ pip install opencv-python 

 

Create a new ROS2 package with dependencies. 

$ cd ~/ros2_ws/src 
$ ros2 pkg create --build-type ament_python camera_stream --dependencies rclpy image_transport cv_bridge sensor_msgs std_msgs opencv-python
 

 

Create the camera_stream_publisher.py file and populate it with the following code: 

import rclpy 
from rclpy.node import Node 
from sensor_msgs.msg import Image 
from cv_bridge import CvBridge 
import cv2 
 
class CameraStreamPub(Node): 
   """ 
   Create a CameraStreamPub class, which is a subclass of the Node class. 
   """ 
   def __init__(self): 
       """ 
       Class constructor to set up the node. 
       """ 
       # Initiate the Node class's constructor and give it a name. 
       super().__init__('camera_stream_pub') 
       
       # Create the publisher. This publisher will publish an Image 
       # to the video_frame_data topic. The queue size is 10 messages. 
       self.publisher_ = self.create_publisher(Image, 'video_frame_data', 10) 
       
       # We will publish a message every 0.1 seconds. 
       timer_period = 0.1 # seconds 
       
       # Create the timer. 
       self.timer = self.create_timer(timer_period, self.timer_callback) 
           
       # Create a VideoCapture object. 
       # The argument '0' gets the default webcam. 
       self.cap = cv2.VideoCapture(0) 
           
       # Used to convert between ROS and OpenCV images. 
       self.br = CvBridge() 
       
   def timer_callback(self): 
       """ 
       Callback function. 
       This function gets called every 0.1 seconds. 
       """ 
       # Capture frame-by-frame. 
       # This method returns True/False as well 
       # as the video frame. 
       ret, frame = self.cap.read() 
 
       if ret == True: 
           # Publish the image. 
           # The 'cv2_to_imgmsg' method converts an OpenCV 
           # image to a ROS 2 image message. 
           self.publisher_.publish(self.br.cv2_to_imgmsg(frame)) 
   
def main(args=None): 
   """ 
   Main function to initialize the node and start the camera stream publisher. 
   """ 
   # Initialize the rclpy library. 
   rclpy.init(args=args) 
   
   # Create the node. 
   camera_stream_publisher_node = CameraStreamPub() 
   
   # Spin the node so the callback function is called. 
   rclpy.spin(camera_stream_publisher_node) 
   
   # Destroy the node explicitly. 
   camera_stream_publisher_node.destroy_node() 
   
   # Shutdown the ROS client library for Python. 
   rclpy.shutdown() 
 
if __name__ == '__main__': 
   main() 

 

Create the camera_stream_subscriber.py file and populate it with the following code: 

import rclpy 
from rclpy.node import Node 
from sensor_msgs.msg import Image 
from cv_bridge import CvBridge 
import cv2 
 
class CameraStreamSub(Node): 
   """ 
   Create a CameraStreamSub class, which is a subclass of the Node class. 
   """ 
   def __init__(self): 
       """ 
       Class constructor to set up the node. 
       """ 
       # Initiate the Node class's constructor and give it a name. 
       super().__init__('camera_stream_sub') 
       
       # Create the subscriber. This subscriber will receive an Image 
       # from the video_frames topic. The queue size is 10 messages. 
       self.subscription = self.create_subscription( 
           Image, 
           'video_frame_data', 
           self.listener_callback, 
           10) 
       self.subscription  # prevent unused variable warning 
       
       # Used to convert between ROS and OpenCV images. 
       self.br = CvBridge() 
       self.running = True 
   
   def listener_callback(self, data): 
       """ 
       Callback function to receive and display images. 
       """ 
       if self.running: 
           # Convert ROS Image message to OpenCV image. 
           current_frame = self.br.imgmsg_to_cv2(data) 
           
           # Display image. 
           cv2.imshow("camera_stream", current_frame) 
 
           # Raise SystemExit exception to quit if ESC key is pressed. 
           if cv2.waitKey(1) == 27: 
               self.running = False 
               cv2.destroyAllWindows() 
               raise SystemExit 
 
def main(args=None): 
   """ 
   Main function to initialize the node and start the camera stream subscriber. 
   """ 
   # Initialize the rclpy library. 
   rclpy.init(args=args) 
   
   # Create the node. 
   camera_stream_subscriber_node = CameraStreamSub() 
   
   # Spin the node so the callback function is called. 
   try: 
       rclpy.spin(camera_stream_subscriber_node) 
   # Exit if SystemExit exception is raised. 
   except SystemExit: 
       print("Camera stream output stopped") 
   
   # Destroy the node explicitly. 
   camera_stream_subscriber_node.destroy_node() 
   
   # Shutdown the ROS client library for Python. 
   rclpy.shutdown() 
 
if __name__ == '__main__': 
   main() 

 

Add the entry points to setup.py inside console_scripts section: 

'camera_stream_pub = camera_stream.camera_stream_publisher:main', 
'camera_stream_sub = camera_stream.camera_stream_subscriber:main', 

 

Since we already specified our dependencies during the package creation itself, we do not need to edit the package.xml file. 

 

Build the package. 

$ cd ~/ros2_ws 
$ colcon build --packages-select camera_stream
 

 

Source the new package. 

$ source install/setup.bash 

 

Run the camera stream publisher node to start publishing the camera frames. 

$ ros2 run camera_stream camera_stream_pub 

 

In another terminal, run the camera stream subscriber node. 

$ cd ~/ros2_ws 
$ source install/setup.bash

$ ros2 run camera_stream camera_stream_sub 

 

The camera frames will be displayed in an OpenCV window. 

image

 

You can press ESC on the active OpenCV window to exit. 

  • Sign in to reply
  • crisdeodates
    crisdeodates over 2 years ago in reply to DAB

    Yes. As long as the camera_stream_publisher node runs in the first terminal, it will continue to capture the camera images.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 2 years ago

    I assume you can continue to capture camera frames and store them in the background even when the display window is closed.