Robotics
  • Technologies
  • More
Robotics
Blog Simulating a Robot XMP-2
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 21 Nov 2015 7:22 AM Date Created
  • Views 2136 views
  • Likes 2 likes
  • Comments 11 comments
  • xmos_startkit
  • xmp-2
  • simulation
  • robotics
  • raspberry_pi2
  • rpi2
  • xmp
  • gazebo
  • rpi
  • xmos
Related
Recommended

Simulating a Robot XMP-2

shabaz
shabaz
21 Nov 2015

image

Introduction

XMP-2 is a small mobile platform intended for robotics experiments. It is constructed from aluminium and uses a few methods described earlier for high accuracy on smooth surfaces.

Check out the coin test in this video: XMP-2 Practice Run

 

It is not always possible to build hardware at the same time as the software, and much time can be saved if software developers can use a simulated robot instead of real hardware.

A free simulation package called Gazebo was previously briefly investigated and it allows a 3D robot model to be created and then physics based interactions can occur.

Now it was time to attempt to simulate XMP-2 and see how the simulation could be controlled as if it were real hardware.

image

 

 

Building XMP-2 (Virtually)

Gazebo has a graphical model editor but it was actually easier to just type the description of they physical XMP-2 into a text file. You just need to be handy with a calculator so that you can calculate centres of the primitive blocks/elements you have available to construct the model.

I started with the square shaped aluminium frame. The real XMP-2 frame measures 140x140mm so I punched in exactly these values into the model.

Next I needed to model the castors. There are two on XMP-2. They were constructed from a cylinder and a sphere for the ball bearing.

For the wheels I used the cylinder primitive shape again. Since I had datasheets for all parts, it was very easy to look up dimensions so that the virtual XMP-2 would be identical in size. If you're building any robot it is a good idea to keep drawings with dimensions on them:

image

In order for Gazebo to understand which axis the wheels rotate about, a further two elements are needed, one per wheel. I didn’t quite understand them in detail, but they appear to work. You will see them in the final model file pasted further below.

image

 

Note that for all of the elements described, their position is represented as the co-ordinate at the centre of the primitive.

Once the model file is complete, it can be given a visual inspection using Gazebo as shown in the graphic rendering above - it looks close enough to the actual XMP-2:

image

 

Here is the complete text based model of XMP-2. If you are building your own virtual robot then it could be used as a guide to see how to construct it:

 

<?xml version='1.00'?>
<sdf version='1.4'>
  <model name="XMP-2">
    <static>false</static>
    <link name='chassis'>
      <pose>0 0 .0275 0 0 0</pose>
      <!-- ****** Box ****** -->
      <collision name='collision'>
        <geometry>
          <box>
            <size>.14 .14 .015</size>
          </box>
        </geometry>
      </collision>
    
      <visual name='visual'>
        <geometry>
          <box>
            <size>.14 .14 .015</size>
          </box>
        </geometry>
      </visual>


      <collision name='casterbase_collision1'>
        <pose>-0.0625 0 -0.01575 0 0 0</pose>
        <geometry>
          <cylinder>
            <radius>0.01</radius>
            <length>0.0165</length>
          </cylinder>
        </geometry>
      </collision>
    
      <visual name='casterbase_visual1'>
        <pose>-0.0625 0 -0.01575 0 0 0</pose>
        <geometry>
          <cylinder>
            <radius>0.01</radius>
            <length>0.0165</length>
          </cylinder>
        </geometry>
      </visual>


      <collision name='casterbase_collision2'>
        <pose>0.0625 0 -0.01575 0 0 0</pose>
        <geometry>
          <cylinder>
            <radius>0.01</radius>
            <length>0.0165</length>
          </cylinder>
        </geometry>
      </collision>
    
      <visual name='casterbase_visual2'>
        <pose>0.0625 0 -0.01575 0 0 0</pose>
        <geometry>
          <cylinder>
            <radius>0.01</radius>
            <length>0.0165</length>
          </cylinder>
        </geometry>
      </visual>
    
    
    
      <!-- ****** Caster ****** -->
      <collision name='caster_collision1'>
        <pose>-0.0625 0 -0.024325 0 0 0</pose>
        <geometry>
            <sphere>
            <radius>0.00635</radius>
          </sphere>
        </geometry>
    
        <surface>
          <friction>
            <ode>
              <mu>0</mu>
              <mu2>0</mu2>
              <slip1>1.0</slip1>
              <slip2>1.0</slip2>
            </ode>
          </friction>
        </surface>
      </collision>
    
      <visual name='caster_visual1'>
        <pose>-0.0625 0 -0.024325 0 0 0</pose>
        <geometry>
          <sphere>
            <radius>0.00635</radius>
          </sphere>
        </geometry>
      </visual>
      <collision name='caster_collision2'>
        <pose>0.0625 0 -0.024325 0 0 0</pose>
        <geometry>
            <sphere>
            <radius>0.00635</radius>
          </sphere>
        </geometry>
    
        <surface>
          <friction>
            <ode>
              <mu>0</mu>
              <mu2>0</mu2>
              <slip1>1.0</slip1>
              <slip2>1.0</slip2>
            </ode>
          </friction>
        </surface>
      </collision>
    
      <visual name='caster_visual2'>
        <pose>0.0625 0 -0.024325 0 0 0</pose>
        <geometry>
          <sphere>
            <radius>0.00635</radius>
          </sphere>
        </geometry>
      </visual>
    </link>


    <!-- ****** Wheels ****** -->
    <link name="left_wheel">
      <pose>0 0.075 0.0275 0 1.5707 1.5707</pose>
      <collision name="collision">
        <geometry>
          <cylinder>
            <radius>0.0275</radius>
            <length>0.008</length>
          </cylinder>
        </geometry>
      </collision>
      <visual name="visual">
        <geometry>
          <cylinder>
            <radius>0.0275</radius>
            <length>0.008</length>
          </cylinder>
        </geometry>
      </visual>
    </link>
    <link name="right_wheel">
      <pose>0 -0.075 0.0275 0 1.5707 1.5707</pose>
      <collision name="collision">
        <geometry>
          <cylinder>
            <radius>0.0275</radius>
            <length>0.008</length>
          </cylinder>
        </geometry>
      </collision>
      <visual name="visual">
        <geometry>
          <cylinder>
            <radius>0.0275</radius>
            <length>0.008</length>
          </cylinder>
        </geometry>
      </visual>
    </link>
  
    <!-- ****** Hinge Joints for Wheels ****** -->
    <joint type="revolute" name="left_wheel_hinge">
        <pose>0 0 -0.03 0 0 0</pose>
        <child>left_wheel</child>
        <parent>chassis</parent>
        <axis>
          <xyz>0 1 0</xyz>
        </axis>
      </joint>
      <joint type="revolute" name="right_wheel_hinge">
        <pose>0 0 0.03 0 0 0</pose>
        <child>right_wheel</child>
        <parent>chassis</parent>
        <axis>
          <xyz>0 1 0</xyz>
        </axis>
      </joint>
    
      <plugin name="model-plugin" filename="build/libmodel-plugin.so"/>
  </model>
</sdf>
 

 

To use the model, create a folder in ~/.gazebo/models called xmp-2 and save the content in a file there (i.e. in ~/.gazebo/models/xmp-2) called model.sdf

 

Next create a configuration file in the same folder called model.config containing this:

 

<?xml version="1.0"?>
<model>
  <name>XMP-2</name>
  <version>1.0</version>
  <sdf version='1.4'>model.sdf</sdf>

  <author>
   <name>shabaz</name>
   <email>shabaz</email>
  </author>

  <description>
    XMP-2 XMOS Mobile Platform 2
  </description>
</model>
 

 

You should now be able to run Gazebo (as described in the earlier blog post) and view XMP-2 and exert force on it in any direction using the graphical user interface. Once you have added XMP-2 to the world view, select 'Save As' from the Gazebo menu and save the XMP-2 robot inside the world view as a file called xmp-2-world.world

The file can be saved in a custom folder off your home folder. For example, call the new folder gazebo_work

If you view the file in an editor, it will look something like this (or just use this version if you prefer):

 

<sdf version='1.5'>
  <world name='default'>
    <light name='sun' type='directional'>
      <cast_shadows>1</cast_shadows>
      <pose>0 0 10 0 -0 0</pose>
      <diffuse>0.8 0.8 0.8 1</diffuse>
      <specular>0.2 0.2 0.2 1</specular>
      <attenuation>
        <range>1000</range>
        <constant>0.9</constant>
        <linear>0.01</linear>
        <quadratic>0.001</quadratic>
      </attenuation>
      <direction>-0.5 0.1 -0.9</direction>
    </light>
    <model name='ground_plane'>
      <static>1</static>
      <link name='link'>
        <collision name='collision'>
          <geometry>
            <plane>
              <normal>0 0 1</normal>
              <size>100 100</size>
            </plane>
          </geometry>
          <surface>
            <friction>
              <ode>
                <mu>100</mu>
                <mu2>50</mu2>
              </ode>
            </friction>
            <contact>
              <ode/>
            </contact>
            <bounce/>
          </surface>
          <max_contacts>10</max_contacts>
        </collision>
        <visual name='visual'>
          <cast_shadows>0</cast_shadows>
          <geometry>
            <plane>
              <normal>0 0 1</normal>
              <size>100 100</size>
            </plane>
          </geometry>
          <material>
            <script>
              <uri>file://media/materials/scripts/gazebo.material</uri>
              <name>Gazebo/Grey</name>
            </script>
          </material>
        </visual>
        <self_collide>0</self_collide>
        <kinematic>0</kinematic>
        <gravity>1</gravity>
      </link>
    </model>
    <physics name='default_physics' default='0' type='ode'>
      <max_step_size>0.001</max_step_size>
      <real_time_factor>1</real_time_factor>
      <real_time_update_rate>1000</real_time_update_rate>
      <gravity>0 0 -9.8</gravity>
      <magnetic_field>6e-06 2.3e-05 -4.2e-05</magnetic_field>
    </physics>
    <scene>
      <ambient>0.4 0.4 0.4 1</ambient>
      <background>0.7 0.7 0.7 1</background>
      <shadows>1</shadows>
    </scene>
    <spherical_coordinates>
      <surface_model>EARTH_WGS84</surface_model>
      <latitude_deg>0</latitude_deg>
      <longitude_deg>0</longitude_deg>
      <elevation>0</elevation>
      <heading_deg>0</heading_deg>
    </spherical_coordinates>
    <model name='XMP-2_0'>
      <static>0</static>
      <link name='chassis'>
        <pose>0 0 0.0275 0 -0 0</pose>
        <collision name='collision'>
          <geometry>
            <box>
              <size>0.14 0.14 0.015</size>
            </box>
          </geometry>
          <max_contacts>10</max_contacts>
          <surface>
            <contact>
              <ode/>
            </contact>
            <bounce/>
            <friction>
              <ode/>
            </friction>
          </surface>
        </collision>
        <visual name='visual'>
          <geometry>
            <box>
              <size>0.14 0.14 0.015</size>
            </box>
          </geometry>
        </visual>
        <collision name='casterbase_collision1'>
          <pose>-0.0625 0 -0.01575 0 -0 0</pose>
          <geometry>
            <cylinder>
              <radius>0.01</radius>
              <length>0.0165</length>
            </cylinder>
          </geometry>
          <max_contacts>10</max_contacts>
          <surface>
            <contact>
              <ode/>
            </contact>
            <bounce/>
            <friction>
              <ode/>
            </friction>
          </surface>
        </collision>
        <visual name='casterbase_visual1'>
          <pose>-0.0625 0 -0.01575 0 -0 0</pose>
          <geometry>
            <cylinder>
              <radius>0.01</radius>
              <length>0.0165</length>
            </cylinder>
          </geometry>
        </visual>
        <collision name='casterbase_collision2'>
          <pose>0.0625 0 -0.01575 0 -0 0</pose>
          <geometry>
            <cylinder>
              <radius>0.01</radius>
              <length>0.0165</length>
            </cylinder>
          </geometry>
          <max_contacts>10</max_contacts>
          <surface>
            <contact>
              <ode/>
            </contact>
            <bounce/>
            <friction>
              <ode/>
            </friction>
          </surface>
        </collision>
        <visual name='casterbase_visual2'>
          <pose>0.0625 0 -0.01575 0 -0 0</pose>
          <geometry>
            <cylinder>
              <radius>0.01</radius>
              <length>0.0165</length>
            </cylinder>
          </geometry>
        </visual>
        <collision name='caster_collision1'>
          <pose>-0.0625 0 -0.024325 0 -0 0</pose>
          <geometry>
            <sphere>
              <radius>0.00635</radius>
            </sphere>
          </geometry>
          <surface>
            <friction>
              <ode>
                <mu>0</mu>
                <mu2>0</mu2>
                <slip1>1</slip1>
                <slip2>1</slip2>
              </ode>
            </friction>
            <contact>
              <ode/>
            </contact>
            <bounce/>
          </surface>
          <max_contacts>10</max_contacts>
        </collision>
        <visual name='caster_visual1'>
          <pose>-0.0625 0 -0.024325 0 -0 0</pose>
          <geometry>
            <sphere>
              <radius>0.00635</radius>
            </sphere>
          </geometry>
        </visual>
        <collision name='caster_collision2'>
          <pose>0.0625 0 -0.024325 0 -0 0</pose>
          <geometry>
            <sphere>
              <radius>0.00635</radius>
            </sphere>
          </geometry>
          <surface>
            <friction>
              <ode>
                <mu>0</mu>
                <mu2>0</mu2>
                <slip1>1</slip1>
                <slip2>1</slip2>
              </ode>
            </friction>
            <contact>
              <ode/>
            </contact>
            <bounce/>
          </surface>
          <max_contacts>10</max_contacts>
        </collision>
        <visual name='caster_visual2'>
          <pose>0.0625 0 -0.024325 0 -0 0</pose>
          <geometry>
            <sphere>
              <radius>0.00635</radius>
            </sphere>
          </geometry>
        </visual>
        <self_collide>0</self_collide>
        <inertial>
          <inertia>
            <ixx>1</ixx>
            <ixy>0</ixy>
            <ixz>0</ixz>
            <iyy>1</iyy>
            <iyz>0</iyz>
            <izz>1</izz>
          </inertia>
          <mass>1</mass>
        </inertial>
        <kinematic>0</kinematic>
        <gravity>1</gravity>
      </link>
      <link name='left_wheel'>
        <pose>0 0.075 0.0275 -0 1.5707 1.5707</pose>
        <collision name='collision'>
          <geometry>
            <cylinder>
              <radius>0.0275</radius>
              <length>0.008</length>
            </cylinder>
          </geometry>
          <max_contacts>10</max_contacts>
          <surface>
            <contact>
              <ode/>
            </contact>
            <bounce/>
            <friction>
              <ode/>
            </friction>
          </surface>
        </collision>
        <visual name='visual'>
          <geometry>
            <cylinder>
              <radius>0.0275</radius>
              <length>0.008</length>
            </cylinder>
          </geometry>
        </visual>
        <self_collide>0</self_collide>
        <inertial>
          <inertia>
            <ixx>1</ixx>
            <ixy>0</ixy>
            <ixz>0</ixz>
            <iyy>1</iyy>
            <iyz>0</iyz>
            <izz>1</izz>
          </inertia>
          <mass>1</mass>
        </inertial>
        <kinematic>0</kinematic>
        <gravity>1</gravity>
      </link>
      <link name='right_wheel'>
        <pose>0 -0.075 0.0275 -0 1.5707 1.5707</pose>
        <collision name='collision'>
          <geometry>
            <cylinder>
              <radius>0.0275</radius>
              <length>0.008</length>
            </cylinder>
          </geometry>
          <max_contacts>10</max_contacts>
          <surface>
            <contact>
              <ode/>
            </contact>
            <bounce/>
            <friction>
              <ode/>
            </friction>
          </surface>
        </collision>
        <visual name='visual'>
          <geometry>
            <cylinder>
              <radius>0.0275</radius>
              <length>0.008</length>
            </cylinder>
          </geometry>
        </visual>
        <self_collide>0</self_collide>
        <inertial>
          <inertia>
            <ixx>1</ixx>
            <ixy>0</ixy>
            <ixz>0</ixz>
            <iyy>1</iyy>
            <iyz>0</iyz>
            <izz>1</izz>
          </inertia>
          <mass>1</mass>
        </inertial>
        <kinematic>0</kinematic>
        <gravity>1</gravity>
      </link>
      <joint name='left_wheel_hinge' type='revolute'>
        <pose>0 0 -0.03 0 -0 0</pose>
        <child>left_wheel</child>
        <parent>chassis</parent>
        <axis>
          <xyz>0 1 0</xyz>
          <use_parent_model_frame>1</use_parent_model_frame>
          <limit>
            <lower>-1e+16</lower>
            <upper>1e+16</upper>
          </limit>
          <dynamics>
            <spring_reference>0</spring_reference>
            <spring_stiffness>0</spring_stiffness>
          </dynamics>
        </axis>
      </joint>
      <joint name='right_wheel_hinge' type='revolute'>
        <pose>0 0 0.03 0 -0 0</pose>
        <child>right_wheel</child>
        <parent>chassis</parent>
        <axis>
          <xyz>0 1 0</xyz>
          <use_parent_model_frame>1</use_parent_model_frame>
          <limit>
            <lower>-1e+16</lower>
            <upper>1e+16</upper>
          </limit>
          <dynamics>
            <spring_reference>0</spring_reference>
            <spring_stiffness>0</spring_stiffness>
          </dynamics>
        </axis>
      </joint>
      <plugin name='model-plugin' filename='build/libmodel-plugin.so'/>
      <pose>1 0.403425 0 0 -0 0</pose>
    </model>
    <state world_name='default'>
      <sim_time>159 732000000</sim_time>
      <real_time>161 509335075</real_time>
      <wall_time>1448069945 796721688</wall_time>
      <iterations>159732</iterations>
      <model name='XMP-2_0'>
        <pose>1.00016 0.400351 0.003177 -0.034765 -3e-06 -1e-05</pose>
        <link name='chassis'>
          <pose>1.00016 0.401307 0.030661 -0.034765 -3e-06 -1e-05</pose>
          <velocity>4.1e-05 -0.000304 -0.000415 -0.000522 0.006631 -0.000157</velocity>
          <acceleration>-0 -0 -0.11343 3.13345 1.32683 3.09945</acceleration>
          <wrench>-0 -0 -0.11343 0 -0 0</wrench>
        </link>
        <link name='left_wheel'>
          <pose>1.00016 0.476261 0.028054 2.25893 1.51619 -2.4543</pose>
          <velocity>3.5e-05 -0.000305 -0.000454 -0.000522 0.001552 2e-05</velocity>
          <acceleration>-0.001578 -2.1e-05 -0.114036 -0.00816 0.000758 0.02095</acceleration>
          <wrench>-0.001578 -2.1e-05 -0.114036 0 -0 0</wrench>
        </link>
        <link name='right_wheel'>
          <pose>1.00016 0.326352 0.033267 -2.26498 1.5166 -0.693561</pose>
          <velocity>4.6e-05 -0.000302 -0.000376 -0.000522 -0.001516 0.000127</velocity>
          <acceleration>0.001578 2.1e-05 -0.112823 -0.008159 0.000702 0.020954</acceleration>
          <wrench>0.001578 2.1e-05 -0.112823 0 -0 0</wrench>
        </link>
      </model>
      <model name='ground_plane'>
        <pose>0 0 0 0 -0 0</pose>
        <link name='link'>
          <pose>0 0 0 0 -0 0</pose>
          <velocity>0 0 0 0 -0 0</velocity>
          <acceleration>0 0 0 0 -0 0</acceleration>
          <wrench>0 0 0 0 -0 0</wrench>
        </link>
      </model>
    </state>
    <gui fullscreen='0'>
      <camera name='user_camera'>
        <pose>2.07864 -0.370742 0.357459 0 0.275643 2.35619</pose>
        <view_controller>orbit</view_controller>
        <projection_type>perspective</projection_type>
      </camera>
    </gui>
  </world>
</sdf>
 

 

As you can see, the world view file has embedded the XMP-2 model in it entirely. The next step is to develop some software to control the model inside this world view.

 

Creating a Software Plugin for Controlling the Model

A software plugin in the form of a shared library was created in order to pass instructions into Gazebo about how and where the model is to move.

 

Firstly, a makefile was created in the same gazebo_work folder created earlier. The file is called CMakeLists.txt and needs to contain the following content:

 

cmake_minimum_required(VERSION 2.8 FATAL_ERROR)

find_package(gazebo REQUIRED)
include_directories(${GAZEBO_INCLUDE_DIRS})
link_directories(${GAZEBO_LIBRARY_DIRS})
list(APPEND CMAKE_CXX_FLAGS "${GAZEBO_CXX_FLAGS}")

add_library(model-plugin SHARED model-plugin.cc)
target_link_libraries(model-plugin ${GAZEBO_LIBRARIES})

set(CMAKE_CXX_FLAGS "${CMAKE_CXX_FLAGS} ${GAZEBO_CXX_FLAGS}")
 

 

The code for the plugin is written in C++ and is shown below. There is a tutorial which covers this in detail. I modified the existing tutorial code such that the code can receive stimulus externally. The code was saved in a file called model-plugin.cc at the same location as the makefile:

 

#include <boost/bind.hpp>
#include <gazebo/gazebo.hh>
#include <gazebo/physics/physics.hh>
#include <gazebo/common/common.hh>
#include <stdio.h>
#include <iostream>
#include <fstream>
#include <string>

using namespace std;

namespace gazebo
{
  class ModelPush : public ModelPlugin
  {
    public: void Load(physics::ModelPtr _parent, sdf::ElementPtr /*_sdf*/)
    {
      // Store the pointer to the model
      this->model = _parent;


      // Listen to the update event. This event is broadcast every
      // simulation iteration.
      this->updateConnection = event::Events::ConnectWorldUpdateBegin(
          boost::bind(&ModelPush::OnUpdate, this, _1));
    }


    // Called by the world update start event
    public: void OnUpdate(const common::UpdateInfo & /*_info*/)
    {
      ifstream fp;
      string line;
      int cmd=0;
      fp.open("command.txt");
      if (fp.is_open())
      {
        while(getline(fp, line))
        {
          if (line.find("move") != string::npos)
          {
            cmd=1;
          }
        }
        fp.close();
      }
      if (cmd==1)
      {
        // Apply a small linear velocity to the model.
        this->model->SetLinearVel(math::Vector3(.03, 0, 0));
      }
    }


    // Pointer to the model
    private: physics::ModelPtr model;


    // Pointer to the update event connection
    private: event::ConnectionPtr updateConnection;
  };


  // Register this plugin with the simulator
  GZ_REGISTER_MODEL_PLUGIN(ModelPush)
}
 

 

Now create a build folder in the same location (so the path is now ~/gazebo_work/build )

and go inside the build folder and type the following (Note: You may need to install cmake if your Linux distribution does not alreagy have this, e.g. type as root user apt-get install cmake ):

 

cmake ../
make
 

 

After a while the build process will have resulted in a file called libmodel-plugin.so

Just as an fyi, the file name matches a name which was originally typed in the model.sdl file too, and it became part of the xmp-2-world.world file too. If you examine those files you'll see it in a line looking like this:

<plugin name="model-plugin" filename="build/libmodel-plugin.so"/>
 

 

The C++ code (model-plugin.cc) shown above contains some modifications I made to allow for communications.

There are many ways of doing this, so one can use their own ideas/initiative. For now I chose a very simple file based method. A socket interface would be a good method too.

My simple method merely checks for the presence of a file called command.txt and executes whatever command is written in that file. It is possible to modify the file contents on-the-fly using either manual typing or under the control of some other program. You can see on line 40 that it checks for the text 'move'. It could be expanded greatly.

 

Why is this useful? Well the other program could be taking input from a serial interface or USB device! The serial interface could be from (say) a Raspberry Pi. This means it is possible to develop robot software to run on the single board computer (SBC) of your choice, and simulate the robot on the PC in order to test the software. The software on the SBC would have no idea if it were a real robot or a simulated robot connected to the serial port.

If you wanted to sell robots then it could potentially allow people to program and try out the simulated robot, and purchase the real thing if they were satisfied it met their need. In other words the simulation would become a sales tool.

Or if you only had one robot but wanted to see how a whole army of them would behave then you could just instantiate multiple copies of the model and multiple copies of the robot software.

 

Running The Virtual Robot

Close down Gazebo if it is currently running, and then in a terminal type the following to start the simulation in paused mode:

gzserver --verbose -u xmp-2-world.world
 

 

In another terminal window bring up the graphical user interface (GUI) by typing the following:

gzclient
 

 

Now click the 'Play' button at the bottom of the GUI in order to run the simulation!

Nothing will happen, because the code is waiting for a command to appear in the command.txt file mentioned earlier, as designed.

 

So, in a third terminal window or using an editor of your choice, create a command.txt file in ~/gazebo_work and type the word

'move' in it and save the file. As soon as the file is saved the virtual robot will begin moving! To stop it, delete the line and save the file again. This of course is just a simple demo so scale it as desired with more functionality.

 

The video here shows the simulation being run:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

To quit out, exit the GUI from the menu and then type Ctrl-C on the terminal running the simulation. It will take 15 seconds or so to quit.

 

Summary

It turns out to be fairly easy to construct a model and then drive it using external control in a virtual world. There could be many uses for this. This has been just a brief post and some more understanding is needed to more accurately simulate the physics of the real robot in the virtual world.

Although the code here uses a text file to control the virtual robot, it would be extremely easy to extend the control over serial or USB. This allows real world sensors and external single board computers to provide data and intelligence to control the virtual robot.

  • Sign in to reply

Top Comments

  • DAB
    DAB over 10 years ago in reply to mcb1 +3
    Hi Mark, The programs that I worked on took many years to develop the prototypes. Using the design specifications, I wrote my simulations to examine how the programs and data would propagate through the…
  • DAB
    DAB over 10 years ago +2
    Great post. You are very correct. Every large project I worked on we simulated hardware and software throughout the development stages to mitigate interface issues as we went. I used to model computer…
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to mcb1 +2
    Hello Mark, in a general vision, as just shabaz point, if the simulation does not define all the parameters it is not reliable in terms of physics. But - I suppose you know this - different types of simulation…
Parents
  • DAB
    DAB over 10 years ago

    Great post.

     

    You are very correct.  Every large project I worked on we simulated hardware and software throughout the development stages to mitigate interface issues as we went.

     

    I used to model computer architectures to make sure that the processors and networks could support the operational software.  I was able to find and correct many hardware and software issues before they became very expensive to correct.

     

    I urge everyone to learn how to use simulations for their projects.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 10 years ago

    Great post.

     

    You are very correct.  Every large project I worked on we simulated hardware and software throughout the development stages to mitigate interface issues as we went.

     

    I used to model computer architectures to make sure that the processors and networks could support the operational software.  I was able to find and correct many hardware and software issues before they became very expensive to correct.

     

    I urge everyone to learn how to use simulations for their projects.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mcb1
    mcb1 over 10 years ago in reply to DAB

    I think simulation has its place, and I'm not putting down Shabaz's work here, but I'm not sure I fully understand what this achieves.

     

    It certainly takes the physical aspect and simulates it, but unless I'm mistaken the weight change, friction of the wheels, motor performance and battery capacity aren't part of the model as shabaz noted with this comment.

    more understanding is needed to more accurately simulate the physics of the real robot in the virtual world

     

    If these aren't accurately plugged into the model, wouldn't the simulation also be faulty.?

    How do you know your figures used in a simulation are real?

     

     

    I get the concept of modelling when you are trying to fit parts together, and design items before actually building them to ensure the behave as expected.

    It's certainly something that has long been done in Automotive design or customising, even before computers were used.

     

     

    http://www.element14.com/community/people/DAB made this comment

    I used to model computer architectures to make sure that the processors and networks could support the operational software.  I was able to find and correct many hardware and software issues before they became very expensive to correct.

    I would be interested in how you did this to better understand the advantage of simulation.

     

    Great work

    Thanks

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to mcb1

    Hello Mark,

     

    in a general vision, as just shabaz point, if the simulation does not define all the parameters it is not reliable in terms of physics. But - I suppose you know this - different types of simulation, you can simulate a certain thing or event partially or completely depending on your needs. For example, in the environment of computer, just when you make a test on what is a certain current consumption while the processor is stressed with a certain operation (i.e. a long loop) you make a simulation specifically oriented to test this parameter. This does not means that the test loop is exactly the loop you provide in you program but the collected information for this specific aspect are extremely useful and correct.

    The same occurs in the case of robotics; It is almost rare that you need to simulate the entire physical system if you are not making a 3D toon: in the very simple case for example ot a motor moving a slider, you can set the motor parameters (physical ones like torque, acceleration, power, frequency etc.) and see if applying a certain weight on the connected belt the motor has the credentials to move it or not.

     

    Not only but in robotics it is not rare that a global full-defined simulations is less useful than separate simulations just to control the isolated parameters influence on the entire system. Only at the end then a global simulation can also introduce the different concurring parameters relationship to the final result.

     

    The ability to create a "world" that reflect only some but perfectly the characteristics of the reality and isolate some parameters, changing them and trying again etc. is the real power of the simulation.

     

    For example I can see that the initial conditions are not reliable to move the heavy weight I need. But I can try incresing the torque, then changing the frequency, modifying the pulleys and so on. And see what happens, then decide what is the parameter that definitely I consider convenient for my needs.

     

    Years ago with the Archaeological Dpt. of the University of Turin, we have mapped and recreated and entire structure of the ancient Pompey before the volcano eruption. Then we have tested on the Catia software (Cad and math and simulation and a lot) what happened to the architectural structures under certain forces like the earthquake etc. This was useful to know with a very good approximation the power and the behaviour of the volcano eruption (that was the "x" incognita). This was a partial simulation but very reliable for the specific yet complex series of target results we was searching for.

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 10 years ago in reply to mcb1

    Hi Mark,

     

    The programs that I worked on took many years to develop the prototypes.  Using the design specifications, I wrote my simulations to examine how the programs and data would propagate through the system architecture.

    What I did was relatively new at the time, mid 1980's.  Today, simulation based development is more the norm than rarity.

    Simulations proved that they were a very inexpensive way to verify designs and computer architectures/communication and data control.

    The key benefit is that you can play a lot of what if games to see how the proposed design will react to different operational scenarios.

     

    As the devices became real, both as prototypes and then as final hardware, the simulations were used to test them and verify capability by inserting the hardware into the simulation driven test environment.

    We could explore very risky operations to see if the hardware would continue to work without risking the hardware or indeed an entire system.

    We also could verify the safety features of the system and look at progressive effects of unit failures of components.

     

    Using simulation also enables you to look at system upgrades long before you commit development and integration costs.

    We proved that you could save a significant amount of money by analysis rather than building and testing prototypes.

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to DAB

    Hi DAB,

     

    What I did was relatively new at the time, mid 1980's.  Today, simulation based development is more the norm than rarity.

     

    Just in that period I was mostly in the market of the first hardware custom boards for 386 PCs. I remember that there was already processors like Z80 and 6502, anyway the biggest players together with the first CPU of Intel was Zylog and Motorola and few other. I remember that HP produced a big and very expensive processor simulator just to see what hardware was responding with certain machine cycles instead of others with one or another processor. Unfortunately I don't remember the name of this modular and very customisable machine I worked with for a couple of years.

     

    Jumping to the future (now) to complete the scenario we should take in account that simulation plays a key role in the development lifecycle of the mobile devices (smartphones and tablets). In this area there are two  kind of simulation. The first is simulating only a part of the application: I mean the application architecture and design, the user interface design and the basic logic. All the processed information instead are fake data. This is very frequently used by the UI designers in the application project phase to show to the client and the developer what should be the final product without writing a line of code. The second is the possibility to simulate the application behaviour - also remotely - on all the devices that the application should provide compatibility without the need for the developer(s) the real availability of them.

     

    When I was working for Nokia special clients we have used intensibely both methods with excellent results.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to mcb1

    Hi Mark!

     

    I would need to add a bit more numbers into it before it became useful. The work in this blog post was really to figure out how to get communications between the simulation application and custom software. Once that mechanism is available then there are ways to model both inside the simulation app and inside the custom code. The simulation app can handle (to some degree) modeling of friction, mass, centre of mass, inertial, etc., so in theory a lot of that

    can be plugged in if the numbers for the desired real hardware are available.

    Where I might want to model (say) battery life would be in the custom code. Basically the custom code would have to act as a wrapper that pretends to be the

    H-bridge, any power supply monitor, etc., so your main robot code (say running on an SBC) could still believe it is talking to real hardware - or alternatively put '#ifdef SIMULATION' into the code running on the SBC.

     

    You are completely right that simulatting XMP-2 is kind-of worthless in the state that the model exists - I only used it because I wanted to see what Gazebo could be used for, so just inserted it in as a learning exercise.


    I think it would make a very good learning tool - I've noticed there are some extremely complicated commercial robot hardware simulations included, so users can

    start programming behaviour (by connecting it to their own software) and see it run in the virtual world. Some of these (even quite basic) educational robots are very expensive - the Willow Garage PR2 is apparently several hundred thousand $$ : ( but has a simulation so it's probably about as close to one as I will get : (

    And probably makes a good sales tool for computer/electronically controlled or monitored mechanics based products, to allow people to run it and see the programmed and physical behaviour combined before they buy for real.