Robotics
  • Technologies
  • More
Robotics
Forum Hi there,can we can just discuss about low cost solutions for generating 4-20 ma current?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 79 subscribers
  • Views 1721 views
  • Users 0 members are here
  • transducers
  • 4-20
  • plc_control
Related

Hi there,can we can just discuss about low cost solutions for generating 4-20 ma current?

coolbox
coolbox over 11 years ago

Hi there,

 

4-20 ma is standard for data acquisition from sensors in industrial environment.There are are many techniques like PWM and DAC for 4-20 ma current generation.But still i want to hear from automation experts for options about generating 4-20 ma.Is any micro controller which can directly output 4-20ma?

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to johnbeetem +1
    The nice thing is it can detect outages as 0 reading is not 0 current, it is 4mA (Just enough to drive the remote sensor and nowadays a micro, ADC, DAC etc) and as it is a current system, can tolerate…
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago

    Directly, probably not but all it takes is the inclusion of a 110R resistor per channel giving a 0.4 – 2.2V range or a 220R to give 0.8 – 4.4V

     

    Depending on the ADC on the micro, this would work just fine (110R for the 3V3 micros and 220R for the 5V micros), this changes if you apply a real VREF but that’s easy math to figure out the required R value to match

     

     

     

    Hope this Helps

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago

    Directly, probably not but all it takes is the inclusion of a 110R resistor per channel giving a 0.4 – 2.2V range or a 220R to give 0.8 – 4.4V

     

    Depending on the ADC on the micro, this would work just fine (110R for the 3V3 micros and 220R for the 5V micros), this changes if you apply a real VREF but that’s easy math to figure out the required R value to match

     

     

     

    Hope this Helps

     

    Peter