Robotics
  • Technologies
  • More
Robotics
Forum Open Collector Output interface to 24V Digital Input, Inverted
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 78 subscribers
  • Views 4786 views
  • Users 0 members are here
  • logic
  • plc
  • signal
Related

Open Collector Output interface to 24V Digital Input, Inverted

tjslip
tjslip over 11 years ago

I have a stepper motor (multi-axis' in fact) that provides a limit signal (E11 NEGATIVE LIMIT) that is open collector output:

image

I need to connect that signal to an opto-isolated 24V digital input (no internal pull-up resistor I assume):

image

 

Currently there is a circuit board installed that does this, and that contains:

  • A regulator IC for 5V
  • A pullup resistor circuit to 5V.
  • An IC (ULN2003 Darlington Array) to up the voltage to 24V and
  • An IC (Philips  74HC14N74HC14N HEX INVERTING SCHMITT TRIGGER to invert the signal (to active high instead of active low I assume)

 

I want to eliminate this custom made circuit board and use "industrial-strength" off-the-shelf DIN rail mounted items to interface the motor limit output with the digital input.

 

I'm a mechanical engineer and am kindly requesting some advice how to do this professionally, without custom circuitry.

 

Thanks in advance.

Tom.

  • Sign in to reply
  • Cancel
Parents
  • dougw
    0 dougw over 11 years ago

    You could connect a Phoenix Contact 2900353 to the E11 signal, but that signal needs a 390 ohm resistor between it and 5V.

    The polarity can be reversed simply by connecting the module slightly differently.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 11 years ago

    You could connect a Phoenix Contact 2900353 to the E11 signal, but that signal needs a 390 ohm resistor between it and 5V.

    The polarity can be reversed simply by connecting the module slightly differently.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer