Robotics
  • Technologies
  • More
Robotics
Forum Convert Existing Automatic Sliding Door to Operate with RPI
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 7 answers
  • Subscribers 78 subscribers
  • Views 2297 views
  • Users 0 members are here
Related

Convert Existing Automatic Sliding Door to Operate with RPI

e14 Contributor
e14 Contributor over 10 years ago

Hi All

 

I would like to start a step by step project but need some advice first.

 

I have 2 x PC boards on separate automatic sliding doors that blew due to a power surge. Each of the boards plug into a 220volt dedicated wall plug. To replace these boards are very expensive. I want to operate the doors using Raspberry PI instead as its much cheaper and you can do so much more.

 

Would i need a Unipi or can i operate the doors with just the RPI?

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    This may sound obvious but the PI can not directly operate the doors, you will need a 3V3 to mains conversion to happen

     

    this could be a relay (Solid State or Mechanical), it should be isolated from the PI power and the PI itself, if the relay is mechanical and has an input able to wirk with 3V3 and the module (Not just the relay) is rated for mains your all set

     

    So in summary, is the pi able to act as a ontroller for the doors - YES

    is the PI able to operate the mains based door control - NO, not directly, you need an interface board (NOT a PI FACE DIGITAL or one of the ebay arduino / RPI relay boards either as there only rated for about 24V even though the relays are able to handle 240V. IE, not safe for amatures or otherwise  at mains voltages

     

    If you provide pictures of the damaged boards and any schematics you may have access to we should be able to help better

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to Robert Peter Oakes

    Some pictures for you.

     

    image

    imageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to e14 Contributor

    Can you provide a close up of the module to the left of the motor or the part number / manufacturer

    It looks like it is the motor power control board

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to Robert Peter Oakes

    Thanks so much for your swift replies. I will take close ups of all the parts model numbers etc and post tomorrow. Have a lovely evening.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Close up of Module as requested

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Motor details:

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Close up of Controller details:

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    I found the installation and service manual:

     

    http://www.assa.se/Other/Entrematic/TechDoc/Installation%20manual/EMSL-T%20INST%20MANUALS%20120223/1006278-EMEI-2.0.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to e14 Contributor

    Awsome, loads of good info

     

    so after reading loads of this in detail

     

    It looks like most of the controller board is actually a power supply and it is entirly possible the controller is still OK and only the PSU section is blown, if this is the case, it may be relativly simple to replace the power supply

    Have you been able to measure any voltages on the controller ?

     

    the one thing that stands out on all of this is the safety compliance, if your going to build a PI version for fun thats one thing, if your going to put it into a commercial building / appartment / Store then it MUST be certified and compliant with local code etc, to not do this could cost you dearly with insurance etc

     

    Most of the components look like there either 24V or 40V (Motor?) so the actual interfacing to a PI would just require a relay board probably

     

    Do you know if the other modules are OK, after the surge hit?

     

    Are the units still installed, I am assuming so based on the pictures, how are you operating the doors right now ?

     

    What is your skill set ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to Robert Peter Oakes

    Yes I've sent the controllers in and they are totally fried. To many parts damaged. They accumulated sea air deposits and eventually became one circuit!

     

    I am aware of the safety compliance and will be using it commercially so i need to make sure i program it the same way it operated before. I've got more than basic programming skills but am not a pro. I also have basic electronic skills but av enough support from a pro locally.

     

    I've got two doors with working motors and modules without controllers. I had one controller in working order as seen in pictures which i swapped with the blown controller on a more important door.

     

    The 2 doors that is not working is not so important. I have the time to repair and program the software besides there is so much support online.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to e14 Contributor

    Hi

     

    Can you confirm the voltage operating range for the motors, from the previous pictures it looks to be 40V but I can not be sure, based on what I have seen so far this would be possible with a PI, an Arduino MEGA, A LAunchpad or many other devices including a few Industrial Controllers (PLC devices) that will already have the interfacing to interact with the higher powered devices

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to e14 Contributor

    Hi

     

    Can you confirm the voltage operating range for the motors, from the previous pictures it looks to be 40V but I can not be sure, based on what I have seen so far this would be possible with a PI, an Arduino MEGA, A LAunchpad or many other devices including a few Industrial Controllers (PLC devices) that will already have the interfacing to interact with the higher powered devices