Robotics
  • Technologies
  • More
Robotics
Forum What is a robot
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 28 replies
  • Answers 1 answer
  • Subscribers 81 subscribers
  • Views 5082 views
  • Users 0 members are here
Related

What is a robot

Workshopshed
Workshopshed over 10 years ago

What distinguishes a robot from other mechanisms such as a drone or ROV (remotely operated vehicle) ?

imageimageimage

  • Sign in to reply
  • Cancel

Top Replies

  • spannerspencer
    spannerspencer over 10 years ago +3
    I'm not sure that there's any distinct difference between robots and machinery. As crjeder says, the word "robot" comes from a Czech play, and was invented as a futuristic word for slave. That said, there…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +2
    If the drone replaces a humans work either fully or partially, or even assists (I guess that's the same as partially) then it should qualify but if all it does is fly around (Like a model plane or car…
  • gadget.iom
    gadget.iom over 10 years ago +2
    "I can't define a robot, but I know one when I see one." - Joseph Engelberger
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    If the drone replaces a humans work either fully or partially, or even assists (I guess that's the same as partially) then it should qualify but if all it does is fly around (Like a model plane or car) but serves no other purpose than entertainment then I would say it is not a ROBOT

     

    So the toy drone not performing deliveries for Amazon or Google but simply a toy for Jonny is not a Robot, the one doing the old work of a human.. Robot loose I know but you get the idea

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Workshopshed
    0 Workshopshed over 10 years ago in reply to Robert Peter Oakes

    Peter, using that "replacing human work" definition and applying it to a lawn mower (which I'd not deem to be a robot) if it was used for mowing the grass would qualify but a lawn mower used for racing would not?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Workshopshed
    0 Workshopshed over 10 years ago in reply to Robert Peter Oakes

    Peter, using that "replacing human work" definition and applying it to a lawn mower (which I'd not deem to be a robot) if it was used for mowing the grass would qualify but a lawn mower used for racing would not?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to Workshopshed

    The term is also coupled with semi or full automation / autonomy and as with the drone example, if the lawn mower where cutting the grass autonomously then Robot fits, if your not aotomating it but simple stick a seat on it and drive it around a course as in racing then its not, as is it is more like a car. now if the car was fully automated and replaced the driver then we would be back to a Robot., You would simply be a passenger and perhaps just provide the destination