Robotics
  • Technologies
  • More
Robotics
Forum N.O. triggered sirin: what do I need to trigger on signal?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 3 answers
  • Subscribers 78 subscribers
  • Views 1379 views
  • Users 0 members are here
Related

N.O. triggered sirin: what do I need to trigger on signal?

e14 Contributor
e14 Contributor over 10 years ago

I am looking at triggering any number of low voltage devices from simple alarm contacts, yet I do not know the name of what I need.

It needs to have 2 separate circuits, 1 for signal and 1 for outputting 9-24v DC when the signal circuit is closed.

 

Thank you.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 10 years ago in reply to e14 Contributor +1 suggested
    Hi Pastor, For safety sake you should have the low voltage supply powered from your mains using something like an AC adapter. This will isolate the high voltage from your system. Then the simplest arrangement…
  • jw0752
    jw0752 over 10 years ago +1 suggested
    Hi Pastor, Here are a couple of simple circuits. This first one will sound the alarm as long as the sensor switch is activated. This second circuit will latch and continue to power the alarm until the…
  • jw0752
    jw0752 over 10 years ago in reply to e14 Contributor +1 suggested
    Hi Pastor, Here is a circuit that I used to demonstrate the function of a Parallax Brand PIR (Passive Infra Red Sensor). The PIR in this circuit is powered with 5 volts and therefore a 5 volt voltage regulator…
Parents
  • gadget.iom
    0 gadget.iom over 10 years ago

    It's difficult to determine what you're trying to achieve. Can you provide a litt more detail?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to gadget.iom

    I need to take a simple Normally open signal to switch on and off a low voltage supply.

     

    When the signal circuit is grounded, the Low voltage circuit should be grounded to supply power.

     

    Example : Infrared sensor detects heat, closes normally open contact - circuit takes signal and closes power - LED turns on, peso sounds, symbol playing monkey plays symbols.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 10 years ago in reply to e14 Contributor

    Hi Pastor,

    For safety sake you should have the low voltage supply powered from your mains using something like an AC adapter. This will isolate the high voltage from your system. Then the simplest arrangement would be to use a relay in series with your switch and low voltage power supply. The relay could then control a different circuit with a different voltage. If the voltage of your lights and cymbal monkey are the same as the low voltage circuit just eliminate the relay and put the cymbal monkey in series with the N/O switch and the power supply. Since I do not know your level of expertise it is difficult to describe in more detail. You mentioned an IR detector which would make the system more complicated as the sensor would need support circuitry to act as a proper switch. To get the best information you may want to check out these instructions for submitting a question that shabaz wrote to help with clarification of presented questions.

     

    How to Ask Questions using the Create Discussion tool

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to jw0752

    The example of an IR sensor is the most likely scenario . I am pretty sure alarm contacts are designed to detect the resistance of the circuit using very low current most likely too low to trigger of a relay, and my main desire is to use standard alarm contacts as signal sources.

     

    What would be needed to beef up the current to trigger a relay?

     

    My knowledge is basic and burg and fire alarms on a technician level. I have zero engineering experience so I have no idea how to make these circuits and what parts I need to get the desired effect, yet am competent enough to understand and build from a diagram.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 10 years ago in reply to e14 Contributor

    Hi Pastor,

    Here is a circuit that I used to demonstrate the function of a Parallax Brand PIR (Passive Infra Red Sensor). The PIR in this circuit is powered with 5 volts and therefore a 5 volt voltage regulator 7805 is required. The sensor measures the temperature of its sensor area. Once the sensor field is stable the sensor will reset and the output will go to 0 volts. If the temperature changes due to someone or something moving in the sensor field the output of the sensor will go high to 5 volts and this in turn will turn on the MOSFET which will turn on the load. The alarm will sound until the sensor field is once again stable.

     

    Newark listing of the PIR:

     

    http://www.newark.com/parallax/555-28027/pir-sensor-180-degree-sensor/dp/11X5850?ost=Parallax+PIR&selectedCategoryId=&categoryName=All+Categories&categoryNameResp=All%2BCategories

     

    Schematic of PIR Circuit:

    image

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 10 years ago in reply to e14 Contributor

    Hi Pastor,

    Here is a circuit that I used to demonstrate the function of a Parallax Brand PIR (Passive Infra Red Sensor). The PIR in this circuit is powered with 5 volts and therefore a 5 volt voltage regulator 7805 is required. The sensor measures the temperature of its sensor area. Once the sensor field is stable the sensor will reset and the output will go to 0 volts. If the temperature changes due to someone or something moving in the sensor field the output of the sensor will go high to 5 volts and this in turn will turn on the MOSFET which will turn on the load. The alarm will sound until the sensor field is once again stable.

     

    Newark listing of the PIR:

     

    http://www.newark.com/parallax/555-28027/pir-sensor-180-degree-sensor/dp/11X5850?ost=Parallax+PIR&selectedCategoryId=&categoryName=All+Categories&categoryNameResp=All%2BCategories

     

    Schematic of PIR Circuit:

    image

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer