Robotics
  • Technologies
  • More
Robotics
Forum N.O. triggered sirin: what do I need to trigger on signal?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 3 answers
  • Subscribers 78 subscribers
  • Views 1388 views
  • Users 0 members are here
Related

N.O. triggered sirin: what do I need to trigger on signal?

e14 Contributor
e14 Contributor over 10 years ago

I am looking at triggering any number of low voltage devices from simple alarm contacts, yet I do not know the name of what I need.

It needs to have 2 separate circuits, 1 for signal and 1 for outputting 9-24v DC when the signal circuit is closed.

 

Thank you.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 10 years ago in reply to e14 Contributor +1 suggested
    Hi Pastor, For safety sake you should have the low voltage supply powered from your mains using something like an AC adapter. This will isolate the high voltage from your system. Then the simplest arrangement…
  • jw0752
    jw0752 over 10 years ago +1 suggested
    Hi Pastor, Here are a couple of simple circuits. This first one will sound the alarm as long as the sensor switch is activated. This second circuit will latch and continue to power the alarm until the…
  • jw0752
    jw0752 over 10 years ago in reply to e14 Contributor +1 suggested
    Hi Pastor, Here is a circuit that I used to demonstrate the function of a Parallax Brand PIR (Passive Infra Red Sensor). The PIR in this circuit is powered with 5 volts and therefore a 5 volt voltage regulator…
Parents
  • jw0752
    0 jw0752 over 10 years ago

    Hi Pastor,

    Here are a couple of simple circuits. This first one will sound the alarm as long as the sensor switch is activated.

     

    image

     

    This second circuit will latch and continue to power the alarm until the Reset Switch is pushed. Both of these circuits use the same power supply for the sensor and the output device.

     

    image

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 10 years ago

    Hi Pastor,

    Here are a couple of simple circuits. This first one will sound the alarm as long as the sensor switch is activated.

     

    image

     

    This second circuit will latch and continue to power the alarm until the Reset Switch is pushed. Both of these circuits use the same power supply for the sensor and the output device.

     

    image

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer