Robotics
  • Technologies
  • More
Robotics
Forum Lidar Lite v3 Irratic Measurement
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Answers 7 answers
  • Subscribers 77 subscribers
  • Views 3751 views
  • Users 0 members are here
  • lidar
  • garmin
Related

Lidar Lite v3 Irratic Measurement

brucewilsonph@yahoo.com.ph
brucewilsonph@yahoo.com.ph over 8 years ago

Hello Everyone!

 

I have a Garmin Lidar Lite v3.

 

There is an obstacle at 24" in from of the Lidar.  About one percent of the time, the Lidar will give a measurement of about 14" or about 9".

 

What could possibly be happening?

 

Bruce

  • Sign in to reply
  • Cancel

Top Replies

  • the48sicks
    the48sicks over 8 years ago +1 suggested
    Hi Bruce Mine does exactly the same, I think Douglas and DAB have it thouh. You can try setting the different modes for short/mid/long range to make it a bit more accurate. In the end I started taking…
  • the48sicks
    the48sicks over 8 years ago in reply to brucewilsonph@yahoo.com.ph +1 suggested
    Hi Bruce Im using the LIDARLite Arduino Library. It gives you options for config and scanning. When you call the distance method there is also a true/false parameter to scan with or without bias correction…
  • brucewilsonph@yahoo.com.ph
    brucewilsonph@yahoo.com.ph over 8 years ago in reply to the48sicks +1
    That information isn't in the Python library. Thank you so much!
Parents
  • DAB
    0 DAB over 8 years ago

    You could be getting reflections from more distant objects that are appearing in the next distance cycle.

    It depends upon the AGC they use and the chirp encoding.

    Given the price of the unit, I would expect it to have just minimal interference circuitry built in, so you will expect to see some erratic behavior.

     

    Is there a highly reflective target in the far field?

    Different reflectivity can introduce errors.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • DAB
    0 DAB over 8 years ago

    You could be getting reflections from more distant objects that are appearing in the next distance cycle.

    It depends upon the AGC they use and the chirp encoding.

    Given the price of the unit, I would expect it to have just minimal interference circuitry built in, so you will expect to see some erratic behavior.

     

    Is there a highly reflective target in the far field?

    Different reflectivity can introduce errors.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • brucewilsonph@yahoo.com.ph
    0 brucewilsonph@yahoo.com.ph over 8 years ago in reply to DAB

    Thank you so very much!  Will have to remember this when I get it into a real working environment.