Robotics
  • Technologies
  • More
Robotics
Forum Phase rotation circuit switching
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 77 subscribers
  • Views 433 views
  • Users 0 members are here
Related

Phase rotation circuit switching

e14 Contributor
e14 Contributor over 15 years ago

I am looking to bring three phase legs and a neutral line into

a test box and , using one switch preferably or switches, swap phase 1 to 2,

2 to 3 and 3 to 1 and 1 to 3, 2 to 1 and 3 to 2.  Can anyone suggest the best way

to accomplish this.  The input is normally 125VAC,@ less than one amp.

  • Sign in to reply
  • Cancel
Parents
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 15 years ago

    Those switches do exist. They are called cross switches. If you intend to switch an inductive load, like a motor, you need more contact spacing to prevent an arc between the contacts when the current is interrupted. The normal voltage between the contacts is already 216 Volt. The best way is a 3 position swith. The middle position is the OFF position. The outer positions are left and right rotation. So you need a 3 position 3 contact switch. Or a 3 position 4 contact switch if you want to have a contact in the neutral wire. Often 3 phase contactors are used, with a control circuit preventing energizing both coils at the same time. This way you can operate a hoist, using an up and a down button.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 15 years ago

    Those switches do exist. They are called cross switches. If you intend to switch an inductive load, like a motor, you need more contact spacing to prevent an arc between the contacts when the current is interrupted. The normal voltage between the contacts is already 216 Volt. The best way is a 3 position swith. The middle position is the OFF position. The outer positions are left and right rotation. So you need a 3 position 3 contact switch. Or a 3 position 4 contact switch if you want to have a contact in the neutral wire. Often 3 phase contactors are used, with a control circuit preventing energizing both coils at the same time. This way you can operate a hoist, using an up and a down button.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to jvdberg@ieee.org

    Thank you Johan,

     

    I appreciate your help.  We found a single deck rotary

     

    switch from Grayhill with 3 poles and 3 positions per

     

    pole at 30 degrees rotation per position. We'll run the neutral

     

    straight through bypassing the switch.

     

     

     

                                                    Chris Kast

     

     

     

     

     

     

     

    **like us on Facebook, search VeriTranz

     

     

     

    *drop by and see us @APTAexpo2011, booth 6056*

     

     

     

    Christopher Kast

     

    Veritech, Inc.

     

    628 Route 10, Unit #4

     

    Whippany, NJ 07981

     

    908-400-6396 (Cell)

     

    973-560-4750 (Office)

     

    973-581-7134 (Fax)

    Attachments: