Robotics
  • Technologies
  • More
Robotics
Forum Servo trouble
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 52 replies
  • Subscribers 80 subscribers
  • Views 7002 views
  • Users 0 members are here
Related

Servo trouble

royston02
royston02 over 12 years ago

I wanted to know if a servo left without power in stationery mode (without making me want to turn it) lift the weight?

Eg:- A skateboard. I just want to stand on itwithout it moving. the skateboard is the servo. Will the skateboard i.e servo stand or fall? No battery. 

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 12 years ago +2
    If you can live with a normal DC motor and use it with a worm gear, it should "lock" when not powered.
  • mcb1
    mcb1 over 12 years ago in reply to royston02 +1
    Try this .. Open your browse and enter this in a google search "how does a servo work" the first two results give a good breakdown of how it works. Mark
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago +1
    Note there are many different systems that fall under the name of SERVO. The one you linked in may be geared but not like the one shown above. A typical Remote control plane/Car/Boat servo is based on…
Parents
  • shabaz
    0 shabaz over 12 years ago

    Hi Royston,

     

    Sometimes it is hard to know where to begin, because the question could be interpreted in many ways. It may take up days of your time to reach the correct answer.

    This was an interesting site just for occasionally referring to (I check it from time to time). If I'm asking a question on forums I'll often pause and then maybe delete and re-type the whole thing:

    https://www.biostars.org/p/75548/

    However probably nowadays it should also state that where possible a picture/diagram can also say a thousand words.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • royston02
    0 royston02 over 12 years ago in reply to shabaz

    Here is the full explanation.

       1)Why are you using servo?

    Ans:It is because in my project I would like to build a transportation jet. The load I want to carry is 15-20kg. A very powerful motor drain all the amps of the battery within no time. So I thought a servo to lift weight. Then I realized it would also drain amps. I was not going to move the servo. It would be stationery. So why should I power it if it can lift the weight without power and signal. SO that is why I  asked the question. Hope this clearifies the problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 12 years ago in reply to royston02

    Thanks Royston, but I am still a bit lost. To me a transportation jet is a vehicle with a gas turbine engine.

    It looks like you want a robotic wheeled vehicle to transport a 20 kg load, but I am just guessing.

    It looks like you want a servo motor to lift the load onto the vehicle. If this is true, you can simply turn off power to the servo (or DC motor) after the load is on the vehicle.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • royston02
    0 royston02 over 12 years ago in reply to dougw

    Alright. many of you are getting confused with transportation jet idea.

    Eg:(took me a long time to think)

    {

    Suppose I was making a robot like a human on wheels and want it to carry weight on the back.I made a rectangular box for it. If I directly mount it on the back of the robot to things:-

    a)It will not have a proper centre of gravity.

    b)It will strain the motors.

    So I thought to use a servo. Servo will drain the battery and I am not moving it. the arm wll be stationery. SO I thought about not powering the servo.

    Will the servo hold the weight the weight without power?

    }

    And I am not using a gas turbine engine because I wanted it to be a green project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • royston02
    0 royston02 over 12 years ago in reply to dougw

    Alright. many of you are getting confused with transportation jet idea.

    Eg:(took me a long time to think)

    {

    Suppose I was making a robot like a human on wheels and want it to carry weight on the back.I made a rectangular box for it. If I directly mount it on the back of the robot to things:-

    a)It will not have a proper centre of gravity.

    b)It will strain the motors.

    So I thought to use a servo. Servo will drain the battery and I am not moving it. the arm wll be stationery. SO I thought about not powering the servo.

    Will the servo hold the weight the weight without power?

    }

    And I am not using a gas turbine engine because I wanted it to be a green project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to royston02

    A diagram will really help for us to visualize what your really trying to build, even if it is a straw man type diagram

     

    Are you trying to make a humanoid like robot on wheels where you want to carry a load on its back ??, and is the plan to use a motor or servo (By the way there both motors and while in motion will consume similar amounts of energy as this is proportional to the work it has to do) to lift a load into place on the back of said humanoid robot

     

    you could use a clamp to hold the load when it gets there,

     

    as I said, a picture will help unbelievably in clarifying what your really trying to achieve as "suppose" statements makes us think you not sure.

     

    Were not trying to be awkward, just your being a little vague

     

    Please post a picture ?

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dragonstyne
    0 dragonstyne over 12 years ago in reply to royston02

    Royston,  thank you for your explanation.  As Peter said, a diagram would help greatly. Based on what you have given us so far:

    I agree a winch servo or a servo modified for continuous movement passed 360 degrees, is the best choice for your project.  However,  it will not hold a load reliability without power.

     

    You may need something in the box the passivity hood the load during transport. Or a transmission with a worm drive or brake to hold the load.

     

    A diagram will confirm this.

     

    Regards,

     

    -Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • royston02
    0 royston02 over 12 years ago in reply to dragonstyne

    http://www.ez-robot.com/Shop/Images/Products/1355/Adapter%20with%20servo.jpg

    http://www.ez-robot.com/Shop/Images/Products/1355-hd.jpg

    Had problems sving a image to the discussion so had to find a similar one/s. Hope you copperate. The fomer one is like the servo clipped to the latter one. The fomer's part clips to the humanoid.(sorry for the lame explanation).The latter will be the rectangular one with the box. Only a different. Once I figure a way to upload picture I will try to.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dragonstyne
    0 dragonstyne over 12 years ago in reply to royston02

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • royston02
    0 royston02 over 12 years ago in reply to dragonstyne

    Goes to a whole new page and in the url shows the file location and displays the picture. What next?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dragonstyne
    0 dragonstyne over 12 years ago in reply to royston02

    Select the picture and press "Insert Picture" lower right side of the pop up.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • royston02
    0 royston02 over 12 years ago in reply to dragonstyne

    http://img.deusm.com/eetimes/2013/10/1319757/max-0087-03.jpg

    In this, the top part is what I want to hold heavy object. I want to use servo under the lower frame to hold the top one. If I don't power the servo, will the frame hold or servo fail? I don't want to load or anything. Just hold the weight on the servo without power.

     

    Can someone make a tutorial for loading custom pictures. My dosen't load.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 12 years ago in reply to royston02

    Hi Royston,

    Will the servo be used to tip load bed like a dump truck?

    If I understand it...

    When the load bed is flat and inactive, it could simply rest on fixed "stop" posts, taking the load off the servo.

    When the servo needs to move the load bed, the load bed would simply lift off the stop post(s) and hinge up.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • royston02
    0 royston02 over 12 years ago in reply to dougw

    The servo is stationery, no tipping, no loading. The thing is that I'm using it to hold load since the motors are brushed. Yo the servo will be kept underneath and I want the servo to carry the weight without transferring to the load to the motors/frame(since all the weight is absorbed by the gears). You all are a long way from my point I've noticed.I prefer you ask everything to clear your mind to the point.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dragonstyne
    0 dragonstyne over 12 years ago in reply to royston02

    Greetings, 

    do you have a drawing the the load plate removed showing how the servo is connected to the vehicle.  That would help. The way servos are designed , I don't see it holding the load plate stationary without help such as a transmission or a support that can be moved out of the way when the load is to be moved.

     

    -Steve