Robotics
  • Technologies
  • More
Robotics
Forum I am interested in a circuit board to control a two digit 7 segment LED.  Information will be coming from my software.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 29 replies
  • Answers 1 answer
  • Subscribers 81 subscribers
  • Views 3636 views
  • Users 0 members are here
  • frontpage
Related

I am interested in a circuit board to control a two digit 7 segment LED.  Information will be coming from my software.

e14 Contributor
e14 Contributor over 12 years ago

I am interested in a circuit board to control a two digit 7 segment LED.  Information will be coming from my software.
I will need the circuit board to show a number (up to 2 digits) and to be able to also have a push button when pressed to turn off the 7 segment LED displaced. 

The quantity of the same board will be from 250 up to 1000 boards.

 

Thanks,

Tim Cloninger

timcloninger@cs.com

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 12 years ago +1
    What is the software running on and how will it interface with the display board. MK
  • michaelkellett
    michaelkellett over 12 years ago in reply to e14 Contributor +1
    I think you will need a custom board to keep this as cheap as possible but it may still cost you a fair bit. It will cost much less if you assemble the display boards yourself. Each board needs to be addressable…
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago +1
    Another thought could be this http://www.sqlskills.com/blogs/paulselec/post/arduino-cascading-shift-registers-to-drive-7-segment-displays.aspx , or based on it anyway, it uses a serial in, serial out mechanism…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    Using an Arduino or TI launchpad for a prototype (Use one with built in USB to save on a device), drive the 7 Segment direct from the uController and your done, when ready for production, simply create custom board with just what you need.

     

    Plugs into a USB of any pc / laptop

     

    driving the 7 Seg displays is the easy bit

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    Using an Arduino or TI launchpad for a prototype (Use one with built in USB to save on a device), drive the 7 Segment direct from the uController and your done, when ready for production, simply create custom board with just what you need.

     

    Plugs into a USB of any pc / laptop

     

    driving the 7 Seg displays is the easy bit

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to Robert Peter Oakes

    what I did not see mention is if the 1000's of boards are to be controlled by a single PC or are destined to be sold as individual devices for separate consumers.

     

    Is this to be a commercial product ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to Robert Peter Oakes

    As I understand it the OP needs one PC talking to many displays - USB won't do (can't chain the devices, can't have enough devices, cables much too pricey etc.)

    Not much point in an Arduino based prototype - need to choose the bits on the basis of lowest cost for making up to 1000 of them - as you say it's easy driving the display - it's the comms (which are not standard on anything) that need developing.

     

    MK