Robotics
  • Technologies
  • More
Robotics
Forum I am interested in a circuit board to control a two digit 7 segment LED.  Information will be coming from my software.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 29 replies
  • Answers 1 answer
  • Subscribers 81 subscribers
  • Views 3676 views
  • Users 0 members are here
  • frontpage
Related

I am interested in a circuit board to control a two digit 7 segment LED.  Information will be coming from my software.

e14 Contributor
e14 Contributor over 12 years ago

I am interested in a circuit board to control a two digit 7 segment LED.  Information will be coming from my software.
I will need the circuit board to show a number (up to 2 digits) and to be able to also have a push button when pressed to turn off the 7 segment LED displaced. 

The quantity of the same board will be from 250 up to 1000 boards.

 

Thanks,

Tim Cloninger

timcloninger@cs.com

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 12 years ago +1
    What is the software running on and how will it interface with the display board. MK
  • michaelkellett
    michaelkellett over 12 years ago in reply to e14 Contributor +1
    I think you will need a custom board to keep this as cheap as possible but it may still cost you a fair bit. It will cost much less if you assemble the display boards yourself. Each board needs to be addressable…
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago +1
    Another thought could be this http://www.sqlskills.com/blogs/paulselec/post/arduino-cascading-shift-registers-to-drive-7-segment-displays.aspx , or based on it anyway, it uses a serial in, serial out mechanism…
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    image

    Hello i am interested in making LED Display ( DOT Matrix or 7-Segment )  for Temperature monitoring application .

    · Large 12.0 inch high characters using Indoor Red LEDS in a 5 x 7 pixel configuration; 4 digits per display. X X X X format

    · Viewing distance up to 550 - 575 feet.

    · Input will be a 4 – 20 ma signal. Output range to be defined by customer.

    · The Analog to Digital converter will be mounted inside the display enclosure. Two signal wires are used for the customers input signal.

    · Windows Calibration software provided to make changes to the calibration for the display.

    • RS232 serial input terminated inside the display at a terminal block.

    · Wall Mount tabs provided located on top of the display for mounting.

    · Approximate Dimensions: 54”L x 18”H x 2.5”D

    LED Intensity:  MCD High-Intensity Digits/Discrete LEDS

    · NEMA 1 extruded aluminum enclosure w/ red acrylic face

    POWER REQUIREMENTS: 220 VAC / 50 HZ ; 6 ft. line cord should provided

     

    Could you help me with the required components list .need

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    image

    Hello i am interested in making LED Display ( DOT Matrix or 7-Segment )  for Temperature monitoring application .

    · Large 12.0 inch high characters using Indoor Red LEDS in a 5 x 7 pixel configuration; 4 digits per display. X X X X format

    · Viewing distance up to 550 - 575 feet.

    · Input will be a 4 – 20 ma signal. Output range to be defined by customer.

    · The Analog to Digital converter will be mounted inside the display enclosure. Two signal wires are used for the customers input signal.

    · Windows Calibration software provided to make changes to the calibration for the display.

    • RS232 serial input terminated inside the display at a terminal block.

    · Wall Mount tabs provided located on top of the display for mounting.

    · Approximate Dimensions: 54”L x 18”H x 2.5”D

    LED Intensity:  MCD High-Intensity Digits/Discrete LEDS

    · NEMA 1 extruded aluminum enclosure w/ red acrylic face

    POWER REQUIREMENTS: 220 VAC / 50 HZ ; 6 ft. line cord should provided

     

    Could you help me with the required components list .need