Robotics
  • Technologies
  • More
Robotics
Forum Fastest Pololu Micro Metal Gearmotor?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 75 subscribers
  • Views 1476 views
  • Users 0 members are here
  • research
  • robotics
  • robots
  • motors
  • electronics
  • automation
Related

Fastest Pololu Micro Metal Gearmotor?

e14 Contributor
e14 Contributor over 11 years ago

I am building a line following robot, and I can't decide which motor would be the fastest. Below I have posted a table of the Micro Metal Gearmotors from Pololu Robotics and Electronics. Here is a product listing and chart of all the motors. Please post the product name, and a link if possible. Thanks! (If you have any other ideas to make a low profile robot awesome, post it in the comments below)image


  • Gearbox Shaft Only means it is the shaft directly from the motor
  • Gearbox & Motor Shafts is an extended shaft

 

Motor TypeStall
Current
@ 6 V
No-Load
Speed
@ 6 V
Stall Torque
@ 6 V
image

 

Gearbox Shaft Only
image

 

Gearbox & Motor Shafts
high-power
(HP)
1600 mA6000 RPM2 oz-in5:1 micro HP
3000 RPM4 oz-in10:1 micro HP10:1 micro HP
1000 RPM9 oz-in30:1 micro HP30:1 micro HP
625 RPM15 oz-in50:1 micro HP50:1 micro HP
400 RPM22 oz-in75:1 micro HP75:1 micro HP
320 RPM30 oz-in100:1 micro HP100:1 micro HP
200 RPM40 oz-in150:1 micro HP150:1 micro HP
140 RPM50 oz-in210:1 micro HP
120 RPM60 oz-in250:1 micro HP
100 RPM70 oz-in298:1 micro HP298:1 micro HP
32 RPM125 oz-in1000:1 micro HP1000:1 micro HP
medium-power
(MP)
700 mA2200 RPM3 oz-in10:1 micro MP10:1 micro MP
730 RPM8 oz-in30:1 micro MP
420 RPM13 oz-in50:1 micro MP
290 RPM17 oz-in75:1 micro MP75:1 micro MP
220 RPM19 oz-in100:1 micro MP100:1 micro MP
150 RPM24 oz-in150:1 micro MP
75 RPM46 oz-in298:1 micro MP
low-power360 mA2500 RPM1 oz-in5:1 micro
1300 RPM2 oz-in10:1 micro
440 RPM4 oz-in30:1 micro30:1 micro
250 RPM7 oz-in50:1 micro50:1 micro
170 RPM9 oz-in75:1 micro
120 RPM12 oz-in100:1 micro100:1 micro
85 RPM17 oz-in150:1 micro
60 RPM27 oz-in210:1 micro
50 RPM32 oz-in250:1 micro
45 RPM40 oz-in298:1 micro298:1 micro
14 RPM70 oz-in1000:1 micro
  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 11 years ago +1 suggested
    Not sure what is so hard about this. The 6000 rpm is the fastest. Whether it is suitable for your application is a different story. This would depend on the power you have available (battery and controller…
  • dougw
    dougw over 11 years ago +1 verified
    It depends on how big your robot is, the diameter of the wheels and how much traction your wheels have. If you have 2 inch wheels driven by a 200 rpm shaft the robot will travel around 20 inches per second…
Parents
  • dougw
    0 dougw over 11 years ago

    It depends on how big your robot is, the diameter of the wheels and how much traction your wheels have.

    If you have 2 inch wheels driven by a 200 rpm shaft the robot will travel around 20 inches per second, which is pretty fast for typical cornering requirements. You can scale the speed back using variable PWM drive to the gearmotors.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 11 years ago

    It depends on how big your robot is, the diameter of the wheels and how much traction your wheels have.

    If you have 2 inch wheels driven by a 200 rpm shaft the robot will travel around 20 inches per second, which is pretty fast for typical cornering requirements. You can scale the speed back using variable PWM drive to the gearmotors.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer