Robotics
  • Technologies
  • More
Robotics
Forum Triac protection against short-circuit
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 77 subscribers
  • Views 1653 views
  • Users 0 members are here
  • tvs
  • short-circuits
  • triac
  • protection
Related

Triac protection against short-circuit

femtotech
femtotech over 11 years ago

Hi!

I have a board with the basic triac driver circuits as described at page 8 (fig. 14) of MOC3052:

 

https://www.fairchildsemi.com/datasheets/MO/MOC3052M.pdf

 

The triac is a BTA204S-600D (600V 4A).

The load is a small electric motor (less than 250W) but there are no snubbers because the leakage is not acceptable for the customer.

 

I tested a resistive load up to 750W with no problems. The circuits works well also with lighter inductive loads, about 100W.

With the original one (250W) after few commutations the triac goes in short-circuit - I guess due to the back-EMF when disabling the triac.

 

I tried with a very big triac (25A, 250A peak) and there are no problems, but of course it's not a good solution.

I also tried with a TVS (275V) to clamp the VAC across the line (between L and N, and between T1 and T2) with no chance.

Also a snubber between L and N does nothing.

 

Any idea?

  • Sign in to reply
  • Cancel
  • D_Hersey
    D_Hersey over 11 years ago

    The spike injects current into the control terminal latching it back on.  The TVS has to change state in order to protect, the triac turns on in the meantime.  A tiny snubber might get the thing to work.  You are using a very-sensitive gate triac which is contrary to your interests.  Being easy to turn on means that it is easy to turn on spuriously.  Back-to-back SCRs are the way the hip kids are doin' it, nowadays.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • femtotech
    femtotech over 11 years ago in reply to D_Hersey

    Thank you for your answer.

    Ok, the spikes spuriously turn on the triac, but why it breaks? I mean, perhaps the spikes are so high they burn the control terminal? Because the triac appears in short-circuit between T1 and T2 when removed from the board.

    About the snubbers, I tried:

     

    - across L+N (across the load device) with no effect

     

    - across T1 and T2: it works, but the small leakage is not accepted by the customer, because there is a little amount of current on the device even when the triac is off (due to the C impedance, of course)

     

    Do you suggest a different position?

    Or another triac I could use for such a load (they are in DPAK).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • D_Hersey
    D_Hersey over 11 years ago

    I hesitate to make too specific of comments because I don't have enough information about your case.  If you post a schematic, maybe I can be more helpful.

     

    Typically, snubbers operate just as well across the switch or across the load.  If the load is normally off, we shunt the load with the snubber.  If it is normally on, we shunt the switch.  Clamps and snubbers do not preclude one another.  Using a clamp allows using a higher-Z snubber, sometimes no snubber.

     

    My first move would be to go to a non-sensitive-gate triac.  Or more probably back-to-back SCR.  Remember to de-rate!

     

    Basic Triac and SCR Projects and Circuits

     

    Check out the last illustration.  There are less ways to turn on back-to-back SCR v. TRIAC.  This helps the situation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • artful_bodger
    artful_bodger over 11 years ago in reply to femtotech

    You could try a choke in series with the triac.  You'd normally fit one to stop noise from the triac conducting out, but it might do it.

    Out of interest, why is the client objecting to leakage.  Is it for a 'green' or medical product?  There is permitted LN (&E) leakage for medical.

    There is an interesting note on the datasheet on type approvals.  As part of the CE approval (assuming your device will be used in the EU), your circuit may be subjected to surges, so it looks like you might need the snubber.  Depends which parts of the EMI standard / target market the product is for.

     

    This is a possible explanation for device destruction.  The motor emf, which triggers the triac conduction, could occur when the mains is at say -230V, and the EMF at say +1000V.  Way outside the triac operating region.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • femtotech
    femtotech over 11 years ago

    Thank you both for explanations and suggestions. Now I understand a little bit more than before :-)