Security and Identification
  • Technologies
  • More
Security and Identification
Blog AIRprint biometric sensor can scan fingerprints from 2 meters away
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Security and Identification to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ZeroSizeObject
  • Date Created: 18 Jan 2011 9:38 PM Date Created
  • Views 941 views
  • Likes 1 like
  • Comments 1 comment
  • security
  • fingerprint_scanner
  • camera
  • wireless
  • safety
Related
Recommended

AIRprint biometric sensor can scan fingerprints from 2 meters away

ZeroSizeObject
ZeroSizeObject
18 Jan 2011
image
 
Over the years, fingerprinting has evolved from an inky mess to pressing fingers on sensor screens to even a few touch-free systems that work at a short distance. Now a company, called Advanced Optical Systems Inc., has developed a prototype of a device that can scan fingerprints from up to two meters away, an approach that could prove especially useful at security checkpoints in places like Iraq and Afghanistan. It detects fingerprints by shining polarized light onto a person's hand and analyzing the reflection using two cameras configured to detect different polarizations. Slightly smaller than a square tissue box, AIRprint houses two 1.3 megapixel cameras and a source of polarized light. One camera receives horizontally polarized light, while the other receives vertically polarized light. When light hits a finger, the ridges of the fingerprint reflect one polarization of light, while the valleys reflect another. The prototype device, which scans a print in 0.1 seconds and processes it in about four seconds, can handle only one finger at a time. Also, the scanned finger must remain at a fixed distance from the device. I guess terrorists can circumvent this technology by being 2 1/2 meters away from the scanner. Or simply defeat it by not standing perfectly still. What do you all think, would you feel more safe or further violated with this device at airports? For more info on AIRprint visit: http://www.aos-inc.com/index.php/home

Zero
  • Sign in to reply
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Const. Wendy Drummond, spokesperson for the 2010 G8-G20 Integrated Security Unit, told CTV News that some key intersections will have more than one of the temporary cameras. In addition, more Board Cameras might yet be used on a rapid-deployment basis once the summit is underway, she said. Others will be inside the inner security zone and won’t be visible to the general public.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 13 years ago

    Const. Wendy Drummond, spokesperson for the 2010 G8-G20 Integrated Security Unit, told CTV News that some key intersections will have more than one of the temporary cameras. In addition, more Board Cameras might yet be used on a rapid-deployment basis once the summit is underway, she said. Others will be inside the inner security zone and won’t be visible to the general public.