Sensors
  • Technologies
  • More
Sensors
Blog Engineers Develop Living Circuit Boards Using Bacteria That Work Like Transistors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 25 Aug 2026 8:55 PM Date Created
  • Views 760 views
  • Likes 4 likes
  • Comments 2 comments
  • research
  • mit
  • on_campus
  • biomimicry
  • organic
  • bio-circuit
  • university
  • innovation
Related
Recommended

Engineers Develop Living Circuit Boards Using Bacteria That Work Like Transistors

Catwell
Catwell
25 Aug 2026

image

MIT has engineered bacteria to function like transistors for living circuit boards. (Image Credit: MIT)

Transistors are used in circuitry to control electrical signal flow. But now there is a bio-inspired one. MIT engineers modified bacteria that can be integrated into larger circuits and perform switching similar to transistors. With this technique, computational systems could operate in biological environments, where it’s challenging to deploy electronics.    

A bacterium called Pantoea agglomerans, found on surfaces like plants, was used as the groundwork for the team’s system. Instead of loading a computational circuit into one cell, they engineered individual bacterial strains for simple switching functionality. They can then connect those components, forming a more complex biological circuit.

The team printed bacterial colonies onto plates containing agar, spacing each colony 5 mm apart. This spacing limits signal transmission to nearby colonies, ensuring each one passes information to the next and creates a one-way path throughout the circuit.

This system features two types of bacterial transistors along with three additional strains that work like molecular relays (OC-6, OC-12, and OHC-14). These resistors don’t respond to electrical current, but rather chemical signals. The OC-6 molecule acts like the control input, turning the transistor on/off. Meanwhile, OC-12 acts like the signal/input being processed. And finally, OHC-14 is the output signal produced by the transistor.

All the relay strains serve as wiring between each component. These turn the output signal into another molecular signal that makes a downstream transistor active. Controlling which bacterial colonies are set beside each other allows the team to modify how data moves through the circuit. This is achieved without the need to genetically redesign the components.

Their technique solves an issue with synthetic-biology circuits. Placing various functions within the same cell crowds the molecular machinery. At the same time, interacting genetic components may cause interference with each other. Isolating those functions into specialized strains enables the team to assemble more complex architectures from a small set of building blocks.

The researchers showed that the bio circuit performs multiple inputs and several types of logic operations. In addition, they developed a demultiplexer that sends a signal toward one of the outputs, depending on a control input. Transistors were combined into more complex circuits, including one that adds two inputs. The biggest circuit they built connected 24 bacterial colonies.

However, these systems aren’t as fast as electronic processors. It takes approximately eight hours to run a calculation. Even then, the top priority isn’t speed. The team believes the system is more ideal for operating where living systems exist. In the future, bacterial circuits could be placed on plant leaves or roots to detect drought and pests, and trigger a biological response.

Have a story tip? Message me here at element14.

  • Sign in to reply
  • Qbit
    Qbit 2 months ago

    Building on DAB's point the real advantage here over electronics isn't speed, it's radiation hardiness and biological self-maintenance. For multi-century deep-space missions, a biological processor that feeds on basic nutrients and repairs its own logic gates could survive harsh cosmic radiation long after silicon degradation!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB 2 months ago

    Could be an interesting way to send out long range probes into the solar system that will take millennia to complete.