Sensors
  • Technologies
  • More
Sensors
Blog LeviPrint Uses Acoustic Levitation for Contactless Fabrication
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 17 Jan 2023 7:45 PM Date Created
  • Views 19795 views
  • Likes 6 likes
  • Comments 1 comment
  • touch
  • hmi
  • aucoustic
  • cabeatwell
  • university
  • innovation
Related
Recommended

LeviPrint Uses Acoustic Levitation for Contactless Fabrication

Catwell
Catwell
17 Jan 2023

image

LeviPrint uses sound to levitate objects and a robotic arm and liquid dispenser to manufacture complex objects. (Image credit: UpnaLab via YouTube)

Researchers from UpnaLab, Smart Cities Institute divisions of the Public University of Navarre, UltraLeap, and the University of São Paulo have developed a contactless method of fabricating objects using acoustic levitation. LeviPrint is a contactless fabrication process using total acoustic trapping of elongated parts. It uses the principle of acoustic trapping and levitation, which is based on the acoustic radiation force of sound waves. In this process, a sound wave is generated and directed toward the elongated part, creating an acoustic trap.

The acoustic trap, together with a robotic arm that moves in the horizontal plane, allows for precise fabrication of parts and objects without contact. This process can be used for a variety of materials and can be used to create complex geometries with high accuracy and repeatability. The process is also highly efficient, as it does not require manual intervention and can be automated. Moreover, it does not generate any additional waste, is environmentally friendly and is an ideal solution for the fabrication of high-precision and complex parts in a cost-effective manner.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

While the LeviPrint system is a novel solution to fabricate parts in a fixed emplacement, it can also be used for additional applications shown during testing. These included building a model ship in a bottle by levitating the parts through the bottle's narrow opening. It also has the potential to be modified to work in liquids instead of air to build objects directly inside living tissue, opening up a host of medical applications.

This must me a noise nightmare for dog and other animals.

Have a story tip? Message me at: http://twitter.com/Cabe_Atwell

  • Sign in to reply
  • cstanton
    cstanton over 3 years ago

    I wondered when we'd start to see practical applications of this. People have managed to manipulate it such that it actually moves the objects while it hovers in the air, too.

    There're some keen limitations at present though.