Sensors
  • Technologies
  • More
Sensors
Blog Researchers Introduce Metalens Microscope for Medical Applications
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 10 Jun 2025 7:46 PM Date Created
  • Views 1946 views
  • Likes 4 likes
  • Comments 0 comments
  • research
  • on_campus
  • cabeatwell
  • university
  • medical
  • sensor
  • innovation
Related
Recommended

Researchers Introduce Metalens Microscope for Medical Applications

Catwell
Catwell
10 Jun 2025

image

The metalens-based microscope can address off-axis aberrations and achieve high-resolution wide-field imaging. (Image Credit: Tao Li and Jiacheng Sun (Nanjing University))

Optical technology could soon change thanks to the introduction of metalenses, which uses nanoscale structures to manipulate light at the subwavelength level. Their lightweight, compact, and ultra-thin design makes them ideal for modern electronics and portable imaging systems. However, metalenses haven't performed as well as traditional microscopes due to the trade-off between field of view (FOV) and resolutions, as well as off-axis aberrations. That could soon change. Researchers at Nanjing University in China developed a wide field of view metalens-based microscope capable of capturing high-resolution images for medical applications. The team believes medical professionals could use it outside laboratory settings without relying on bulky equipment.

To address the limitation, the team deployed a doublet metalense design, which consists of two metalenses placed on each side of a silica substrate combined with annular illumination. Both the metalenses are made of silicon nitride nano-fins, produced as high-aspect-ratio squares with precise dimensions and arranged at carefully calculated intervals. This configuration corrects common distortions and enhances resolution to optimize image performance.

"Our metalens microscope, featuring a FOV of up to 150 μm and a half-pitch-resolution of 310 nm, far exceeds the highest resolution ever reported in meta-microscopy," says corresponding author Dr. Tao Li.

image
The metalense microscope and its application in bio diagnostics. (Image Credit: SPIE Digital Library)

The team's 4 cm x 4 cm x 5 cm portable prototype can image tiny cellular features across a 150-micrometer field with a 310 nanometers resolution. It also achieved 1 mm FOV with a half-pitch resolution of 620 nm. With that capability, the team used the system to image changes in cervical cancer cells that are normally observed under larger laboratory microscopes. They imaged different stages of cancer development within the same FOV, revealing nuclear enlargement, deformation, and division. Medical professionals can improve diagnostic capabilities as it provides them with comprehensive images of tissue samples.

"Our experimental results demonstrate high-quality microscopic bioimages that are comparable to those obtained from traditional microscopes within a compact prototype, highlighting its potential applications in portable and convenient settings," says Li.

This technology could be practical for applications requiring portability and high-performance imaging in mobile monitoring, field research, and low-resource medical settings. It can also be integrated into microelectronic devices for emerging technologies, such as biomedical automation or state-of-the-art systems. The team's breakthrough, which combines performance with portability, leads to high-performance metadevices across optical applications.

Have a story tip? Message me at: http://twitter.com/Cabe_Atwell