Sensors
  • Technologies
  • More
Sensors
Sensor Forum Sensing Baby Kicks
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 350 subscribers
  • Views 2619 views
  • Users 0 members are here
  • ip_iot
Related

Sensing Baby Kicks

ipv1
ipv1 over 10 years ago

I have made a belt for sensing when our unborn child kicks from the inside. This is useful for tracking activity and health of the baby. In my current configuration, I am using a piezoelctric sensor strip but there are a few issues.

  1. The strip is small and cannot cover a large surface area.
  2. It will not discriminate between kicks and movement caused by the mother herself.


I was able to condition the signals and send them over BTLE but the sensor is an issue.

Can anyone suggest? Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • ipv1
    ipv1 over 10 years ago +3
    Interesting theories. Dough 's solution will need too much tweaking but will be a better one in the long run. Jan's solution has one issue- the cloth worn tightly will be uncomfortable over time. But I…
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to ipv1 +3
    In my defence, I'm going to suggest to buy stretching resistive cloth
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to Jan Cumps +3
    http://openmaterials.org/materials-101-electrotextiles/ Electrolycra from Mindsets : looks and feels like ordinary lycra but it’s highly conductive. Its conductivity in one direction depends on how tightly…
Parents
  • kholt62
    kholt62 over 7 years ago

    Were you able to figure this out? Sure would love to give it a try!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 7 years ago in reply to kholt62

    I would develop something like this is my wife was pregnant - maybe play some music as feedback for the baby. I have developed a soft belt with sensors that could be used for this. It was developed for physiotherapy applications, but it would easily sense and discriminate a baby kick.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • kholt62
    kholt62 over 7 years ago in reply to dougw

    Hi Douglas,

    I love the music idea. Could you share it with me? I have a lot of time on my hands right now. LOL

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 7 years ago in reply to kholt62

    Early learning is a fascinating topic. I have some very old memories of sensations from before I could talk. I cannot vocalize them well because I had no language to describe them, but some sensations trigger those memories.

    Lots of studies show that unborn babies respond to sounds and music, altering their activity or their heart rate. Some studies show that late in pregnancy babies can even recognize their mother's voice.

    Beyond just providing richer stimulation through audio, it would be interesting to provide information, in case it is possible for some level of learning. For example if they always hear "standing up" when the mom stands up or "lying down" when she lays down, maybe they would start to associate words with sensations they are actually experiencing.

    Or if they always hear "kick" when they kick, maybe they would associate with the action. It would be cool if you could say kick and the baby kicks in response.

    Of course the Mom could just talk to her baby, but acoustic coupling from air to a body is very inefficient and dramatically attenuated.

    I would use a surface driver like bone conduction headphones to provide audio at a low volume - it wouldn't require much volume to couple into n the womb, since the surface driver would directly vibrate the Mom's skin surface. The system could be used to talk to a baby more efficiently, or it could be used to provide automated feedback based on sensors such as a kick sensor or a tilt sensor.

    Many mothers have tried audio stimulation of their babies and some claim it is a critical part of early development, but it is wise to check out what is considered safe and what others' experiences have been.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 7 years ago in reply to kholt62

    Early learning is a fascinating topic. I have some very old memories of sensations from before I could talk. I cannot vocalize them well because I had no language to describe them, but some sensations trigger those memories.

    Lots of studies show that unborn babies respond to sounds and music, altering their activity or their heart rate. Some studies show that late in pregnancy babies can even recognize their mother's voice.

    Beyond just providing richer stimulation through audio, it would be interesting to provide information, in case it is possible for some level of learning. For example if they always hear "standing up" when the mom stands up or "lying down" when she lays down, maybe they would start to associate words with sensations they are actually experiencing.

    Or if they always hear "kick" when they kick, maybe they would associate with the action. It would be cool if you could say kick and the baby kicks in response.

    Of course the Mom could just talk to her baby, but acoustic coupling from air to a body is very inefficient and dramatically attenuated.

    I would use a surface driver like bone conduction headphones to provide audio at a low volume - it wouldn't require much volume to couple into n the womb, since the surface driver would directly vibrate the Mom's skin surface. The system could be used to talk to a baby more efficiently, or it could be used to provide automated feedback based on sensors such as a kick sensor or a tilt sensor.

    Many mothers have tried audio stimulation of their babies and some claim it is a critical part of early development, but it is wise to check out what is considered safe and what others' experiences have been.