Sensors
  • Technologies
  • More
Sensors
Sensor Forum Sensing Baby Kicks
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 350 subscribers
  • Views 2610 views
  • Users 0 members are here
  • ip_iot
Related

Sensing Baby Kicks

ipv1
ipv1 over 10 years ago

I have made a belt for sensing when our unborn child kicks from the inside. This is useful for tracking activity and health of the baby. In my current configuration, I am using a piezoelctric sensor strip but there are a few issues.

  1. The strip is small and cannot cover a large surface area.
  2. It will not discriminate between kicks and movement caused by the mother herself.


I was able to condition the signals and send them over BTLE but the sensor is an issue.

Can anyone suggest? Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • ipv1
    ipv1 over 10 years ago +3
    Interesting theories. Dough 's solution will need too much tweaking but will be a better one in the long run. Jan's solution has one issue- the cloth worn tightly will be uncomfortable over time. But I…
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to ipv1 +3
    In my defence, I'm going to suggest to buy stretching resistive cloth
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to Jan Cumps +3
    http://openmaterials.org/materials-101-electrotextiles/ Electrolycra from Mindsets : looks and feels like ordinary lycra but it’s highly conductive. Its conductivity in one direction depends on how tightly…
Parents
  • dougw
    dougw over 10 years ago

    Interesting sensor challenge.

    Assuming the kicks generate a different spectrum of accelerations than a movement, perhaps an accelerometer or microphone would provide an easier signal to analyze. (Low-cost Piezo sensors generally have a resonant frequency that make spectral analysis difficult)

    Another method might be to use a different sensor to detect when mother is moving and ignore the kick sensor at these times. This sensor would be mounted closer to her muscles and further from the baby. It could even use EMG sensors (electromyography).

    Doug

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 10 years ago

    Interesting sensor challenge.

    Assuming the kicks generate a different spectrum of accelerations than a movement, perhaps an accelerometer or microphone would provide an easier signal to analyze. (Low-cost Piezo sensors generally have a resonant frequency that make spectral analysis difficult)

    Another method might be to use a different sensor to detect when mother is moving and ignore the kick sensor at these times. This sensor would be mounted closer to her muscles and further from the baby. It could even use EMG sensors (electromyography).

    Doug