Sensors
  • Technologies
  • More
Sensors
Sensor Forum How to build in watertight ultrasonic transducer in a watertight box..
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 353 subscribers
  • Views 2665 views
  • Users 0 members are here
  • watertight
  • molding
  • range sensor
  • ultrasonics transducer
Related

How to build in watertight ultrasonic transducer in a watertight box..

alkrojen
alkrojen over 10 years ago

Hi fellow engineers

 

We have designed a range sensor by using this ultrasonics transducer

MCUSD18A40B12RS - MULTICOMP - TRANSCEIVER, 40KHZ, 18MM, METAL | Farnell element14 Danmark

as both a receiver and transmitter

It works fine on the PCB alone. But when we put the PCb into a plastic box, with  a hole matching the tip of the sensor, it no longer works

We  can make it work by cutting the hole bigger, so that the entire sensor is exposed. But then the box is no longer water tight..

 

The idea was that it should all be molded into the box, but this will also not be possible since this will require that the hole is tight

 

So my question is does anybody know how such a transducer is supposed to be installed in a box  and still work?

 

br.

Allan

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 10 years ago +1
    The problem with this kind of sensor is that the entire metal body is part of the resonant structure. They are widely used in car reversing systems so you can look at plenty of examples of how they are…
  • michaelkellett
    michaelkellett over 10 years ago

    The problem with this kind of sensor is that the entire metal body is part of the resonant structure. They are widely used in car reversing systems so you can look at plenty of examples of how they are mounted. The basic scheme is to use a soft rubber or silicone gasket or washer between the hard case and the sensor. The performance of the sensor is always affected so you need to make careful measurements and be sure that your production process is well controlled.

    The entire conical part of the sensor needs to protrude beyond the soft mounting.

     

    O rings are often too stiff and can give rise to a lot of short time-constant echoes which limit the shortest range you can measure.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • alkrojen
    alkrojen over 10 years ago in reply to michaelkellett

    Hi Michael

     

    Thanks  for your quick reply. Do you know where I can find such a gasket for the sensor?

    Have looked at Farnell but so far without success..

     

    br.

    Allan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 10 years ago in reply to alkrojen

    I've never found ready made ones - the easiest way for small numbers is to cast them from silcone rubber. Make sure you get a nice soft kind.

    For large numbers you will need to get them moulded specially.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • alkrojen
    alkrojen over 10 years ago in reply to michaelkellett

    I found this: new design 20khz ultrasonic transducer with red rubber case,China ultrasonic transducer Supplier & Manufacturer - Donggu…

    Is it such a rubber case you mean?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 10 years ago in reply to alkrojen

    That's the sort of thing but  a poor example since you would not be able to make it seal up to the main case very well.

     

    Better ones are more like grommets to deal onto the box but for full waterproofness you will need glue as well.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • coppermage
    coppermage over 10 years ago

    Mount the sensor over a 12mm hole so the wires will pass through. With the plastic box  use either 3M 4000UV (West Marine #3760204 or similar) or possibly  a Marine Silicone Seal (e.g. West Marine #542704 or similar) as a bedding compound/glue, and run wires from the back of the part  to your circuit board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • D_Hersey
    D_Hersey over 10 years ago

    If MK is right, which he is an insufferable amount of times*, you may get better reproducability by laser-cutting your gaskets out of sheet SiO2.  Don't try to laser anything with Cl.

     

    ==========

     

    *Like Groundskeeper Willie with a meter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • D_Hersey
    D_Hersey over 10 years ago

    https://www.youtube.com/watch?v=PvtQNSEJhns

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • midwestdeb
    midwestdeb over 10 years ago

    The way this is handled in the marine industry (200Khz transducers are used for depth sounders) is that the sensor is remote from the electronics. And the sensor is usually water-proof and comes with some type of mount. Not sure if this would work in your case... But see Simrad 200-35 as an example: Acoustic sensor / level / for boats / fishfinder - 200-35 - Simrad  They have a line of transducers - some for fish finders are broad dispersion, some are narrow beam and more suitable for depth-sounding and measuring the level in storage tanks. And I only use them as an example.

     

    You may be able to either use one of their transducers or at least see how they handled the problem of keeping saltwater away from electronics.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • midwestdeb
    midwestdeb over 10 years ago

    On a related note, there are conformal coatings that you can cover electronics in that make them waterproof. Not sure how this would impact your sensor.

     

    And some marine electronics are embedded in epoxy or other plastic - though heat can be a problem depending.