Sensors
  • Technologies
  • More
Sensors
Sensor Forum How to build in watertight ultrasonic transducer in a watertight box..
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 353 subscribers
  • Views 2669 views
  • Users 0 members are here
  • watertight
  • molding
  • range sensor
  • ultrasonics transducer
Related

How to build in watertight ultrasonic transducer in a watertight box..

alkrojen
alkrojen over 10 years ago

Hi fellow engineers

 

We have designed a range sensor by using this ultrasonics transducer

MCUSD18A40B12RS - MULTICOMP - TRANSCEIVER, 40KHZ, 18MM, METAL | Farnell element14 Danmark

as both a receiver and transmitter

It works fine on the PCB alone. But when we put the PCb into a plastic box, with  a hole matching the tip of the sensor, it no longer works

We  can make it work by cutting the hole bigger, so that the entire sensor is exposed. But then the box is no longer water tight..

 

The idea was that it should all be molded into the box, but this will also not be possible since this will require that the hole is tight

 

So my question is does anybody know how such a transducer is supposed to be installed in a box  and still work?

 

br.

Allan

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 10 years ago +1
    The problem with this kind of sensor is that the entire metal body is part of the resonant structure. They are widely used in car reversing systems so you can look at plenty of examples of how they are…
Parents
  • coppermage
    coppermage over 10 years ago

    Mount the sensor over a 12mm hole so the wires will pass through. With the plastic box  use either 3M 4000UV (West Marine #3760204 or similar) or possibly  a Marine Silicone Seal (e.g. West Marine #542704 or similar) as a bedding compound/glue, and run wires from the back of the part  to your circuit board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • coppermage
    coppermage over 10 years ago

    Mount the sensor over a 12mm hole so the wires will pass through. With the plastic box  use either 3M 4000UV (West Marine #3760204 or similar) or possibly  a Marine Silicone Seal (e.g. West Marine #542704 or similar) as a bedding compound/glue, and run wires from the back of the part  to your circuit board.