Sensors
  • Technologies
  • More
Sensors
Sensor Forum Sensor that can detect short range obstruction
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 352 subscribers
  • Views 2786 views
  • Users 0 members are here
  • motion sensor short range
Related

Sensor that can detect short range obstruction

e14 Contributor
e14 Contributor over 10 years ago

Hi Community,

 

I'm planning on a creating a device that would be helpful for blind people to detect short range obstruction from waist above that walking sticks can't. What type of motion sensor would be preferred for this situation? I also plan on connecting it to a raspberry pi device?

  • Sign in to reply
  • Cancel

Top Replies

  • waelect
    waelect over 10 years ago +1
    I saw a device made by some students for a final year project at Curtin University that used Ultrasonic. The application was suitable as they wanted it to be used as a walking stick but I can a few problems…
Parents
  • waelect
    waelect over 10 years ago

    I saw a device made by some students for a final year project at Curtin University that used Ultrasonic. The application was suitable as they wanted it to be used as a walking stick but I can a few problems for above the waist if it need to be wide angle.

     

    • There is plenty of Broadband IR noise from the sun so it may saturate the signal.
    • The Ultrasonic sensor is a better bet but is directional. How directional will end being how the sensor is read and a few things.

     

    Lot of testing to be done but I would steer toward Ultrasonic than IR. IR though is cheaper and easier to implement so it should not take long to see any bugs develop.

     

    Malcolm

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • waelect
    waelect over 10 years ago

    I saw a device made by some students for a final year project at Curtin University that used Ultrasonic. The application was suitable as they wanted it to be used as a walking stick but I can a few problems for above the waist if it need to be wide angle.

     

    • There is plenty of Broadband IR noise from the sun so it may saturate the signal.
    • The Ultrasonic sensor is a better bet but is directional. How directional will end being how the sensor is read and a few things.

     

    Lot of testing to be done but I would steer toward Ultrasonic than IR. IR though is cheaper and easier to implement so it should not take long to see any bugs develop.

     

    Malcolm