Sensors
  • Technologies
  • More
Sensors
Sensor Forum Sensor that can detect short range obstruction
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 352 subscribers
  • Views 2786 views
  • Users 0 members are here
  • motion sensor short range
Related

Sensor that can detect short range obstruction

e14 Contributor
e14 Contributor over 10 years ago

Hi Community,

 

I'm planning on a creating a device that would be helpful for blind people to detect short range obstruction from waist above that walking sticks can't. What type of motion sensor would be preferred for this situation? I also plan on connecting it to a raspberry pi device?

  • Sign in to reply
  • Cancel

Top Replies

  • waelect
    waelect over 10 years ago +1
    I saw a device made by some students for a final year project at Curtin University that used Ultrasonic. The application was suitable as they wanted it to be used as a walking stick but I can a few problems…
  • gadget.iom
    gadget.iom over 10 years ago

    Have you looked at any sensors so far?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to gadget.iom

    I"m thinking of using an PIR or Ultrasonic motion sensor

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • waelect
    waelect over 10 years ago

    I saw a device made by some students for a final year project at Curtin University that used Ultrasonic. The application was suitable as they wanted it to be used as a walking stick but I can a few problems for above the waist if it need to be wide angle.

     

    • There is plenty of Broadband IR noise from the sun so it may saturate the signal.
    • The Ultrasonic sensor is a better bet but is directional. How directional will end being how the sensor is read and a few things.

     

    Lot of testing to be done but I would steer toward Ultrasonic than IR. IR though is cheaper and easier to implement so it should not take long to see any bugs develop.

     

    Malcolm

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mconners
    mconners over 10 years ago

    Hey, I did a couple of posts on using ultrasonic and pir sensors with the Ras Pi in the stem section, you can check them out here:

     

    PIR-fect

    Ping))) Me!!!

     

     

    they're just basic examples of how to use them, but they are simple devices.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 10 years ago

    Check out Maxbotix sensors - they have a selection of sensors with different beam angles.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    I am doing project to detect obstacles in front of visually impaired persons and warn them via audio output through ear phones (warn them the distance and position say left,right etc of the obstacle in front of them). I found MULTICOMP  MCUSD16P40B12ROMCUSD16P40B12RO TRANSCEIVER suitable I also found MA40S4R/S suitable But I donot know how to use MULTICOMP  MCUSD16P40B12ROMCUSD16P40B12RO TRANSCEIVER to measure distance of obstacle Please reply if anyone knows how to measure distance using MULTICOMP  MCUSD16P40B12ROMCUSD16P40B12RO TRANSCEIVER

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to dougw

    But Maxbotix sensor are costly starting from $30. I found MULTICOMP  MCUSD16P40B12ROMCUSD16P40B12RO TRANSCEIVER can be used But I donot know what are two pins of MULTICOMP  MCUSD16P40B12ROMCUSD16P40B12RO TRANSCEIVER And how to trigger it

    I mean how to use MULTICOMP  MCUSD16P40B12ROMCUSD16P40B12RO TRANSCEIVER to measure distance?

    MULTICOMP  MCUSD16P40B12ROMCUSD16P40B12RO TRANSCEIVER costs just$6

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hi,

     

    An ultrasonic sensor should do your work at the primary level.

     

    Also, you may set range for the ultrasonic sensor so that it will work only for the short range (say, 1-5 metres).

     

    Do let me know of your progress.

     

    Akhil kapoor

    http://www.25robot.com/2015/04/getting-started-with-robotics.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    Yes ultrasonic sensor will be suitable. I found MULTICOMP  MCUSD16P40B12ROMCUSD16P40B12RO TRANSCEIVER is an ultrasonic sensor that is very compact has a wide beam angle It has only two pins But I cant find information on how touse MULTICOMP  MCUSD16P40B12ROMCUSD16P40B12RO TRANSCEIVER to measure distance Can you tell how to measure distance using it The circuit and concept

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    Okay.

     

    Did you do the right search using different keywords on the web ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>