Sensors
  • Technologies
  • More
Sensors
Sensor Forum Do you have a question on MEMS Sensors? Ask our Expert, Donna Sandfox
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 73 replies
  • Subscribers 353 subscribers
  • Views 10016 views
  • Users 0 members are here
  • products
  • Mechanical
  • components
  • photomicrosensors
  • sensors
  • expert
  • support
  • omron
  • mems
  • engineering
  • rf
  • switch
  • answers
  • mass_flow
  • vibration
  • question
Related

Do you have a question on MEMS Sensors? Ask our Expert, Donna Sandfox

e14 Contributor
e14 Contributor over 15 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Sensors in the element14 Community Sensors group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community

image

Donna Sandfox

Donna Sandfox is the Product Manager for Sensors and MEMS Products for Omron Electronic Components LLC.  Her primary area of expertise is in MEMS Mass Flow Sensors.  She also supports Omron’s pressure, thermal IR, tilt/vibration and optical (photomicrosensors) sensors, as well as their RF MEMS Switch products.  Donna received her bachelor’s degree in mechanical engineering from Southern Illinois University and an MBA from Roosevelt University.


 


  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 15 years ago in reply to DAB +1
    Hi Don! Thank you, and thanks for the question. While volumes can be written comparing and contrasting all of the different technologies available for measuring gas flow, I'll try to give a reasonably…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to vsluiter +1
    Hello, Thanks for your reply. The problem has now been solved. There was an error in the catalogue which has now been corrected. The correct sensors are with me and ready for test in my project. Thanks…
Parents
  • DAB
    DAB over 15 years ago

    Hi Donna,

     

    Welcome to Element14.

    I know I've been lazy in not researching this myself, but could you explain why the MEMS approach is considered better than existing sensor technology?

    Everyone is talking like its the next best thing since the IPAD, so I am curious where the hype is coming from and what the true merits to the technology might be.

     

    Thanks,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to DAB

    Hi Don!

    Thank you, and thanks for the question.  While volumes can be written comparing and contrasting all of the different technologies available for measuring gas flow, I'll try to give a reasonably brief answer by limiting it to non-MEMS thermally based mass flow measurement.

     

    MEMS mass flow sensors are constructed of two sets of thermopiles with a heater between them.  Each thermopile set is comprised of several very small (obviously) thermocouples connected in series.  This design makes the MEMS mass flow chip very sensitive compared to a single set of thermocouples (< 1cm/sec can be measured).  The MEMS chip also has a very fast response time (<5 msec) and low power consumption.

     

    Omron's MEMS chip employs deep top-etching and dielectric thin layer deposition manufacturing techniques resulting in a high surface area to volume ratio, further improving sensitivity. 

     

    Sometimes seeing is easier than reading; if you'd like to see some graphical representation of what I've described above we have a Product Training Module on our website at:  http://www.components.omron.com/components/web/webfiles.nsf/PTM.html.

     

    One final note, when constructing a flow sensor... The MEMS chip (or other basic measurement technology) is important, but also are the supporting circuitry (for signal processing and temperature compensation) and the physical design of the flow path (a solid understanding of fluid dynamics is required to ensure good flow characteristics for accurate measurement results).

     

    Hope this was helpful!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to DAB

    Hi Don!

    Thank you, and thanks for the question.  While volumes can be written comparing and contrasting all of the different technologies available for measuring gas flow, I'll try to give a reasonably brief answer by limiting it to non-MEMS thermally based mass flow measurement.

     

    MEMS mass flow sensors are constructed of two sets of thermopiles with a heater between them.  Each thermopile set is comprised of several very small (obviously) thermocouples connected in series.  This design makes the MEMS mass flow chip very sensitive compared to a single set of thermocouples (< 1cm/sec can be measured).  The MEMS chip also has a very fast response time (<5 msec) and low power consumption.

     

    Omron's MEMS chip employs deep top-etching and dielectric thin layer deposition manufacturing techniques resulting in a high surface area to volume ratio, further improving sensitivity. 

     

    Sometimes seeing is easier than reading; if you'd like to see some graphical representation of what I've described above we have a Product Training Module on our website at:  http://www.components.omron.com/components/web/webfiles.nsf/PTM.html.

     

    One final note, when constructing a flow sensor... The MEMS chip (or other basic measurement technology) is important, but also are the supporting circuitry (for signal processing and temperature compensation) and the physical design of the flow path (a solid understanding of fluid dynamics is required to ensure good flow characteristics for accurate measurement results).

     

    Hope this was helpful!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • DAB
    DAB over 15 years ago in reply to e14 Contributor

    Hi Donna,

     

    Thanks for the website direction.  I will spend some time getting educated, but I appreciate your quick response.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hello Donna

                            This is vamshi from india,persuing my graduation we are working on a project based on brain signals,will u please suggest any sensors that can capture and conver them to voltages so that each different thought will  work as input to microcontroller.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Wow, I don't have any idea on that one!

    Anyone else out there want to take a shot at this question??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 14 years ago in reply to e14 Contributor

    Hi Vamshi,

     

    Look at the headset called MindWave from Neurosky.  It is reusable and comes with its own software.

    I just ordered one last week for about 110 USD.  I look forward to its delivery.

     

    Hope this helps.

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to DAB

    Hello sir this is vamshi from india we are doing project for disabled people, our project title is"Thoughts into action " is based on moving wheel chair without anyone's help, thoughts in your mind will controle the wheelchair to move forward,backward,turn left and turn right.

    I need your technical assistance sir we are about to do work on MSP430F MicroController series sir,and devise to recieve signals from brain to give input to MC. Sir i need to talk to you sir if you are free please make a call at +918686260302

     

     

    Thanking you in anticipation sir.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 14 years ago in reply to e14 Contributor

    Hi Vamshi,

     

    The time difference between the US and India make phone calls difficult. Please ask your questions via email and I may be able to help.

    You might also contact your local Texas Instruments supplier for information.

     

    Thanks

    DAB