Sensors
  • Technologies
  • More
Sensors
Sensor Forum Rough environment rotation speed sensor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 354 subscribers
  • Views 1753 views
  • Users 0 members are here
Related

Rough environment rotation speed sensor

e14 Contributor
e14 Contributor over 11 years ago

Hello altogether,

 

I want to measure the rotation speed of a auxiliary fan which is enclosed in a duct pipe system.

There will be humidity and steam from boiling water (can compare to cooking on a gas hob in the kitchen)

 

The fan blades are made of plastic.

 

I was recommended to use an optical sensor, but I am worried that the steam will interfere.

 

Has anybody experience with something like this and can recommend a certain type of sensor or maybe even a special product?

 

Thanks guys!

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 11 years ago in reply to gadget.iom +2
    I am worried that the steam will interfere If the pipe is that full of steam, I think the plastic blades will be the biggest issue. Many of the sensors use IR and work at very close distances. You might…
  • tekmeister
    tekmeister over 11 years ago +1
    Optical might work, but I'd be looking at using a laser. Any chance you can swap the fan motor out to one that provides feedback via a 3rd wire?
  • tekmeister
    tekmeister over 11 years ago in reply to gadget.iom +1
    I was going to mention hall effect sensors. The reason I went with reed switches was because they operate over a wider temperature range, but I suppose for steam (~100 degrees C) hall effect will be fine…
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    Thanks to all of you for the feedback.

     

    I have a device called "Duct Blaster" http://products.energyconservatory.com/minneapolis-duct-blaster-system/

     

    It is used to measure pressure/airflow within a system. (They sell for determination of leakage in housing ventilation systems)

     

    Their meters are set to standard ambient conditions 20ºC, 1013.25hPa

    As I use the Duct blaster to measure the air movement of a hot airflow, the density will change. Hence I need to work out a corrective factor for the indicated airflow.

     

    It is quite easy for the temperature and the barometric pressure, but the steam (vapor and condensate) will effect the density as well.

     

    By knowing the rotation speed of the blades, I can calculate the real airflow without any corrective factors.

    (N1/N2) = (D1/D2)-3 (Q1/Q2)

    D = Fan size

    N = Rotational speed

    P = Pressure

    Q = Volume flow rate 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 11 years ago in reply to e14 Contributor

    Have you considered using a small microphone and using the sound to determine fan speed?

     

    You should get a measurable difference when the fan blade passes by the mic, which would allow you to directly measure the fan speed.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • DAB
    DAB over 11 years ago in reply to e14 Contributor

    Have you considered using a small microphone and using the sound to determine fan speed?

     

    You should get a measurable difference when the fan blade passes by the mic, which would allow you to directly measure the fan speed.

     

    DAB