Sensors
  • Technologies
  • More
Sensors
Sensor Forum Rough environment rotation speed sensor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 354 subscribers
  • Views 1748 views
  • Users 0 members are here
Related

Rough environment rotation speed sensor

e14 Contributor
e14 Contributor over 11 years ago

Hello altogether,

 

I want to measure the rotation speed of a auxiliary fan which is enclosed in a duct pipe system.

There will be humidity and steam from boiling water (can compare to cooking on a gas hob in the kitchen)

 

The fan blades are made of plastic.

 

I was recommended to use an optical sensor, but I am worried that the steam will interfere.

 

Has anybody experience with something like this and can recommend a certain type of sensor or maybe even a special product?

 

Thanks guys!

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 11 years ago in reply to gadget.iom +2
    I am worried that the steam will interfere If the pipe is that full of steam, I think the plastic blades will be the biggest issue. Many of the sensors use IR and work at very close distances. You might…
  • tekmeister
    tekmeister over 11 years ago +1
    Optical might work, but I'd be looking at using a laser. Any chance you can swap the fan motor out to one that provides feedback via a 3rd wire?
  • tekmeister
    tekmeister over 11 years ago in reply to gadget.iom +1
    I was going to mention hall effect sensors. The reason I went with reed switches was because they operate over a wider temperature range, but I suppose for steam (~100 degrees C) hall effect will be fine…
Parents
  • kas.lewis
    kas.lewis over 11 years ago

    Sounds like something that the TI LAUNCHXL-F28027F LaunchPad with the BOOSTXL-DRV8301 Motor Drive BoosterPack may be able to solve. TI seems to say this setup can be used to measure the position of a motor without the need of any external sensors. Would be intresting to see if this really does work, good luck.

     

    Kas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 11 years ago in reply to kas.lewis

    Hi Kas,

     

    Yes the TI board has the ability to self measure the stator position using the EMF on the coils.

     

    TI uses this information to control the current into the wires to rapidly spin the motor and control the speed.

     

    I think this technology only works with the new Brushless motors though.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • DAB
    DAB over 11 years ago in reply to kas.lewis

    Hi Kas,

     

    Yes the TI board has the ability to self measure the stator position using the EMF on the coils.

     

    TI uses this information to control the current into the wires to rapidly spin the motor and control the speed.

     

    I think this technology only works with the new Brushless motors though.

     

    DAB