Sensors
  • Technologies
  • More
Sensors
Sensor Forum Pressure sensor analog output does not make sense.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 351 subscribers
  • Views 2967 views
  • Users 0 members are here
  • waveform
  • pressure
  • output
  • tscdann150pgucv
  • honeywell
  • analog
  • sensor
Related

Pressure sensor analog output does not make sense.

e14 Contributor
e14 Contributor over 11 years ago

Good day,

 

I purchased Honeywell  TSCDANN150PGUCVTSCDANN150PGUCV pressure sensor few days ago

(link: https://my.element14.com/webapp/wcs/stores/servlet/ProductDisplay?catalogId=15001&langId=83&storeId=10188&krypto=xMs4olW0ElyxVaI%2FiD7ayZ5miUzDDbUiA%2F7psz4Sm5%2BmDjc2R3PzNnQmGmmZzO4WoRArmd0pQrtS%0Aw%2F8ti98Qrw%3D%3D&ddkey=http%3ALogoff)

 

I connected the output+ and output- to the oscilloscope to see the output waveform. Unfortunately, what I observe is just some noise. And then, I realise that the output is too small. And according to its datasheet, amplifier circuit is needed. So, I added the circuit to amplify the output. However, with no luck, the output is just does not make any sense.

 

Therefore, I hope that someone experienced can help me with this two question:

1. Is the analog output differential or single ended after the amplification? (Well, initially I thought was differential because it has both Vout+ and Vout- pins, but just want to be sure)

2. If anyone use this particular sensor before, what is the analog output in term of voltage? How many times (or gain) does the amplifier circuit need to set?

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 11 years ago

    According to link you gave, you got a TSC, not a NSC series. So you measure differential or gauged, but not absolute. Did you solder it or breadboard it? What voltage at Vsupply are you using? Can you describe the application in more detail like what medium type used air or liquid? Picture of what you have? The data sheet is quite detailed if you follow it carefully. Possibly the voltage is noisy and that could be problem with output since the device is extremely accurate.

    See below table to setup the device correctly:

    • Differential Output is proportional to the difference between the pressures applied to each port (Port 1 – Port 2).
    • Gage Output is proportional to the difference between applied pressure and atmospheric (ambient) pressure

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    Initially, I thought that the output of the sensor is AC since it has both Vout+ and Vout- but end up it is DC analog output. It make sense now. Thank you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    Most sensors I have seen are DC because easier to use and fits the MCU environment. The dataset is under documents for the link you set above. Would be curious what you plan to do with this project.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    I am doing a pressure detector, that will warn the user when the pressure exceed certain level.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    I am doing a pressure detector, that will warn the user when the pressure exceed certain level.