Sensors
  • Technologies
  • More
Sensors
Sensor Forum Hydroponic system nutrient sensors help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 21 replies
  • Answers 15 answers
  • Subscribers 361 subscribers
  • Views 7692 views
  • Users 0 members are here
Related

Hydroponic system nutrient sensors help

xan326
xan326 over 13 years ago

Hi all, I'm going to be building a hydroponic system soon being controlled and monitored by a board (most likely beaglebone). But I need help with finding sensors and connecting them, I have literally no idea what connect tivity any boards have (rasberry pi, arduino, beaglebone/beagleboard, atmel) and if they're just USB, then finding a way to convert connections to usb. But I'll get into that later.

The sensors I need are:

Dissolved Oxygen

Hydrogen

Carbon

Nitrogen

Potassium

Phosphorus

Calcium

Magnesium

Sulfur

Boron

Chlorine

Copper

Iron

Molybdenum

Manganese

Zinc

Nickel

Sodium

Cobalt

Selenium

Silicon

Then PH and Flow rate sensors

 

Anyways, if anyone knows of any place to get these sensors please tell me or post a link. Also if they're not natively USB, explain a way (or post a link to an article) on how to convert the connection to usb.

Thanks to everyone that will help! This is my first project using any of the boards like beagle or arduino.

 

Also does anyone know of any pumps; both air and water; that can be run from one of the boards?

  • Sign in to reply
  • Cancel

Top Replies

  • davewr
    davewr over 13 years ago in reply to xan326 +1 suggested
    Just one more note -- if you consider the question answered - mark it as answered as a courtesy to me and to everyone reading the thread. If you have more questions start a new thread with specific questions…
  • aphexfx
    0 aphexfx over 12 years ago in reply to dlmz06

    Hey OP are you still working on this project?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I have a lot of experience in Hydroponics, I have designed hydroponic solutions from the ground up and done testing on them. Daniel is right you dont need to monitor everything you have listed. You have listed all the major components was well as all the micro-nutrients needed to maintain the plants. All you have to do is monitor the PH and TDS in solution and simply flush and re-new as needed.

     

    However, if you are trying to monitor an experiment and determine the uptake of given nutrients within solution so you can simply add back what was removed. You are looking for a spectrophotometer which you would need to make and interface to any of the micro-controllers. You would use it to do Absorption spectroscopy on the solution. Samples could be diverted from the main flow line into a secondary line for testing then released back into the main flow line after the test. Most spectrophotometers use a cuvette for sample preparation. These tend to be plastic but in the case of UV spectroscopy they are quartz. You would have to look up each of the chemicals you list and determine what spectrum they absorb. You would also need to make sure that the sample test area is made of a material that will not absorb the spectrum you are trying to identify. If any of them are in the UV spectrum then you will need to use quartz at the sample point and the design gets much more complicated.

     

    None of this is easy or simple, I would suggest that you stick to the standard PH/TDS tests unless you are up for a challenge. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Problemchild
    0 Problemchild over 12 years ago in reply to davewr

    I must agree with what David says here. The sensors are similar for Ponds/Hydroponics/Aquaponics etc.

     

    If you want to test for a specific  compound or ion you need to do the chemical test for it using the reagents as David stated. Most are designed then to change colours for a colour sensor to pick up. The tests can be automated using some kind of dosing kit to introduce an amount of reagent into a test vessel.

    Probably more useful is to use the sensors that measure directly for dissolved O2, pH,TDS etc(I believe the NH3 sensor is reasonable too). All these are quite expensive (in the 10's-100's) depending on the particular sensor and how scientific you want to be.

     

    Good luck with your project ... John A

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • kidiccurus
    0 kidiccurus over 12 years ago

    Seems no one has talked about actually interfacing the sensors with USB so I will try and cover that here. All of the boards you have described can use gpio pins to read sensors, often through i2c. Converting a sensor to usb is not generally desirable unless the final device is a usb connected sensor. Personal recommendation is arduino. It can interface with most things. It can also read analogue values which if often helpful for cheaper sensors. The only reason to use beaglebone or pi is if you want a computer interface or web connectivity, otherwise arduino is cheaper. You also get more gpio per pound (or dollar or euro or yen) with arduino. When you find your sensor I can help you use it correctly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Problemchild
    0 Problemchild over 10 years ago in reply to davewr

    I must say that we've looked in to this before for a friend and found in practice  you do not need to measure continuously nothing happens that fast although you do need to keep a regimen of just how often and running around a small out fit with a TDS truncheon generally isnt often enough.

     

    I think the problem is that if you are making it operate automatically and on a small scale you will find it awkward to dip in say a PH or TDS meter yet they do get contaminated overtime so you cant really leave them in solution. The indirect method via colour change reagents gets past this at the expense of requiring some dosing equipment and way of extracting a sample.. all very awkward to do reliably for a cheap price!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • czaleu
    0 czaleu over 10 years ago

    Hello Good day sir, I'm actually a engineering student. Electronics Engineering to be precised. Sir i would like to ask if your project is done? because I was really amaze about the concept and would like to try it out. Specifically on the part of the availability of the sensors.

     

    I am finding a way to have a sensor for the following elements on the water:

    - Nitrogen

    - Phosphorus

    - Potassium

     

    I'll be gladly be grateful for your response.

    Very much needed.

     

    Thank you for your support and Godspeed.

     

     

    P.s.

    This would be my email: zaleucenas@gmail.com

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michael.webb@csiro.au
    0 michael.webb@csiro.au over 10 years ago in reply to czaleu

    @

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michael.webb@csiro.au
    0 michael.webb@csiro.au over 10 years ago in reply to xan326

    Hi Xander,

    You may want to look at the following reference:

    Webb MJ (1993) A multichannel pH controller for solution culture systems. Plant and Soil, 155/156: 501-504.

    It describes a multichannel system for monitoring and adjusting pH in six separate hydroponics systems, hourly. The  Orion meter had seven channels which could be switched using a command from a computer. You will note the date, 1993, so yes old technology by today's standard (eg RS232 communications !); but the principles are the same.

    Equally, this Orion system could be connected to different ion-selective electrodes and an electrical conductivity probe inserted into one hydroponics system. It has been a while since I have been involved with hydroponics, but apart from pH (which is a hydrogen ion selective electrode), I think there have been developments in other ion-selective electrode ( eg Ca2+, K+, NO3-, NH4+ ) . Note that these measure nutrient in there ionic form, So nitrogen is measured as both nitrate and ammonium ions, Phosphorus, if a probe exists, would be measured as phosphate (the form and valency will depend on the pH); but this doesn't matter as it is the ionic form that is taken up by plant roots.

    Note that pH affects the uptake of phosphate (see Webb MJ and Loneragan JF (1985). The importance of environmental pH during root development on phosphate absorption. Plant Physiol., 79: 143-8.)

    I am not aware of any probes for the micronutrients; but as other have mention, you generally will not need to worry too much about these between solution changes. However, it is possible to control the 'activity' of the metal micronutrients such that the activity is near-constant. It is the 'activity' that the plant roots 'see' rather than the concentration (see Webb MJ, Norvell WA, Welch RM, Graham RD (1993). Using a chelate-buffered nutrient solution to establish the critical solution activity of Mn2+ required by barley (Hordeum vulgare L.). Plant Soil, 153:195-205).

    You will need to be careful with boron as the range between deficiency and toxicity is quite narrow.

     

    If the solution is constantly aerated, you will not need to monitor O2, and CO2 will be purged.

     

    I hope this helps.

    Cheers

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • nightparrot
    0 nightparrot over 9 years ago

    I know this is several years old but found this today Libelium Smart Water Sensor Platform Adds Ion Monitoring

     

    Not sure the price but probably several hundred $s.

     

    And if you search thru their pages they have something about the lowran and connecting via Pi, beagle, etc

     

    Place to buy the board and probes:  https://www.cooking-hacks.com/smart-water-ions-sensor-board

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • smanand
    0 smanand over 9 years ago

    Dear All,

    Im new to aquaponics, hydroponics. i understand the content in the water is critical for both.

     

    Thanks to Xander Zoolander, i was thinking of the same problem ,

    I also acknowledge other experts in the field who says real time monitoring is not required.

     

    Having said that, i would appreciate experts comments on my view(im probably, over excited and optimistic that there is a way out)

     

    The reason i believe a real time monitoring will help

    1. Measure the effect of feeding fish, will help me know quantity and interval of the feed. ex. after feeding the fish , in the next few hours if i know the quality of water. i would know how much minerals in the water, will help me do course correction on day 1. i believe this will help me save time.

    2. effect of environment on the quality of water.

    3. know when to take action instead of waiting for an 'event' to occur.

    4. Will help me decide if i have to increase or decrease the no of fish or plants. currently i have a ballpark figure, which may not be real for my environment.

     

    currently, these are learned over time by trial and error. takes months to get it perfect.

    my objective is not to have an automated system but to have total control of the system.

     

    I also checked Libelium Smart Water Sensor, how reliable it is? does it solve the problem?.. im not looking at the price at this moment.

     

    Would appreciate any feedback.

    Thank in advance

    anand

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<>