Sensors
  • Technologies
  • More
Sensors
Sensor Forum Can Gyroscopes/Accelerometers still be useful under constant vibration?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 350 subscribers
  • Views 852 views
  • Users 0 members are here
  • accelerometer;gyroscope;vibration;
Related

Can Gyroscopes/Accelerometers still be useful under constant vibration?

e14 Contributor
e14 Contributor over 13 years ago

I'm involved in a project which requires me to measure as many facets of the tattoo process as I possibly can. I'm wondering if any gyroscope/accelerometer measurements would be trashed by the constant vibration, or can I mitigate those effects with a creative algorithm? Would one be better suited than the other, or should I use both in tandem? I don't need super-precise positional information, but it would be great to see the difference between a vertical and horizontally held needle, as well as the transitions between.

 

I have no experience whatsoever with gyroscopes or accelerometers. I'll probably test it out with some breakout board regardless of the feedback, but would really appreciate any informed opinion on the matter.

 

Thanks!

  • Sign in to reply
  • Cancel
  • michaelkellett
    0 michaelkellett over 13 years ago

    By all means give it a try but you are right to be worried about the vibration.

    If you try to measure small low frequency signals from a sensor which is also subject to high levels of higher frequency stimulation (any sensor not just accelerometers and gyros) then you must at least make sure that the sensor stays within it's linear range.

     

    Sometimes HF noise (random or periodic) is actually beneficial so long as you can filter it out again - example are dithering (used to help mitigate quantising effects) and HF bias used with magnetic tape recorders.

     

    I suspect that accelerometers will be more tolerant of high levels of out of band vibration than gyros (because the gyros rely on vibrating structures inside to work) but I haven't tested this.

     

    You would be able to use an accelerometer with perhaps a +/- 2g range if there were no vibraion but one with a bigger range might give better results overall in your application.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • DAB
    0 DAB over 13 years ago

    I agree with Mike,

     

    You can always filter out the vibration.  If you use another sensor that picks up the vibration, you can use an Op Amp to feed the inverted vibration onto your accelerometer inputs to get a cleaner signal.

     

    You usually need to integrate the accelerometer data to get changes in velocity and position, so you just need to isolate the error induced by the vibration.

    This is a common problem on airframes as they fly through buffeting winds.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to michaelkellett

    Thanks! I'm far more confident now knowing the physics of the process aren't hopeless. I'll probably end up testing both an accelerometer and gyroscope just to see what I can see.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • vsluiter
    0 vsluiter over 13 years ago

    Hello Streuzucker,

     

    First, let's get your requirements straight; you ask for positional information, AND about whether the needle is horizontal or vertical. The first is position, the latter orientation (angle of object with respect to fixed world).

    Getting position requires you to set a 'zero' point, after which you have to integrate an accelerometer twice (first integration gives velocity, second integration gives position). However, this will drift tremendously, especially if your vibration causes higher frequencies than what your sample rate can cover.

    Getting orientation is mostly done by integrating the gyroscope once and/or using the accelerometer to find the angle with respect to the gravity vector. Finding gravity vector works fine for slow movements, and you could filter out the vibrations if you're only interested in low speed movements.

    Finally, I'd like to suggest two options for you if you're interested in orientation:

    • look into RC (Radio Control) groups, as a lot of people there use orientation sensing by MEMS sensors, using various filters with differing complexity
    • Have a look at the MPU9150, which is a Gyro / Accelero / Magneto combisensor. In Germany it's distributed by Scantec. There's arduino code available to get orientation output
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to vsluiter

    Thank you for the reply. My requirements are vague, that's true. Maybe I can explain myself a bit better.

     

    The concept behind the project is to measure everything I can about the tattoo process, then use those metrics to create some secondary visual art (primary being the tattoo itself). So I wouldn't exactly use the accelerometer/gyroscope data for the pinpoint telemetry. I'm mostly interested in getting a few stable data sources that I can map to some aspect of the visual output. For example, I could use processed values from a 3-axis gyroscope to inform the RGB values of the shape I'm currently coloring.

     

    So in that respect, I have a lot of slack when it comes to things like calibration and drift since my final output is going to be more or less arbitrary anyway.

     

    And thanks for the part recommendation! I was looking at the MPU9150 last night, it seemed like it fit my needs perfectly. And now that you've seconded the nomination, I think I'll pull the trigger and get one!