Sensors
  • Technologies
  • More
Sensors
Sensor Forum Can Gyroscopes/Accelerometers still be useful under constant vibration?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 350 subscribers
  • Views 854 views
  • Users 0 members are here
  • accelerometer;gyroscope;vibration;
Related

Can Gyroscopes/Accelerometers still be useful under constant vibration?

e14 Contributor
e14 Contributor over 13 years ago

I'm involved in a project which requires me to measure as many facets of the tattoo process as I possibly can. I'm wondering if any gyroscope/accelerometer measurements would be trashed by the constant vibration, or can I mitigate those effects with a creative algorithm? Would one be better suited than the other, or should I use both in tandem? I don't need super-precise positional information, but it would be great to see the difference between a vertical and horizontally held needle, as well as the transitions between.

 

I have no experience whatsoever with gyroscopes or accelerometers. I'll probably test it out with some breakout board regardless of the feedback, but would really appreciate any informed opinion on the matter.

 

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    0 michaelkellett over 13 years ago

    By all means give it a try but you are right to be worried about the vibration.

    If you try to measure small low frequency signals from a sensor which is also subject to high levels of higher frequency stimulation (any sensor not just accelerometers and gyros) then you must at least make sure that the sensor stays within it's linear range.

     

    Sometimes HF noise (random or periodic) is actually beneficial so long as you can filter it out again - example are dithering (used to help mitigate quantising effects) and HF bias used with magnetic tape recorders.

     

    I suspect that accelerometers will be more tolerant of high levels of out of band vibration than gyros (because the gyros rely on vibrating structures inside to work) but I haven't tested this.

     

    You would be able to use an accelerometer with perhaps a +/- 2g range if there were no vibraion but one with a bigger range might give better results overall in your application.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to michaelkellett

    Thanks! I'm far more confident now knowing the physics of the process aren't hopeless. I'll probably end up testing both an accelerometer and gyroscope just to see what I can see.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to michaelkellett

    Thanks! I'm far more confident now knowing the physics of the process aren't hopeless. I'll probably end up testing both an accelerometer and gyroscope just to see what I can see.