Sensors
  • Technologies
  • More
Sensors
Sensor Forum How to use pressure sensor (Honeywell NBPMLNN060PGUNV)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 351 subscribers
  • Views 1376 views
  • Users 0 members are here
Related

How to use pressure sensor (Honeywell NBPMLNN060PGUNV)

e14 Contributor
e14 Contributor over 13 years ago

I have acquired a 0-60psi pressure sensor, namely the NBPMLNN060PGUNV (nr. 2146011 from Farnell).

According to the datasheet sensitivity of the device should typically be 21mV/V/Full range. Essentially I figured that I would be able to get a ~100mV output

difference from the device - if connected to a 5V supply - measured between pins 2 and 4 (21mV * 5V = 105mV).

But when I connect the sensor to the supply, the output voltage is only 4mV, and decreasing when I increase the pressure.

When output voltage reaches 0, nothing else happens even if I increase the pressure further. Needless to say, this behaviour seems a bit peculiar to me.

 

Can anyone verify if this behaviour is correct? Because sensing on a voltage of only 4mV or less is rather difficult in my application.

 

For testing purposes, if I up the supply voltage to 10V, the output voltage also doubles (~9mV). But it is still a very small voltage difference to work with.

Am I doing something wrong or do I need to add a differential amplifier circuit to get higher voltage differences?

 

Thank you for your time.


Regards,

David Larsen

AKJ Inventions ApS.

  • Sign in to reply
  • Cancel
  • vsluiter
    0 vsluiter over 13 years ago

    Hello David,

     

     

    Please bear in mind that you've bought the NBP....060PGversion, which gives the difference between measured and surrounding atmospheric pressure (see datasheet page 5, top of page) . The NBP...060PAversion gives absolute pressure. That at least clarifies why you see no output when you're not applying pressure at all.  The output pressure you see is probably the offset (+/-7mV/V maximum).

     

     

    The only thing that puzzles me is that the output voltage decreases with increasing pressure.... 

     

     

    Good luck,

     

    Victor

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to vsluiter

    Hello Victor,

     

    thank you for your reply. Yes, the "offset"/error does seem reasonable as you mention.

    I did purposefully purchase the *PG-version, in order to avoid problems caused by surrounding pressure differences.

     

    But as you point out, the decrease in voltage is rather mysterious.

     

    Thanks,

    David.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Nobody out there seen this kind of behaviour before?

     

    Or for that matter have been using this type fo device?

     

    I'll take any experience, as it might just suggest a way for me to get the device working.

    (Anything in the order of "Never use un-loaded" is appreciated as well, seeing how something has to be a miss in my way of using the device.  - Assuming it is working properly of course).

     

    Thanks,

    David.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • vsluiter
    0 vsluiter over 13 years ago in reply to e14 Contributor

    Have you tried what it does when you make vacuum? Does the voltage go up then? Any chance the voltage goes up with decreasing pressure? Just a thought, I hope others have more useful hints / tips.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 13 years ago in reply to vsluiter

    I was wondering if you had mis-identified the pins but if you did I would expect the offset to be about 1/3 of the excitation voltage.

    What is the voltage between the output pins and ground ? (I expect 1/2 the excitation voltage).

    I wonder if you just have  a faulty sensor ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi guys, sorry for the late reply.

     

    Thank you very much for your input!

    I made sure all connections were correct and then I tested the vacuum response. It also decreased when changing the pressure.

    So obviously something was wrong.

     

    It contacted the manufacturer, but due to no response (partly causing the long response time) I ended up purshasing another unit.

     

    This one I double-checked everything and sure enough, the thing generally worked as expected.

    I'm now getting 130mV @ 3-4bar, expecting 150-200 mV.

     

    For now I consider my problem solved, and once again: Thank you guy for the help!

     

    Cheers,

    David Larsen.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • vsluiter
    0 vsluiter over 13 years ago in reply to e14 Contributor

    You're welcome. Thanks for reporting it's solved now!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • himanshuws
    0 himanshuws over 12 years ago

    Dear all,

     

     

    I am trying to get the pressure readings from the NBPDLNN030PAUNV. Could someone please let me know what logic/code should I use to obtain the pressure. Also, which pin to use to get the pressure readings I mean Vout- or Vout+ . I am using an arduino board and trying to take the pressure reading from both Vout- and Vout+ separately using the logic

     

     

    const float Null = 0.00; // Null VDC

      const float Sensitivity = 21.0;  // Sensitivity

      pressure = analogRead(ADC_HONEYWELL);

      pressureVDC = (float)pressure * 0.0048828125; // (5/1024 = 0.0048828125)

      pressureVDC = pressureVDC - Null;

      pressurePSI = pressureVDC / Sensitivity * 1000;

     

     

    None of the pin is giving me correct readings. Please let me know how should I write a code to obtain correct pressure readings. I have also searched on the internet but could not get any details about the code to get the pressure.Do I need to connect the Vout- and Vout+ pins some how and then take the pressure reading or do I need to include both Vout- and Vout+  in some logic to find the correct pressure readings.

     

     

    I am novice to sensors/automation/electronics. Could someone please suggest me a good blog/tutorial/book which I can follow to get started in this field.

     

     

    Waiting for your reply!!

     

     

    Regards,

    Himanshu