Sensors
  • Technologies
  • More
Sensors
Sensor Forum How to use pressure sensor (Honeywell NBPMLNN060PGUNV)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 351 subscribers
  • Views 1383 views
  • Users 0 members are here
Related

How to use pressure sensor (Honeywell NBPMLNN060PGUNV)

e14 Contributor
e14 Contributor over 13 years ago

I have acquired a 0-60psi pressure sensor, namely the NBPMLNN060PGUNV (nr. 2146011 from Farnell).

According to the datasheet sensitivity of the device should typically be 21mV/V/Full range. Essentially I figured that I would be able to get a ~100mV output

difference from the device - if connected to a 5V supply - measured between pins 2 and 4 (21mV * 5V = 105mV).

But when I connect the sensor to the supply, the output voltage is only 4mV, and decreasing when I increase the pressure.

When output voltage reaches 0, nothing else happens even if I increase the pressure further. Needless to say, this behaviour seems a bit peculiar to me.

 

Can anyone verify if this behaviour is correct? Because sensing on a voltage of only 4mV or less is rather difficult in my application.

 

For testing purposes, if I up the supply voltage to 10V, the output voltage also doubles (~9mV). But it is still a very small voltage difference to work with.

Am I doing something wrong or do I need to add a differential amplifier circuit to get higher voltage differences?

 

Thank you for your time.


Regards,

David Larsen

AKJ Inventions ApS.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi guys, sorry for the late reply.

     

    Thank you very much for your input!

    I made sure all connections were correct and then I tested the vacuum response. It also decreased when changing the pressure.

    So obviously something was wrong.

     

    It contacted the manufacturer, but due to no response (partly causing the long response time) I ended up purshasing another unit.

     

    This one I double-checked everything and sure enough, the thing generally worked as expected.

    I'm now getting 130mV @ 3-4bar, expecting 150-200 mV.

     

    For now I consider my problem solved, and once again: Thank you guy for the help!

     

    Cheers,

    David Larsen.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi guys, sorry for the late reply.

     

    Thank you very much for your input!

    I made sure all connections were correct and then I tested the vacuum response. It also decreased when changing the pressure.

    So obviously something was wrong.

     

    It contacted the manufacturer, but due to no response (partly causing the long response time) I ended up purshasing another unit.

     

    This one I double-checked everything and sure enough, the thing generally worked as expected.

    I'm now getting 130mV @ 3-4bar, expecting 150-200 mV.

     

    For now I consider my problem solved, and once again: Thank you guy for the help!

     

    Cheers,

    David Larsen.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • vsluiter
    0 vsluiter over 13 years ago in reply to e14 Contributor

    You're welcome. Thanks for reporting it's solved now!