Sensors
  • Technologies
  • More
Sensors
Sensor Forum liquid level sensor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 2 answers
  • Subscribers 353 subscribers
  • Views 3204 views
  • Users 0 members are here
  • level
  • sensor
Related

liquid level sensor

e14 Contributor
e14 Contributor over 11 years ago

hi,

i am designing a remote monitoring system for a small solar water heater. in this set up the water vapor is condensed and is collected in a container.I need to find a suitable sensor for measuring the collected liquid level.The amount of liquid collected is very minimal and the container is open at the top.If anybody have a suggestion please reply immediately.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 11 years ago in reply to e14 Contributor +1 suggested
    Hi Aiswaryaa, Have you checked out Spark Fun? They have a liquid height sensor. https://www.sparkfun.com/products/10221 John
  • dougw
    dougw over 11 years ago +1
    Any capacitance measurement circuit can be used to measure water depth as accurately as as your capacitance meter. The capacitor "plates" to be measured are simply vertical wires running up the length…
  • dougw
    dougw over 11 years ago in reply to markvenn +1
    It would work fine even with pretty large spacing and it doesn't matter if the container is conductive, although with a conductive container it would work better if the sense (insulated) wire is at least…
Parents
  • dougw
    0 dougw over 11 years ago

    Any capacitance measurement circuit can be used to measure water depth as accurately as as your capacitance meter. The capacitor "plates" to be measured are simply vertical wires running up the length of your container. The capacitance between the wires is directly proportional to the depth of water. One of the wires cannot be permitted to contact the water, so it needs to be insulated wire - I just run an insulated wire to the bottom and back up, to avoid having to seal the bottom end. The higher the dielectric constant of the wire, the larger the capacitance reading. For your small depth application you should use teflon coated wire for a high capacitance, but you can also increase capacitance simply by running more loops of wire to the bottom and back.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • markvenn
    0 markvenn over 11 years ago in reply to dougw

    Douglas

    Is there a maximum distance apart that this would work? I don't mean miles, just should it work across a bath tub sized gap? Assuming not an iron bath tub.

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 11 years ago in reply to markvenn

    It would work fine even with pretty large spacing and it doesn't matter if the container is conductive, although with a conductive container it would work better if the sense (insulated) wire is at least a couple of inches away from the edge.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 11 years ago in reply to markvenn

    It would work fine even with pretty large spacing and it doesn't matter if the container is conductive, although with a conductive container it would work better if the sense (insulated) wire is at least a couple of inches away from the edge.