Sensors
  • Technologies
  • More
Sensors
Sensor Forum Using inductive proximity sensors to measure displacement.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 25 replies
  • Answers 1 answer
  • Subscribers 352 subscribers
  • Views 7135 views
  • Users 0 members are here
  • sensors
  • proximity
  • inductive
Related

Using inductive proximity sensors to measure displacement.

e14 Contributor
e14 Contributor over 11 years ago

http://uk.farnell.com/multicomp/mcpip-t30l-001/sensor-m30-pnp-shielded-no/dp/2218049

 

I just bought these, later did I found out that inductive proximity sensors can detect metal in close proximity rather than the distance. I wanted to know if it's possible to by any simple modifications to this sensor that may result in measuring distance. I want to measure displacements of a steel shaft from 0~10mm and I am unable to find a cheap non-contact sensor for that purpose.

 

I had a read here: Position – Sensor Solutions | DigiKey TechZone


"Inductive sensors use a coil to generate a high frequency oscillating magnetic field to detect metallic objects. When a metal target enters the sensing field, eddy currents are induced in the target, which reduces the signal amplitude and triggers a change of state in the sensor output."

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago in reply to e14 Contributor +1
    You need to specify or describe your system in much more detail for anyone to make a decent sensor recommendation: The first question is " why not measure the force directly" - unless you describe the…
Parents
  • D_Hersey
    0 D_Hersey over 11 years ago

    Let me echo Doug W.'s concern about stray fields with the capacitance scheme.  To avoid this you may be able to build a Faraday shield.  This can be perforated, as long as the diameter of the holes is smaller than 1/4 wave at your highest frequency of interest.

     

    If you google for it, you can find a capacitance multiplier circuit that can be constructed from an op-amp.  This works for a capacitor that is returned to the supply.   Also google for an 'op-amp relaxation oscillator.'  The output of which you can count.  Using the multiplier increases sensitivity, while using the CCO gives you a squared-up signal that is easy to transmit.  You can get all of this functionality integrated from vendors such as TI.  I think their trade name is CapSense.

     

    You might want to use a machine scale on your 'slot' to know the point you are measuring.  You might use a ballscrew car to move your sensor.  If you get a dual-shaft motor, you can operate manually or by controller.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 11 years ago

    Let me echo Doug W.'s concern about stray fields with the capacitance scheme.  To avoid this you may be able to build a Faraday shield.  This can be perforated, as long as the diameter of the holes is smaller than 1/4 wave at your highest frequency of interest.

     

    If you google for it, you can find a capacitance multiplier circuit that can be constructed from an op-amp.  This works for a capacitor that is returned to the supply.   Also google for an 'op-amp relaxation oscillator.'  The output of which you can count.  Using the multiplier increases sensitivity, while using the CCO gives you a squared-up signal that is easy to transmit.  You can get all of this functionality integrated from vendors such as TI.  I think their trade name is CapSense.

     

    You might want to use a machine scale on your 'slot' to know the point you are measuring.  You might use a ballscrew car to move your sensor.  If you get a dual-shaft motor, you can operate manually or by controller.