Sensors
  • Technologies
  • More
Sensors
Sensor Forum Adapting a medical pendant to sense motion
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 350 subscribers
  • Views 652 views
  • Users 0 members are here
  • pendant
  • motion_detector
  • medical
  • schedule
Related

Adapting a medical pendant to sense motion

e14 Contributor
e14 Contributor over 11 years ago

I'm new here so I apologize if I'm posting this in the wrong forum.


Here's the deal: I've got a 97 year old grandmother in an assisted living facility who is prone to falling at night when she gets up to use the bathroom. Although she wears a pendant around her neck, unfortunately at her age she forgets to press it preemptively to have someone assist her. Inevitably she falls in the bathroom while maneuvering herself around and because she forgets she's wearing the pendant she lays there screaming for help in the hopes that someone will hear her or that she'll be rescued during the next regularly scheduled night check.


All of this made me think, there has to be a better solution. What if she had a box with a motion sensor? It's only active during a predetermined period that we can modify. If the motion sensor is triggered it would immediately trigger a built-in pendant which would notify the staff so that by the time she made it over to the restroom, they arrive to help her.


I'm not experienced enough to build this myself. I'd love some recommendations regarding who / where I can find someone to build the unit. Of course I would provide a pendant to be modified and adapted.

 

Best,

Howard

  • Sign in to reply
  • Cancel
Parents
  • dougw
    0 dougw over 11 years ago

    There are several motion sensors that could do something like this, but if they are sensitive enough to be sure to turn on, they may also turn on from other motion that should not cause an alarm.

    You could rig an old "electric eye" (light beam interruption detector) to detect when a person crosses from one space to another and trigger a warning from that.

    You could have a simple switch on a door to detect when it is opened or closed and trigger off that. (like an Enocean solar powered reed switch)

    You could have an RFID system that detects when someone is in a small room and triggers a warning from that.

    You could use a sensitive MEMS pressure sensor that can detect changes in elevation of a few inches - to detect when the sensor is near the floor and trigger off that.

    Probably the simplest is to connect a simple door switch to a separate pendant permanently mounted on the door jamb.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 11 years ago

    There are several motion sensors that could do something like this, but if they are sensitive enough to be sure to turn on, they may also turn on from other motion that should not cause an alarm.

    You could rig an old "electric eye" (light beam interruption detector) to detect when a person crosses from one space to another and trigger a warning from that.

    You could have a simple switch on a door to detect when it is opened or closed and trigger off that. (like an Enocean solar powered reed switch)

    You could have an RFID system that detects when someone is in a small room and triggers a warning from that.

    You could use a sensitive MEMS pressure sensor that can detect changes in elevation of a few inches - to detect when the sensor is near the floor and trigger off that.

    Probably the simplest is to connect a simple door switch to a separate pendant permanently mounted on the door jamb.