Sensors
  • Technologies
  • More
Sensors
Sensor Forum CO2 sensor for low volumes
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 348 subscribers
  • Views 5796 views
  • Users 0 members are here
Related

CO2 sensor for low volumes

Runzolf
Runzolf over 4 years ago

Hi,

I'm a student in medical engineering, looking for a new CO2 sensor for my veterinary support setup. What I'm looking for is to monitor the CO2 level in mice and rats exhalation. We are talking about ~4ml of tidal volume (volume per breath), which is a crucial factor. The update rate should be at least 4sec / 0.25Hz, while the range I'm looking for is max 100'000ppm / 10%. Even 5% could actually be fine.
Right now I have two K33 30% CO2 sensors, which seems perfect, but unluckily they stopped working so I'm looking for an alternative.
Also, the sensor must offer I2C / UART connection, in order to interface it with a microcontroller.

Any advice is really appreciated!
Rodolfo

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 4 years ago in reply to fmilburn +3
    That's an interesting part. Quite slow, (66ms) and poor accuracy at low CO2 levels. It works by measuring thermal conduction (of the gas I think) and is sensitive to thermal gradients but the data sheet…
  • Runzolf
    Runzolf over 4 years ago in reply to Runzolf +2
    I found it from another manufacturer's site: "The Active detector is sensitive in the range of absorption of the target gas, while the Reference detector wavelength bands are chosen in a region of the…
  • michaelkellett
    michaelkellett over 4 years ago in reply to Runzolf +2
    On page 11 of the data sheet you can see that the different devices offered use channel 1 as a non target gas responsive reference channel. This is because the IR source will not give the same output over…
Parents
  • fmilburn
    fmilburn over 4 years ago

    This isnt an area where I have much knowledge but did you look at the Sensiron STC-31?  https://sensirion.com/media/documents/7B1D0EA7/61652CD0/Sensirion_Thermal_Conductivity_Datasheet_STC31_D1_1.pdf

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 4 years ago in reply to fmilburn

    That's an interesting part. Quite slow, (66ms) and poor accuracy at low CO2 levels. It works by measuring thermal conduction (of the gas I think) and is sensitive to thermal gradients but the data sheet doesn't go into details.

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Runzolf
    Runzolf over 4 years ago in reply to michaelkellett

    The undetailed datasheet is quite annoying, or maybe it just states that the sensor is just a "ON / OFF" type, so the datasheet just describes in which LED working frequency range is more effective.

    Couldn't find it at higher-res: 

    image

    There is also an evaluating kit sold, which is basically the LED and the tube already built, which could save me a lot of hassle. It doesn't specify how powerfull should the LED be, it should depend on the NEP right? It states 2.7*10e-10 on the cheaper one, and "mean 70" on the dual sensor one. What ranges should I look for, in case I really wanted to go down that road?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Runzolf
    Runzolf over 4 years ago in reply to michaelkellett

    The undetailed datasheet is quite annoying, or maybe it just states that the sensor is just a "ON / OFF" type, so the datasheet just describes in which LED working frequency range is more effective.

    Couldn't find it at higher-res: 

    image

    There is also an evaluating kit sold, which is basically the LED and the tube already built, which could save me a lot of hassle. It doesn't specify how powerfull should the LED be, it should depend on the NEP right? It states 2.7*10e-10 on the cheaper one, and "mean 70" on the dual sensor one. What ranges should I look for, in case I really wanted to go down that road?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • fmilburn
    fmilburn over 4 years ago in reply to Runzolf

    I would get in touch with Sensiron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Runzolf
    Runzolf over 4 years ago in reply to fmilburn

    Oh, I think I replied to the wrong parent comment, I was talking about the KEMET. But for sure, I will get in contact with them.