Sensors
  • Technologies
  • More
Sensors
Sensor Forum Angle detection
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 350 subscribers
  • Views 2669 views
  • Users 0 members are here
  • Outboard engine angle project..
Related

Angle detection

Lou_Blue
Lou_Blue over 4 years ago

I have a boat. The engine can be tilted up or down, coving a range of around 260° from fully up to fully down. I would like a more sophisticated sensor that is better than the 5 mercury tilt switches I'm currently using, which works pretty well. This is useful for fuel efficiency and shallow water hazards.

Is there an upgrade available that I can fit in my engine?

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 4 years ago +2
    Your post has an angle theme so in the interest of community promotion there are two RoadTest that might give some insight. /products/roadtest/rt/roadtests/561/mps_magnetic_angle_p /products/roadtest…
  • robogary
    robogary over 4 years ago +1
    Are you asking if there is a commercially available alternative for engine positioning system and indication ? Are you looking for an infinitely adjustable angle position control ? Not sure this is the…
  • michaelkellett
    michaelkellett over 4 years ago +1
    This seems a very wide range of tilt angle, on my last (long time ago) power tilt outboard I think the range was about 90 degrees. Can you provide some pictures. My experience of boats suggests that…
Parents
  • shabaz
    shabaz over 4 years ago

    I can't think of anything of-the-shelf that could directly replace 5 mercury switches in an existing system. It may be possible to use a different type of sensor provided some circuitry was developed to interface it.

    Perhaps a sensor like this:

    https://www.newark.com/sensor-solutions-te-connectivity/g-nsdog2-003/mems-inclinometer-mems-30v-module/dp/03AC1403?st=inclimometer

    However, the range of that is 180 degrees, not 260 degrees. I don't know what accuracy and reliability you need, but a couple of those sensors might work, positioned so that they cover the full range you require. It's no bad thing to use two sensors, because if one fails, then the other can continue working until the failed one is replaced. You might also need some mechanical dampening for long life of the sensors (although the sensor PDF datasheet ( https://www.farnell.com/datasheets/2267166.pdf ) does suggest use with engines, they may require mounting to dampen vibrations (I'm guessing - I know nothing in this area). The datasheet does not mention boat applications (there could be all sorts of environmental issues using it for this application, like corrosion for instance).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 4 years ago

    I can't think of anything of-the-shelf that could directly replace 5 mercury switches in an existing system. It may be possible to use a different type of sensor provided some circuitry was developed to interface it.

    Perhaps a sensor like this:

    https://www.newark.com/sensor-solutions-te-connectivity/g-nsdog2-003/mems-inclinometer-mems-30v-module/dp/03AC1403?st=inclimometer

    However, the range of that is 180 degrees, not 260 degrees. I don't know what accuracy and reliability you need, but a couple of those sensors might work, positioned so that they cover the full range you require. It's no bad thing to use two sensors, because if one fails, then the other can continue working until the failed one is replaced. You might also need some mechanical dampening for long life of the sensors (although the sensor PDF datasheet ( https://www.farnell.com/datasheets/2267166.pdf ) does suggest use with engines, they may require mounting to dampen vibrations (I'm guessing - I know nothing in this area). The datasheet does not mention boat applications (there could be all sorts of environmental issues using it for this application, like corrosion for instance).