Sensors
  • Technologies
  • More
Sensors
Sensor Forum Angle detection
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 350 subscribers
  • Views 2665 views
  • Users 0 members are here
  • Outboard engine angle project..
Related

Angle detection

Lou_Blue
Lou_Blue over 4 years ago

I have a boat. The engine can be tilted up or down, coving a range of around 260° from fully up to fully down. I would like a more sophisticated sensor that is better than the 5 mercury tilt switches I'm currently using, which works pretty well. This is useful for fuel efficiency and shallow water hazards.

Is there an upgrade available that I can fit in my engine?

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 4 years ago +2
    Your post has an angle theme so in the interest of community promotion there are two RoadTest that might give some insight. /products/roadtest/rt/roadtests/561/mps_magnetic_angle_p /products/roadtest…
  • robogary
    robogary over 4 years ago +1
    Are you asking if there is a commercially available alternative for engine positioning system and indication ? Are you looking for an infinitely adjustable angle position control ? Not sure this is the…
  • michaelkellett
    michaelkellett over 4 years ago +1
    This seems a very wide range of tilt angle, on my last (long time ago) power tilt outboard I think the range was about 90 degrees. Can you provide some pictures. My experience of boats suggests that…
Parents
  • dougw
    dougw over 4 years ago

    Does this sensor simply indicate what angle you are manually setting the motor to, or is it used as feedback in a motorized angle setting mechanism?

    A simple accelerometer can measure angle with respect to gravity (which is what mercury switches do) - just like the accelerometer in most smart phones. It may need filtering to remove boat accelerations, or you could have one on the boat and one on the motor.

    If it is manual, you could just make a bracket to place your phone in while making the adjustment and run a tilt angle app. 

    The BBC micro:bit has a built-in accelerometer. I did a project that showed its use in measuring angles. Unfortunately all the links on this site that point to that project are broken, but here is one of the videos from that project:

    https://www.youtube.com/watch?v=T1dI5m7DBO4

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 4 years ago

    Does this sensor simply indicate what angle you are manually setting the motor to, or is it used as feedback in a motorized angle setting mechanism?

    A simple accelerometer can measure angle with respect to gravity (which is what mercury switches do) - just like the accelerometer in most smart phones. It may need filtering to remove boat accelerations, or you could have one on the boat and one on the motor.

    If it is manual, you could just make a bracket to place your phone in while making the adjustment and run a tilt angle app. 

    The BBC micro:bit has a built-in accelerometer. I did a project that showed its use in measuring angles. Unfortunately all the links on this site that point to that project are broken, but here is one of the videos from that project:

    https://www.youtube.com/watch?v=T1dI5m7DBO4