Sensors
  • Technologies
  • More
Sensors
Sensor Forum Any ideas for low-cost Thermocouple Interfacing methods?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 347 subscribers
  • Views 8532 views
  • Users 0 members are here
  • thermocouple
  • thermistor
Related

Any ideas for low-cost Thermocouple Interfacing methods?

shabaz
shabaz over 4 years ago

Note: See here for a project that resulted from this discussion: BLE EasyTempProbe 

Hi,

Since thermocouple measurement ICs are getting expensive/hard to find, I wished to use a single channel ADC, for thermocouple measurements (actually, I want to use a dual channel ADC for two thermocouples, but it's likely the same problem just doubled!).

The trouble is, the cold end of the thermocouple needs measuring too, and I was thinking of using a thermistor for that because that's easier to obtain (and cheaper) than an IC sensor. In summary, I wished to multiplex a thermistor and a thermocouple.

I've come up with the diagram below so far and wish to use it in an environment where the cold junction might be in the range of -40 to +50 deg C, and the thermocouple might be in the range of -40 to +400 deg C (maybe a Type J thermocouple). I think it will have an error of a few deg C. The ADC is 16-bit, and I likely won't be using the whole range of it. The ADC has a PGA of up to 8X, so it will be set to 8X when measuring the thermocouple.

The main benefit of the proposal below is that it is cheap since it just needs a couple of transistors and a few resistors. I could think of more complex circuits for a more accurate measurement, but it would be nice to see if this is good enough, or if it could be tweaked to be good enough unless anyone has other suggestions.

If it works, this would be a cheap way (under $5, ADC included) to have two thermocouples each with their own compensation, with the drawbacks that accuracy might be a few degrees at best, and no isolation either, unfortunately. 

Any ideas would be gratefully appreciated, since I'm sure I may be missing some great techniques, missing the wood for the trees, etc! Has anyone come across any low-cost methods to do such a thing? Any mistakes I'm making?

image

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 4 years ago +6
    Thinking out loud: Both transistors off, no path on input to 0V so ADC pins 2 and 3 pulled to 3.3V, probably outsiede ADC common mode range. Both transistors on, both sides of thermocouple pulled to…
  • shabaz
    shabaz over 4 years ago +3
    Hi fmilburn (Replying here to remove the comment indent, since I wanted to share some diagrams) I've had a shot at doing it, and was close to giving up since I was seeing huge errors!, but it was…
  • shabaz
    shabaz over 4 years ago +3
    I had a short bit of time to try to prototype this, it is not tested yet. The jumper positions on the left select different resistors, to simulate the thermistor, to be at a temperature of -30, 0, 25 or…
Parents
  • dougw
    dougw over 4 years ago

    The TC resistance is just 1 or 2 ohms per foot so do you really need Q2? The TC voltage can be subtracted from the thermistor reading.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to dougw

    Hi Doug,

    Everything interacts a bit, at a first approximation it's just the thermocouple voltage, but I'm down in the single-digit millivolts and it's harder to model with that precision without Spice, which the microcontroller won't have. I need to spend half a day or so properly modeling this, and start getting a feel for how much overall error there could be.It might be that the Q2 is not needed, if there isn't much difference in error with any model I can achieve in Excel.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 4 years ago in reply to shabaz

    Hi Shabaz,

    I am curious about “It might be that the Q2 is not needed, if there isn't much difference in error with any model I can achieve in Excel.” I am interested in hearing more detail and how how that exercise goes when you are finished. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fmilburn
    fmilburn over 4 years ago in reply to shabaz

    Hi Shabaz,

    I am curious about “It might be that the Q2 is not needed, if there isn't much difference in error with any model I can achieve in Excel.” I am interested in hearing more detail and how how that exercise goes when you are finished.