Sensors
  • Technologies
  • More
Sensors
Sensor Forum AHT10 - I2C problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 41 replies
  • Subscribers 344 subscribers
  • Views 13239 views
  • Users 0 members are here
  • sensors
  • AHT10
Related

AHT10 - I2C problem

msimon
msimon over 3 years ago

I just bought AHT10 humidity and temperature sensor. I have seen that it supports I2C and it is cheap so I didn't think thoroughly and bought two. I wanted to try them then I encounter a problem that only a single AHT10 can be connected to single I2C bus. I thought it is related to static address but it is worse (breakout board also showing two address but no details in the datasheet). The datasheet says that "Only a single AHT10 can be connected to the I2C bus and no other I2C devices can be connected." It sounds like traditional serial communication like RS232 not I2C. 

Is it normal to advertise it as an I2C device? and I also wonder what is the technical issue preventing to connect other devices with different address. Did you have any experience similar to this on any other sensor?

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 3 years ago +4
    Have you tried using the AHT10 with another device on the same I²C bus to see what happens ? It may be that it doesn't observe the stop condition so doesn't release itself from the host and continues…
  • BigG
    BigG over 3 years ago in reply to beacon_dave +4
    Both datasheets (AHT10 & AHT20) show that the sensor operates on microAmps, so powering by GPIO is possible too...
  • michaelkellett
    michaelkellett over 3 years ago +3
    I had a quick look at the data sheet. They don't appear to offer an explanation for why it doesn't work with other devices. I've used several other I2C humidity sensors and lots of I2C devices of other…
Parents
  • michaelkellett
    michaelkellett over 3 years ago

    I had a quick look at the data sheet. They don't appear to offer an explanation for why it doesn't work with other devices.

    I've used several other I2C humidity sensors and lots of I2C devices of other kinds. This is the first one I've seen that doesn't really work in an I2C bus system at all. (Some others have issues.)

    The good news is that it is very easy to make I2C devices work with normal IO pins so it should might be possible for you to connect it up without killing your I2C bus if you need that for other things.

    If you describe your system a bit more (schematic, controller type, pictures) it might be possible to make some definite suggestions.

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • msimon
    msimon over 3 years ago in reply to michaelkellett

    Hi  michaelkellett , I am planning to use it for Save the Bee design challenge. I can use GPIO as you suggested, use I2C mux, or simply change the sensor but I wonder is it normal? I just bought it because it supports I2C so I thought I could use the same pins for various devices but it is not possible. This is a cheap product so I don't mind. I wonder it is my mistake or its product's fault. I also want to learn is there any weird things similar to this. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 3 years ago in reply to msimon

    It's definitely not normal. I can't think of any other I2C chips that make such a requirement.

    I've used TI and Sensirion Humidity  sensors with no problems.

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 3 years ago in reply to msimon

    It's definitely not normal. I can't think of any other I2C chips that make such a requirement.

    I've used TI and Sensirion Humidity  sensors with no problems.

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • msimon
    msimon over 3 years ago in reply to michaelkellett

    I see. Someone used the term "partial compliance". I think it should be stated in the data sheet and on the seller's page as it doesn't comply with the actual protocol.