Sensors
  • Technologies
  • More
Sensors
Sensor Forum AHT10 - I2C problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 41 replies
  • Subscribers 344 subscribers
  • Views 13222 views
  • Users 0 members are here
  • sensors
  • AHT10
Related

AHT10 - I2C problem

msimon
msimon over 3 years ago

I just bought AHT10 humidity and temperature sensor. I have seen that it supports I2C and it is cheap so I didn't think thoroughly and bought two. I wanted to try them then I encounter a problem that only a single AHT10 can be connected to single I2C bus. I thought it is related to static address but it is worse (breakout board also showing two address but no details in the datasheet). The datasheet says that "Only a single AHT10 can be connected to the I2C bus and no other I2C devices can be connected." It sounds like traditional serial communication like RS232 not I2C. 

Is it normal to advertise it as an I2C device? and I also wonder what is the technical issue preventing to connect other devices with different address. Did you have any experience similar to this on any other sensor?

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 3 years ago +4
    Have you tried using the AHT10 with another device on the same I²C bus to see what happens ? It may be that it doesn't observe the stop condition so doesn't release itself from the host and continues…
  • BigG
    BigG over 3 years ago in reply to beacon_dave +4
    Both datasheets (AHT10 & AHT20) show that the sensor operates on microAmps, so powering by GPIO is possible too...
  • michaelkellett
    michaelkellett over 3 years ago +3
    I had a quick look at the data sheet. They don't appear to offer an explanation for why it doesn't work with other devices. I've used several other I2C humidity sensors and lots of I2C devices of other…
Parents
  • Andrew J
    Andrew J over 3 years ago

    Does look like you’re pretty stuffed with that device using I2C directly.  You could just swallow the cost and get an AHT20 (or alternately, if you describe your requirements someone here may be able to better advise).  As Michael says, you can skip the I2C bus and use other pins.  This post links to a GitHub library that provides a solution: https://www.stm32duino.com/viewtopic.php?t=1338

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • msimon
    msimon over 3 years ago in reply to Andrew J

    Hi  Andrew J , it is not an expensive product so money is not an issue. However AHT20 also not a good option as it has also have a static addressing. But it works with other I2C devices as mentioned datasheet. I am thinking bit banging on normal GPIO. I may buy other sensors but I want to see options. And also question it is normal or not. I think it is not normal and many people share the same opinion on the link you have provided. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • msimon
    msimon over 3 years ago in reply to Andrew J

    Hi  Andrew J , it is not an expensive product so money is not an issue. However AHT20 also not a good option as it has also have a static addressing. But it works with other I2C devices as mentioned datasheet. I am thinking bit banging on normal GPIO. I may buy other sensors but I want to see options. And also question it is normal or not. I think it is not normal and many people share the same opinion on the link you have provided.