Sensors
  • Technologies
  • More
Sensors
Sensor Forum AHT10 - I2C problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 41 replies
  • Subscribers 344 subscribers
  • Views 13244 views
  • Users 0 members are here
  • sensors
  • AHT10
Related

AHT10 - I2C problem

msimon
msimon over 3 years ago

I just bought AHT10 humidity and temperature sensor. I have seen that it supports I2C and it is cheap so I didn't think thoroughly and bought two. I wanted to try them then I encounter a problem that only a single AHT10 can be connected to single I2C bus. I thought it is related to static address but it is worse (breakout board also showing two address but no details in the datasheet). The datasheet says that "Only a single AHT10 can be connected to the I2C bus and no other I2C devices can be connected." It sounds like traditional serial communication like RS232 not I2C. 

Is it normal to advertise it as an I2C device? and I also wonder what is the technical issue preventing to connect other devices with different address. Did you have any experience similar to this on any other sensor?

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 3 years ago +4
    Have you tried using the AHT10 with another device on the same I²C bus to see what happens ? It may be that it doesn't observe the stop condition so doesn't release itself from the host and continues…
  • BigG
    BigG over 3 years ago in reply to beacon_dave +4
    Both datasheets (AHT10 & AHT20) show that the sensor operates on microAmps, so powering by GPIO is possible too...
  • michaelkellett
    michaelkellett over 3 years ago +3
    I had a quick look at the data sheet. They don't appear to offer an explanation for why it doesn't work with other devices. I've used several other I2C humidity sensors and lots of I2C devices of other…
Parents
  • shabaz
    shabaz over 3 years ago

    Just curious, what is the scenario where they will both be deployed connected to the same microcontroller?
    Ordinarily, the distance cannot be too great with I2C (i.e. i2C not normally used for local/remote sensing, unless remote is something inside the same enclosure (usually). Do you intend to have the sensors connected over a long distance?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • msimon
    msimon over 3 years ago in reply to shabaz

    I am planning to put one inside the hive the other outside the hive on the same microcontroller. I am thinking to put them roughly 10cm away from each other located on the top of the hive. However, the configuration may change as there are various thermal spots inside the hive. Actually, I may need more than two still researching characteristic of the hive temperature. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to msimon

    I see; in that case, perhaps something like this could be useful, it's a low-cost component (PCA9548A), called an I2C Multiplexer if you're looking for such types of parts. Then you're free to add quite a lot of sensors. 

    Personally I'd do it in software though (i.e. using GPIO pins) if there are enough pins. But this could be a scalable way for up to 8 devices (actually up to 64 devices, since you can install many of these PCA.. chips but that seems an unlikely scenario).

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago in reply to msimon

    I see; in that case, perhaps something like this could be useful, it's a low-cost component (PCA9548A), called an I2C Multiplexer if you're looking for such types of parts. Then you're free to add quite a lot of sensors. 

    Personally I'd do it in software though (i.e. using GPIO pins) if there are enough pins. But this could be a scalable way for up to 8 devices (actually up to 64 devices, since you can install many of these PCA.. chips but that seems an unlikely scenario).

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • msimon
    msimon over 3 years ago in reply to shabaz

    Actually, there may be a translation error. It works with TMP102 sensor. I also think GPIO is a good option.

    I won't invest in a mux for these unreliable sensors. I just want to play with them and see how I can mitigate it. If things not sorted, I will buy a better sensor.